DIY Test Instrumentation
  • Challenges & Projects
  • Project14
  • DIY Test Instrumentation
  • More
  • Cancel
DIY Test Instrumentation

Blog

  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DIY Test Instrumentation to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • DIY 3-D Printed 4-Wire Kelvin LCR Adapter for SMD Components

    fmilburn
    fmilburn
    In this post, I present a DIY 3D printed adapter for 4-wire Kelvin measurement of SMD components with an LCR meter.  The adapter has been tested with the Multicomp Pro handheld LCR meter (rebranded Hantek 1833C) and should work with the DER DE-5...
    • 23 Sep 2021
  • The Missing Link (BBC-PCB)

    dougw
    dougw
    BackgroundI recently used breadboards in a couple of projects and rediscovered some of their utility as well as many of the myriad reasons why I stopped using them years ago.I started to list all the reasons why I was turned off breadboards, in a hum...
    • 15 Aug 2021
  • SCDVM : Solar Cell Characteristic Measurement

    dubbie
    dubbie
    For the DIY Test Instrument Project14 Challenge I decided that I wanted to make something using a graphic display and something I have been playing with this summer (when the sun actually shines!) are solar cells. Solar cells are interesting things a...
    • 13 Aug 2021
  • SSFG - Simple stupid function generator

    amgalbu
    amgalbu
    I recently went through this blog postCreating a function generator from an Arduino board that can be programmed by means of a VT100 serial terminal looks a good idea to. After all, it's a very common scenario to have a PC on your workbench and, ...
    • 11 Aug 2021
  • DIY 100kHz VCO - Build & Test

    navadeepganeshu
    navadeepganeshu
    VCO -- A black box that provides an oscillating electrical signal whose frequency can be controlled by providing DC voltage input to it.Voltage Controlled Oscillators are fairly popular circuits used as subsections in PLLs, Music Synthesizers, Test a...
    • 10 Aug 2021
  • Pico Puffer

    scottiebabe
    scottiebabe
    Introducing, the Pico Puffer a high precision capacitance meter. With the name puffer being a fun adaptation of the short-form saying of pico-farads as puffs. My hope for this project is to be able to make a capacitive soil moisture measurement....
    • 10 Aug 2021
  • Instrument Control Board - Detailed Information and Testing

    Andrew J
    Andrew J
    Introduction Apologies to anyone who has read a lot of this already, I just couldn’t work out how to turn an existing blog into a Project14 entry.  If you have read any of those posts, then much of this information will be familiar but th...
    • 5 Aug 2021
  • IRRF 2000 the IR and RF Tester

    gam3t3ch
    gam3t3ch
        Sometimes there is just no tool that will get the job done quickly and efficiently so sometimes we have to modify an existing tool or create our own to accomplish what we need in much less time then prior methods.   I work primar...
    • 3 Aug 2021
  • 3D Printed Surface Mount Test Lead Tweezers

    fmilburn
    fmilburn
    In this post, I am going to show the process I went through to build SMD test measurement tweezers.  Will they work?  I started with loose goals in mind, iterated, and made something physical daily with what was at hand. 18 July 2...
    • 1 Aug 2021
  • Simplester - a simple cable tester

    koudelad
    koudelad
    DIY Test Instrumentation        Submit an EntrySubmit an Entry Monthly Themes   | Monthly Poll   |  Back to homepage   DIY Test Instrumentation      &...
    • 17 Jul 2021
  • Viewing Noise with a Measurement Amplifier

    shabaz
    shabaz
    Table of Contents Introduction Block Diagram Circuit Diagram Power Entry Input Stage First Gain Stage Filter Stage Attenuator Second Gain Stage Offset Null Low Power Indicator Proto Area Circuit Board and Construction Enclosure Frequency Respo...
    • 16 Jul 2021
  • A gadget for power monitoring of SBCs and MCU boards

    embeddedguy
    embeddedguy
    DIY Test Instrumentation        Submit an EntrySubmit an Entry Monthly Themes   | Monthly Poll   |  Back to homepage  Give Us Your Ideas on DIY Test Instrumentation Projects in the...
    • 4 Jul 2021
  • Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester vi (shifting gears!)

    phoenixcomm
    phoenixcomm
    U.S. Air Force Senior Master Sgt. Mike Chandler, 142nd MaintenanceSquadron out of the Portland Air National Guard, displays his avionicsElectronics Systems Test Station (ESTS) cable tester that he designedPhoto by: Airman First Class Andrew Kobialka ...
    • 3 Jul 2021
  • Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester v

    phoenixcomm
    phoenixcomm
    U.S. Air Force Senior Master Sgt. Mike Chandler, 142nd MaintenanceSquadron out of the Portland Air National Guard, displays his avionicsElectronics Systems Test Station (ESTS) cable tester that he designedPhoto by: Airman First Class Andrew Kobialka ...
    • 1 Jul 2021
  • Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester iv

    phoenixcomm
    phoenixcomm
    U.S. Air Force Senior Master Sgt. Mike Chandler, 142nd MaintenanceSquadron out of the Portland Air National Guard, displays his avionicsElectronics Systems Test Station (ESTS) cable tester that he designedPhoto by: Airman First Class Andrew Kobialka ...
    • 1 Jul 2021
  • Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester iii

    phoenixcomm
    phoenixcomm
    U.S. Air Force Senior Master Sgt. Mike Chandler, 142nd Maintenance Squadron out of the Portland Air National Guard, displays his avionics Electronics Systems Test Station (ESTS) cable tester that he designed. Photo by: Airman First Class Andrew Kobia...
    • 27 Jun 2021
  • Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester ii

    phoenixcomm
    phoenixcomm
    Design Overview: As I said in the last blog I am going to use an Arduino Mega 256 not for its I/O capabilities, but for its memory size.  Getting to 50 pins is really 100 pins! Ouch. The only way I can achieve this is to use 4 16 bit I/O expand...
    • 24 Jun 2021
  • Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester i

    phoenixcomm
    phoenixcomm
      In its simplest form, you would have a wire and a DVM with its leads on both ends like you would measure resistance. With more wires comes more headaches. And this is what I want to test for: Pin-out connector A to Pin-out connecto...
    • 20 Jun 2021