DIY Test Instrumentation
  • Challenges & Projects
  • Project14
  • DIY Test Instrumentation
  • More
  • Cancel
DIY Test Instrumentation
Blog Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester ii
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DIY Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 24 Jun 2021 2:17 PM Date Created
  • Views 3730 views
  • Likes 7 likes
  • Comments 5 comments
  • mcp23017
  • arduino mega 2560
  • i2c lcd display
  • diytestinstrumentationch
  • i2c expander
Related
Recommended

Project14 | DIY Test Instrumentation: Build Your Own Test Instrumentation!: Automated Cable Tester ii

phoenixcomm
phoenixcomm
24 Jun 2021

imageDesign Overview: As I said in the last blog I am going to use an Arduino Mega 256 not for its I/O capabilities, but for its memory size.  Getting to 50 pins is really 100 pins! Ouch. image

The only way I can achieve this is to use 4 16 bit I/O expander. Enter the MCP23017 which has a High-speed I2CTm interface (100KHz, 400KHz, 1.7MHz) and I can have eight (8) devices on this bus at one time. But I will only use 2 expanders on the input, and two more on the output.   I will also include an I2CTm interfaced LCD panel for display and control. The Arduino itself will read the buttons to scroll through the cables, or to enable the flying probe. I can interface the tester to my PC via USB or Ethernet (later). Well for better or worse, here it is. 

UPDATE - 6 JUN 2021
On one side I will have 3 MCP2317 as to also allow me to use a DB-37. and BTW it is just as easy to add the DB-37 to both sides.  image

 

 

 

Device Unit Pins
MCP23017 1 1 - 16
" 2 17 - 32
" 3 33 - 37
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +1
    Chris, Routing 50 I/Os is quite a task. I know that you use CAN a lot in your design. It's hard to get i2c routed over a distance, because it doesn't have a physical layer designed to go far. Would it…
  • DAB
    DAB over 5 years ago +1
    Reminds me of one of my early jobs in building a missile test station. Dozens of cables, hundreds of wires. I was very glad when that job was done. DAB
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to Jan Cumps +1
    Jan Cumps Jan. If I used the can for transport I still need 50 pins and I don't know of a can-based I/O expander it will up the parts count and I am trying to KISS (Keep It Simple Stupid). And just for…
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to Jan Cumps

    /members/jancumps 50 wires are not much work on a plane!! lucky me I did not have to build the dam things!! now I do Persevere

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to phoenixcomm

     I still need 50 pins

    yes, but not 50 wires routing from a single source all around the vehicle. They can be branched out locally at the point of load

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to Jan Cumps

    Jan Cumps  Jan. If I used the can for transport I still need 50 pins and I don't know of a can-based I/O expander

    it will up the parts count and I am trying to KISS (Keep It Simple Stupid). And just for giggles 4 x 16 = 64 total pins Not Bad.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    Reminds me of one of my early jobs in building a missile test station.

    Dozens of cables, hundreds of wires.

     

    I was very glad when that job was done.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago

    Chris,

    Routing 50 I/Os is quite a task.

    I know that you use CAN a lot in your design.

    It's hard to get i2c routed over a distance, because it doesn't have a physical layer designed to go far.

    Would it help to build CAN-commanded 50-pin connectors? Not complex ones, just smart enough to be able to read/write each of the pins?

     

    edit. I'm not referring to the cable tester, I'm referring to the requirement to have cable beams of 50 I/O wires from one component to the next ...

    in the late 80's I worked for truck company DAF, and these were the things I struggled with at the time image:

    image

    Image source: wiring harness of a DAF 95. Source: https://www.trucks.nl/tweedehands-daf-kabelboom-95-ati-4642437-vd

    CAN should solve at least part of that.