Electromagnetism
  • Challenges & Projects
  • Project14
  • Electromagnetism
  • More
  • Cancel
Electromagnetism
Blog One String Electric Guitar #5 : Assembling the Final Guitar Body
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Electromagnetism to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 8 Apr 2019 12:34 PM Date Created
  • Views 2983 views
  • Likes 11 likes
  • Comments 10 comments
  • electric guitar
  • electromagnetismch
Related
Recommended

One String Electric Guitar #5 : Assembling the Final Guitar Body

dubbie
dubbie
8 Apr 2019

Once the final guitar body had been shaped it was time to paint it. I decided to follow a painting strategy of undercoat then top coat of spray paint. The undercoat was just a wood primer and undercoat combined, which I sanded down after the first coat and then undercoated it again and sanded it again to try and get as smooth a finish as reasonable. The undercoat did show up many imperfections which I thought I had eliminated by using the wood filler. I must have been looking the other way as there are several quite obvious dips and imperfections. Still, I was in the painting phase and I didn't want to delay any more.

 

image

 

For the top coat I decided to spray paint as I thought this would give me the smoothest finish. I made myself an ad-hoc spray booth inside my garage as it was too wet and cold to do this outside. I first sprayed everything with a white acrylic gloss finish which was pretty good but showed up even the tiniest imperfection. It would feel smooth but imperfections could still be seen. I'm not sure what size imperfections can be detected by a finger tip but I have always thought it was in the microns, but from looking at my guitar I think I may be wrong!

 

image

 

In the photographs it doesn't look that different but you can just seen the gloss sheen on the bottom edge near the pickup hole.

 

As the backend of the guitar body has the 'classic' arrow feather shape I decided to carry that forward with the paint. Having seen other guitars that were white and red I decided to use the same combination. The brightest red I could obtain was cherry red which was exactly what I was looking for. I used masking tape to cover the white part with newspaper, hoping it would not pull off the white when it was removed. Fortunately it didn't but somehow part of the newspaper must have become wet as some of the ink transferred to the guitar body. Fortunately I was able to just touch it up with white spray.

 

image

 

 

image

 

image

 

It looks OK but the paint surface is quite fragile, probably because it is just acrylic rather than enamel, but the acrylic was cheaper. You make your choice and then you have to stick with it. I could cover everything with a clear varnish to protect the paint and get a better gloss finish but time is running out and it would be even more expense. I think I have spent more on paint than anything else for this project.

 

I think it looks OK. I re-assembled the string holding parts and tensioning as all the holes were still available. I think it might even sound a little bit better.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

All I have to do now is re-insert the pickup and add the headphone amplifier and it will be finished. There is just about enough time to get that all done before the end of the competition.

 

Dubbie

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +3
    Looking good! That turned out looking quite sharp. Good luck with the final push to complete your project! Gene
  • dubbie
    dubbie over 7 years ago in reply to genebren +3
    Gene, Thanks for this. It does look pretty much like I had hoped/planned it would, although perhaps not as smooth or hardwearing. The replacement case for the amplifier is printing as I type. The first…
  • 14rhb
    14rhb over 7 years ago +3
    Nice design and paint finish - I cannot help thinking that KISS will be knocking on your door for a production run. Rod
Parents
  • crewedaddy
    crewedaddy over 7 years ago

    You need to add a strip of hard plastic or bone near to the headstock for the string to tension over. It's called the nut and it's where the scale length will start from. Pointless adding frets until you put that in, it'll never stay in tune.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • crewedaddy
    crewedaddy over 7 years ago

    You need to add a strip of hard plastic or bone near to the headstock for the string to tension over. It's called the nut and it's where the scale length will start from. Pointless adding frets until you put that in, it'll never stay in tune.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 7 years ago in reply to crewedaddy

    Richard,

     

    Thanks for reminding me of this. I had been planning to put one of these in but time ran out. Maybe I'll return to it at some time just to see if I can add some frets and get some better tuning.

     

    Dubbie