Electromagnetism
  • Challenges & Projects
  • Project14
  • Electromagnetism
  • More
  • Cancel
Electromagnetism

Blog

  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Electromagnetism to participate - click to join for free!

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • An Attempt at Building a DIY Spring Reverb Tank Using Electromagentism

    tariq.ahmad
    tariq.ahmad
    www.youtube.com/watch Originally Posted by aptbartmess I love the sound of the old mechanical spring reverbs found in Hammond organs and Fender amps. I've been wanting to make my own and when this month's science contest was announced I decid...
    • 19 Nov 2021
  • Smarthab: Door Strikes 2

    phoenixcomm
    phoenixcomm
    Good Electric Strikes are not cheap. Yes, you can buy one for 30 - 50 dollars but in the end, you might not like it. Remember here is definitely: You Get What You Paid For It. So think twice before you drop your bucks on some cheap imported crap! ...
    • 24 Apr 2019
  • 3000A clamp table and amplifier update #2

    three-phase
    three-phase
    I have done some more work today on the current amplifier and found that I did not have the input turned up to a high enough voltage to obtain the full 1A output, so I have now repeated the test and monitored the heat output from the amplifier. ...
    • 15 Apr 2019
  • Measuring Electromagnets - the Magneto Mutant Magnetic Measurement Meter (MMMMM-1000)

    shabaz
    shabaz
    IntroductionWhen making electromagnets, it is difficult to know for sure what kind of magnetic flux density has been achieved. This is because it depends a lot on practical construction factors, where on the electromagnet it is measured, and the core...
    • 15 Apr 2019
  • 3000A clamp table and amplifier update #1

    three-phase
    three-phase
    I haven't had much chance to work on the clamp table this week so it isn't quite complete, the majority of the time has been spend building and testing the current amplifier after the PCB had arrived. For the clamp table,  I have cu...
    • 14 Apr 2019
  • Easy Peasy Non-Contact Electricity Detector (Not a Metal Detector)

    mahmood.hassan
    mahmood.hassan
    Before building this device I have tried lots of different design but in every circuit there were some issues, either it was also a metal detector or detect human as AC voltage source. I even built a device using instrumentation amplifier, 2nd order...
    • 14 Apr 2019
  • One String Electric Guitar #6 : Final Assembly and Working Guitar

    dubbie
    dubbie
    After all the painting and finishing off the One String Electric Guitar has been finished. I re-installed the pickup and wired it directly into the headphones amplifier  as this enabled me to create an untethered system that I could then plug d...
    • 11 Apr 2019
  • One String Electric Guitar #5 : Assembling the Final Guitar Body

    dubbie
    dubbie
    Once the final guitar body had been shaped it was time to paint it. I decided to follow a painting strategy of undercoat then top coat of spray paint. The undercoat was just a wood primer and undercoat combined, which I sanded down after the first c...
    • 8 Apr 2019
  • The KLINGMAGON Subspace Probe

    dougw
    dougw
    No wires, no batteries, no solar panels, no screws, no glue and no suction cups, but a Klingmagon Subspace Probe can scavenge power to operate and cling to a vertical window without supports. I have been planning to build an outdoor digital thermome...
    • 8 Apr 2019
  • 3000A current clamp table and amplifier

    three-phase
    three-phase
    ElectromagnetismEnter Your Electronics & Design Project for a chance to win a $100 Shopping Cart!Back to The Project14 homepage Project14 HomeMonthly ThemesMonthly Theme Poll IntroductionFor my entry in the electromagnetism contest, I decide...
    • 7 Apr 2019
  • One String Electric Guitar #4 : Making the Final Guitar Body

    dubbie
    dubbie
    Having created the prototype one string electric guitar body and pickup I wanted to be able to hear the sounds it makes. I don't have a guitar amplifier so I decided to use an ordinary music amplifier instead but this needs a pre-amp to make it w...
    • 28 Mar 2019
  • One String Electric Guitar #3 : Completing the Prototype

    dubbie
    dubbie
    As the prototype body for the one string electric guitar has been completed the next step is to make the pickup coil. I have previously made a 3D printed bobbin to wind the coil on so all I need now is to select the wire to be used and wind it. I hav...
    • 21 Mar 2019
  • One String Electric Guitar # 2 : Building the Guitar

    dubbie
    dubbie
    I thought I would start the building of the guitar body with the pickup itself. As I have a magnet which I think is suitable I decided to 3D print a bobbin that fitted it to hold the winding coil. The magnet is 8 mm in diameter and 15 mm in length so...
    • 14 Mar 2019
  • One String Electric guitar #1 : Getting Started

    dubbie
    dubbie
    I saw the Project14 monthly topic of Electromagnetism and thought about it for a bit and couldn't think of anything that I could do - there didn't seem anyway of involving mobile robots in this, so I had decided not to participate. Some time ...
    • 11 Mar 2019
  • Onoring Alessandro Volta: How to make a Salt Water Battery

    toolkitman
    toolkitman
    Here is more a tutorial to make a battery i remember when i was young to have made one of this have a look at the link, it's not mine (wiki source) but i know how to make it! https://www.wikihow.com/Make-a-Homemade-Battery Here is shown how...
    • 23 Feb 2019
  • Cigarette computer

    toolkitman
    toolkitman
    I was thinking after seeing the size of the Raspberry Pi Zero to how the measures will be the next two generations of desktop computers. I guess they will not be wider than a cigarette and you will come to the suppression of the USB ports and HDMI an...
    • 23 Feb 2019
  • Wireless HDMI Solution

    toolkitman
    toolkitman
    Dear Element14,Mine more than a project is an idea on how to make work a modern computer with HDMI to a HDMI monitor or tv with a wirless connection, i know there is wirless for wifi router bluetooth for devices but noneuntil now have look inside the...
    • 23 Feb 2019
  • Smarthab: Door Strikes

    phoenixcomm
    phoenixcomm
    I use an electric door strike, on Smarthab, it is relay controlled via 24VAC from the room controller. The room controller is a TI C3200 LaunchPad, this gives me ethernet access so there is no money wasted. The room controller talks to an external ke...
    • 23 Feb 2019
  • Flipping Core Memory Bits Directly With a Magnetic Stylus

    abg123
    abg123
      This project is turning into a product! Check out the dedicated website www.Core64.io for the latest information. [The snake game works!!! Jump to the bottom of the post to see it in action!]   I’ve been captivated by magnetism, a...
    • 22 Feb 2019