Electromagnetism
  • Challenges & Projects
  • Project14
  • Electromagnetism
  • More
  • Cancel
Electromagnetism
Blog One String Electric Guitar #6 : Final Assembly and Working Guitar
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Electromagnetism to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 11 Apr 2019 1:28 PM Date Created
  • Views 3879 views
  • Likes 13 likes
  • Comments 22 comments
  • electric guitar
  • electromagnetismch
  • one string guitar
Related
Recommended

One String Electric Guitar #6 : Final Assembly and Working Guitar

dubbie
dubbie
11 Apr 2019

After all the painting and finishing off the One String Electric Guitar has been finished. I re-installed the pickup and wired it directly into the headphones amplifier  as this enabled me to create an untethered system that I could then plug directly into the main music amplifier that I have. It would have been interesting to plug the guitar directly into a proper guitar amplifier but time has now run out so this will not be happening.

 

The existing box for the headphones amplifier was not suitable for fixing directly to the guitar body so I designed a 3D printed one. This took much longer than I had anticipated. For the first version I didn't wait long enough for the printer plate to warm up as I only waited until it was 50 degrees centigrade whereas it really needs to be higher, at least 55 - 60 C, so the box didn't stick to the plate. The second version, which I amended so that all the plugs and controls had the correct opening, didn't have the correct openings, in fact they were worse than the first version. I think I may have been viewing the box back-to-front when entering the design, so that version was no good. As time was rapidly running out I decided to go for a much simpler design of just a rectangular box with a side slot for all the important controls and connections. It does mean I will have to unscrew the box when I want to recharge it but that was the price of getting it finished. For this project I wanted to make something that was functionally complete and nicely finished and packaged, so it had to be.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

As you can see and hear from the video it looks pretty much like an electric guitar and makes a gratifying electric guitar like sound. It has tone, volume and overdrive controls. I do play a tune of sorts in the video, anyone know what it is? Not a normal electric guitar song but as I am no musician this is about the best I can manage. The tune deteriorates after a bit as I don't know where the next notes are.

 

I haven't tuned the string, although I have demonstrated previously that it can be done and I didn't add any frets. Time has run out and to be honest I have had enough of it. The sun is shining and I am going to sit outside for a bit with a can of sugar free, caffeine free coke. I may even have a doze.

 

Dubbie

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago +6
    This was a fun build to watch and well done and finished. I immediately recognized the tune from the Sound of Music. I could almost hear Julie Andrews trying to keep up with you. The built in Fuzz Tone…
  • dubbie
    dubbie over 7 years ago in reply to jc2048 +5
    Jon, The tune, if it could be called that, which sort of appears after the first few seconds is Doe a deer a female deer from Mary Poppins I think. After a bit it then degenerates into random plonking…
  • dubbie
    dubbie over 7 years ago in reply to jw0752 +5
    John, Good to know my playing wasn't too bad!!!. It was fun to build, mostly. Soldering the wires for the pickup was a real challenge. My eyesight is not so good now and the coil wire was so thin that…
  • clem57
    clem57 over 6 years ago in reply to dubbie

    Being only one string, I can understand the lonelinessimage.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to clem57

    Thanks, I liked the paint job as well. and the construction. It was amazing and interesting to see what could be achieved with relatively simple mechanical and electrical/electronic components. Sadly, it just sits in a corner now neglected and alone.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 6 years ago

    Wonderful project dubbie . Quite an inspiration. I like the paint job mostly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    Hi dubbie, I really enjoyed watching your project come along in your series of blogs, and the professional finish that you achieved; so much so that it is on my list of things to build image. I'll be looking out for your next cool project idea.

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to aptbartmess

    Patrick,

     

    Thanks for the support. It was a fun build. It was the first time (that I can remember!) when I created a completed product for the project and it took a lot of time making the wooden parts and then painting it. I am thinking of fixing it to the wall somewhere (possibly the garage!) as a decorative item as I don't think I will learn to play it.

     

    Yes, I am planning to be involved in future Project14 activities, but I think I'll stick more to the robots in future, much easier.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>