Electronic Art
  • Challenges & Projects
  • Project14
  • Electronic Art
  • More
  • Cancel
Electronic Art
Blog Electronic Art app controlled by Arduino Uno
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Electronic Art to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ilvyanyatka
  • Date Created: 28 Aug 2020 2:23 AM Date Created
  • Views 5950 views
  • Likes 12 likes
  • Comments 24 comments
  • electronic art app
  • electronicartch
  • c#.net
  • arduino
Related
Recommended

Electronic Art app controlled by Arduino Uno

ilvyanyatka
ilvyanyatka
28 Aug 2020

My project is an electronic Art App controlled by Arduino Uno.

The app connects to Arduino port. goes full screen, and starts drawing abstract geometrical figures based on parameters it reads from the Arduino. The user can can control what the app is drawing using potentiometers, switches, and a push button. Everything can be controlled by Arduino, there is no need for keyboard and mouse (after connecting to Arduino port). App can be used for meditation, or just to relax. Drawings can be saved in real time using push button.

 

Push button 1 – clears app screen

Push button 2 - save the screenshot of the drawing

Switch 1 – Start/Stops drawing

Switch 2 – controls line type. Line type can be an Arc (Bezier curve) or a straight line

Potentiometer 1 – controls line width

Potentiometer 2 – controls an angle for a drawing

Potentiomenter 3 - controls drawing speed

 

The app itself is written in C#.NET. To communicate between .NET and Arduino I used open source Sharer library, it is awesome and it can be found here:

https://github.com/Rufus31415/Sharer

 

Fun fact: When testing the board I ran into a problem that all analogRead() functions returned incorrect values. I could not figure out why, it was driving me crazy. I was sure that I fried both of my Arduinos somehow. But finally I figured out that connections on my $1 breadboard were not wired properly. I changed the breadboard and everything started working right away.

 

 

Schematics (updated):

image

 

 

Demo video: (can also be found on YouTube: https://youtu.be/DOUr6JplXHg )

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Additional demo video for using save screenshots and changing drawing speed

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Couple of screenshots:

image

 

and

image

 

 

and

image

 

 

This is how the board looks like:

image

Arduino code, and NET main module with math and Arduino communication code will be attached soon.

Update: Code on Github: https://github.com/ilvyanyatka/ElectronicArtWithArduino

Before I added "Save screenshot" functionality, the code was cross platform. Now .NET code is Windows specific. To make it cross platform again one need to remove all the functionality related to "Select Windows Dialog" and "Take Screenshot". I am planning to come back to it later.

Attachments:
Electronic_Art.ino.txt.zip
  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 6 years ago in reply to jw0752 +5
    I thought it was a fun project also. Well done
  • ilvyanyatka
    ilvyanyatka over 6 years ago in reply to jw0752 +4
    Thank you John, will do it tomorrow! I am glad you liked it!
  • ilvyanyatka
    ilvyanyatka over 6 years ago in reply to jw0752 +4
    John, I will, because it is so much fun. This projects bring a lot of emotions. When I was working on this one, all of analogRead values for all the pins were totally wrong. I thought I fried both of my…
Parents
  • dubbie
    dubbie over 6 years ago

    Victoria,

     

    This produces some good art effects. Do you have a method for printing out to make permanent copies? Also, it would be interesting to try diffeerent shapes, perhaps more rectangular as well as circles/ovals.

     

    A good project.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ilvyanyatka
    ilvyanyatka over 6 years ago in reply to dubbie

    Dubbie

    Thank you for the ideas!

    To print the screenshots I used the "Print Screen" button, but it will be pretty easy to add to the app a hot key for printing (I am trying to avoid menus, because I want to use the whole area of a screen).

     

    Adding other geometrical figures could be fun. I will just need something like a 4-positions switch for it. Btw, what is the correct term for it it in English?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to ilvyanyatka

    Victoria,

     

    A four position switch is pretty much a suitable term.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to ilvyanyatka

    "...Adding other geometrical figures could be fun. I will just need something like a 4-positions switch for it..."

    You may find that at some point 4 positions won't be enough. You perhaps may need to use an up/down & select method using three push button switches to select the geometrical figure from a list.

     

    You can also get rotary encoders with built-in pushbutton that can work well for this task

    https://www.adafruit.com/product/377

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 6 years ago in reply to ilvyanyatka

    "...Adding other geometrical figures could be fun. I will just need something like a 4-positions switch for it..."

    You may find that at some point 4 positions won't be enough. You perhaps may need to use an up/down & select method using three push button switches to select the geometrical figure from a list.

     

    You can also get rotary encoders with built-in pushbutton that can work well for this task

    https://www.adafruit.com/product/377

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ilvyanyatka
    ilvyanyatka over 6 years ago in reply to beacon_dave

    Hello Dave,

     

    Thank you. Rotary encoders look like very useful components. I never heard of them before.

     

    For Up/Down/Select controls, I am trying to avoid any UI elements on the screen. Trying to keep it completely black.

    I coded a prototype using just .NET code, no Arduino. But UI controls make part of the screen unusable and make graphics look not so fun, not so relaxing.

    With Arduino it is easier to control the data. In this case used don't need a mouse and keyboard at all, and can change the angle from, for example, 30 degree to 179 degree in split second. When using UI controls, like track bar, it takes several seconds to change the value; and graphics code picks up the values in between that I am also trying to avoid.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to ilvyanyatka

    Hi Victoria,

     

    Yes, the rotary encoder technique tends to rely on some other means of displaying the options list. It doesn't have to be on the main display screen though, you could have LEDs with text labels indicating the currently selected geometry, or a 2-line LCD display panel on the controller device.

     

    However, yes, as you point out, the speed of being able to change the value could be an issue with a rotary encoder solution.

     

    It is all part of the fun of user interface design. image