Project14
  • Challenges & Projects
  • More
Project14
Forum What Changes Would You Like to See Made to Project14?
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 105 replies
  • Subscribers 207 subscribers
  • Views 16026 views
  • Users 0 members are here
Related

What Changes Would You Like to See Made to Project14?

tariq.ahmad
tariq.ahmad over 5 years ago

Its been a long time since we've made any kind of changes to the format of Project14 but its due for an upgrade.   Its natural for programs to evolve overtime and things can't stay the same forever. We've experimented with different things with the program and some have been received more enthusiastically than others.   I'm starting this thread to see what kind of changes you would like to see us to make with this program.  What shouldn't be touched,  what would make things more exciting, and how do we grow the program without turning it into something different?  Should it be something different?   Where does Project14 fit in with the larger community?  Before getting this conversation underway, I would like to stress that the goal is to improve not diminish the program.  My managers have been very supportive from the beginning of this program and I want to reward their confidence.   Some of these changes are workload related.  Others are business related.  I'm open to all ideas and suggestions.

 

Topics on the Table:

 

- Launch Themes Every Other Month or Keep them Monthly?

- Shorter Contests or Longer Contests?

- If we have fewer contests Is there Stuff We Can Do In-Between?

- How Can We Make It Easier For More People to Participate?

- Should We have Bigger Prizes?

- Should we have a giveaway before we launch every contest?

- Most Importantly How Do We Make These More Fun?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago +12
    Great work tariq.ahmad . Project14 is a great program that enjoys sufficient participation to keep the monthly project pace lively. If you calculate the time between when the new topic poll looks conclusive…
  • tariq.ahmad
    tariq.ahmad over 5 years ago +10
    Thanks ntewinkel , >> Another option could be an extension or variation to the short evening/weekend projects, making it more of a teaching/learning thing: encouraging others to copy the project for themselves…
  • fmilburn
    fmilburn over 5 years ago +10
    Hi Tariq, I'm glad you are having a look at how to improve the program but I have to say it is already very good. I think monthly is about right. It is probably more work for you but I find all of the…
Parents
  • 14rhb
    14rhb over 5 years ago

    Reading some of the comments made me think of a different style of Project14 that could be mixed in-between the existing ones, perhaps this undertaken only every other month. The idea would be for Element14 to put together a low-cost component bag that all applicants could ask to receive, the contents themselves could be up for discussion each month as we now discuss the theme. However this Project14 would be to make something interesting using 2+ of the items. The low-cost 'surprise bag' of components that sponsors maybe have donated - new product lines in the IC field are always interesting. It would be a bit like the Experimenting with Polymer Capacitors and Experimenting with Inductors challenges but with a much more random approach to the parts. For the fun and again low-cost Element14 could always draw on the bargain components that are already being sold off at reduced rates?

     

    As I thought this through some more I wonder if the parts aren't carefully chosen it could prevent some prospective builders from taking part e.g. inclusion of mainly SMT parts

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to 14rhb

    Maybe the first project could be an introduction to SMD parts with one of those learn to solder SMD boards.   I don’t find larger SMD parts any harder to hand solder than through hole and my eyes and nerves are not so good anymore.   It does require an appropriate tip and finer solder but that is about it.  I even volunteer to design some PCBs, have them fabricated, and send them to Tariq for distribution.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 5 years ago in reply to fmilburn

    That would be a great idea and very generous of you offering to help design boards. Helping develop confidence to build in SMT is a great way for Avnet to make more of their product range available as most 'cool' function ICs are only available in SMT. I've noticed an increasing trend to various BGA formats as well but won't worry about that yet. I've found even QFN are possible with hand-soldering, the trick is to design with enough of the pad visible that solder can be flowed onto and then capillary action takes it under the IC....assuming a nice amount of liquid flux has been added first image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • hugohu
    hugohu over 5 years ago in reply to fmilburn

    I usually can do 0603 comfortably with a SP25(but ya know that iron really sucks so I'm hoping to win the Holiday special so I can get a better iron with the shopping cart)

     

    The first time I soldered SMD passives(not ICs) was with a solder kit, which was noice but then there's also down to 0402.

     

    But yeah, I feel really comfortable after around 2 weeks of practice and assembling those corgis, so...

     

    I actually like SMD better than THT.

     

    Well, not BGA and QFN.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hugohu
    hugohu over 5 years ago in reply to fmilburn

    I usually can do 0603 comfortably with a SP25(but ya know that iron really sucks so I'm hoping to win the Holiday special so I can get a better iron with the shopping cart)

     

    The first time I soldered SMD passives(not ICs) was with a solder kit, which was noice but then there's also down to 0402.

     

    But yeah, I feel really comfortable after around 2 weeks of practice and assembling those corgis, so...

     

    I actually like SMD better than THT.

     

    Well, not BGA and QFN.