Project14
  • Challenges & Projects
  • More
Project14
Forum 12VDC UPS Project
  • News
  • Member Updates
  • Competitions
  • Forum
  • Documents
  • Theme Suggestions
  • Polls
  • Members
  • More
  • Cancel
  • New
Join Project14 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 201 subscribers
  • Views 276 views
  • Users 0 members are here
  • solid state
  • UOS
Related

12VDC UPS Project

Atalantia
Atalantia 3 days ago

Hello People,

I try to outline a 12V UPS for my router. The commercial things I see are either to complicate, means have to much functions or they use a relay. I want to build a solid state switch that is faster than a relay. I have a first sketch. What do you think thats the right direction?

The battery has her own BMS it's not in the circuit here. The comparator is the watchdog who activates the switch in case of a power outage. There are a few diodes to prevent return current. A few resistor to adjust the components margins. R4 is a trimm-pot. Works as a pull-down resistor and adjust the threshold for the comparator.

PS: I know. The input voltage has to be higher than 12V. 

image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett 3 days ago +3
    The comparator and switch are not really doing anything useful. Two diodes will do the business quite easily. Both cathodes to the output, one anode to the 12V DC in and one to the battery. It is…
  • geralds
    geralds 3 days ago in reply to Atalantia +3
    Hi look here, an idea: This is a very simple "UPV". The switching time is not the big problem if you make a buffer (Elko-accu) during toggling the relay. It's just an idea.
  • dang74
    dang74 3 days ago +2
    I think you will need second resistor connected to R1 to form a voltage divider. Otherwise I think your comparator will always select the battery. The comparator should also have a bypass capacitor connected…
Parents
  • michaelkellett
    michaelkellett 3 days ago

    The comparator and switch are not really doing anything useful.

    Two diodes will do the business quite easily.

    Both cathodes to the output, one anode to the 12V DC in and one to the battery.

    It is a good idea to disconnect the battery from the load if its voltage drops too low but your circuit doesn't do that.

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Atalantia
    Atalantia 3 days ago in reply to michaelkellett
    michaelkellett said:
    It is a good idea to disconnect the battery from the load if its voltage drops too low but your circuit doesn't do that.

    The dropout voltage of the battery is managed by the BMS. It's not in the circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 3 days ago in reply to Atalantia

    Hi look here, an idea:

    ups simple

    This is a very simple "UPV".

    The switching time is not the big problem if you make a buffer (Elko-accu) during toggling the relay.

    It's just an idea.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 3 days ago in reply to geralds

    I did near-identical circuit with my home router a few years ago. I just used 8xAA cells (non-rechargeable) since it is very rare here to have outages. I would possibly use Ni-MH if I were to do it again today.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Atalantia
    Atalantia 3 days ago in reply to geralds

    The goal is to do it with a solid state switch. No relay. I'll try to modifier this circuit to a solid state.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx 3 days ago in reply to geralds

    I wonder if putting another diode between battery anode and output wouldn't be beneficial in this case? Than way, big C wouldn't be needed - output would be powered using this additional diode during relay toggle, and in a steady state diode would be shorted by the relay contact, eliminating power loss on diode's voltage drop?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 3 days ago in reply to Atalantia

    Solid-state relays are okay—a perfectly viable option. Solid-state changeover switches are a bit komplexer.

    But please don't forget about the leakage current (return current in µA) inherent to semiconductor switches; the battery will feel that.
    True isolation (via a mechanical contact) would be better; that way, you avoid equalization currents, which are also highly temperature-dependent. Leakage currents drain the battery without providing any benefit.

    Don't be afraid to use a relay.

    The "only" potential issue is:
    the contact sticking shut even after the relay has de-energized; the contact joint can melting, current switch off lightning.
    With a DC relay, the iron core can become permanently magnetized if the relay remains energized by direct current for extended periods.
    One possible solution for monitoring this is to use a second contact with an LED to indicate whether the circuit is closed or open.

    A more complex approach involves applying a short negative pulse to the relay coil upon switch-off to collapse the magnetic field.
    This is achieved using a second winding around the iron core (utilizing back-EMF).

    ->> One more point regarding your circuit:
    Make sure to include deep-discharge protection and a charge cutoff for the battery; otherwise, the battery will eventually be ruined.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Atalantia
    Atalantia 2 days ago in reply to geralds

    OK, now I understand why all the USV I came along have a relay. Maybe I shouldn't reinvent it. Sweat smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds 2 days ago in reply to Atalantia

    I understand you perfectly. I’m a tinkerer too—someone who always wants to improve everything, and I mean *everything*.
    My hammer is always within reach, "pangs!", and I already have new ideas.a bit knowledgeBit by bit, a drop of knowledge...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds 2 days ago in reply to Atalantia

    I understand you perfectly. I’m a tinkerer too—someone who always wants to improve everything, and I mean *everything*.
    My hammer is always within reach, "pangs!", and I already have new ideas.a bit knowledgeBit by bit, a drop of knowledge...