Fighting Germs
  • Challenges & Projects
  • Project14
  • Fighting Germs
  • More
  • Cancel
Fighting Germs
Blog 5% Chlorine solution disinfectant station
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Fighting Germs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: cypresstwist
  • Date Created: 22 Mar 2020 7:24 PM Date Created
  • Views 1600 views
  • Likes 7 likes
  • Comments 2 comments
  • fightinggermsch
  • covid-19
  • water pump
  • motor
  • chlorine
Related
Recommended

5% Chlorine solution disinfectant station

cypresstwist
cypresstwist
22 Mar 2020
image

Fighting Germs

Enter Your Electronics & Design Project for a chance to win an $200 Shopping cart of product!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

So I came up with this idea to build something that would allow me to disinfect my shoes and my electric scooter before entering my apartment. I am building a chlorine pump that has a pot for liquid flow. A 5 liter 5% chlorine solution inside has a tube in it with a 5V water pump and an on/off switch. The tube goes outside through a hole above the door entrance and down the wall to the front door where a box with an on/off potentiometer and a deep tray allows you to wash non-organic stuff with disinfectant.It has an ESP32-CAM webcam inside that allows me to watch what the person outside is doing.


A 10cm by 6cm plastic enclosure holds a motor speed regulator that regulates the flow. A flexible plastic tube goes in.

image

A plastic tray outside, under the black box, gathers the solution that pours through the tube.

image

This wooden stand will be mounted on the wall and give the plastic tray a place to sit in at hand level.

image

image

The black box lid is mounted on the outside wall with screws.

image

Thin electric cables for the motor speed regulator run along the plastic tube.

image

Motor speed regulator, pot knob, enclosures, water pump and switch.

image

Tubing goes outside through the wall.

image

Trying to fit the ESP32 CAM in the box along with a step-down converter and the motor speed regulator:

image

Day two: I dont want to stay outside more than I need to but I've managed to install everythin needed outside my door and make the wire connections. Had to drop the WiFi cam because I already have a webcam pointed in that direction and the ESP32-CAM I had would not fit in the plastic box alongside the volume calibrator.


This simple On/Off switch will power the circuit from the inside:

image

image

I've installed everything needed outside my door in my appartment building. If the switch inside powers the circuit then the yellow pot can act as a secondry switch allowing to complete the circuit once activated then it will slowly more and more liquid into the tray until turned off. The more you turn the knob, the faster the water pump will pump liquid up the tube from a 5 liter plastic bottle. I need to put a brush in front of the tray. The tray can be taken down and put on the floor to better scrub shoes and the wheels of my electric scooter.

image

image

image

Day #3: I don't go out much so working on the outside-the-door part of the project depends on the times I am forced to dress up and go buy food and whatnot. It then takes a while to carefully take my surgical gloves off, discard of them properly, disinfect my hands and face, take down my FFP2 N95 mask and disinfect that too, place my clothes in a safe place then wash my hands and face again for about two minutes. It's like a ritual. But on the inside part of the project I used two screws to fit the inner control box on the wall and glued the edges so it won't move. Will have to do that for the outside box too these days. There's a 5 liter 5% Chlorine solution beneath it and the 5V water pump is inside.

image

If you're wondering what's with the thick white line - that's where the thin power cables go. They're underneath it. So I won't have to drag them across the top part of the walls.

image

Power is delivered via a 12V to 5V and 3.3V converter that also has an On/Off switch. I've used hot glue to secure the contacts in it.

image

Will test it tomorrow if I have to go out.

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +3
    Looks like a useful comcept. Dubbie
  • 14rhb
    14rhb over 6 years ago +2
    This is great work - even the door frame has been drilled. Look forward to seeing it in action.
Parents
  • dubbie
    dubbie over 6 years ago

    Looks like a useful comcept.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    Looks like a useful comcept.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down