Fighting Germs
  • Challenges & Projects
  • Project14
  • Fighting Germs
  • More
  • Cancel
Fighting Germs
Blog Boston Dynamics' Spot robot being used on the frontline in hospitals
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Fighting Germs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 30 Apr 2020 8:07 PM Date Created
  • Views 1835 views
  • Likes 6 likes
  • Comments 3 comments
  • hmi
  • fightinggermsch
  • robotics
  • robot
  • cabeatwell
  • covid 19
Related
Recommended

Boston Dynamics' Spot robot being used on the frontline in hospitals

Catwell
Catwell
30 Apr 2020
image

Fighting Germs

Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

It’s during times like these that inspire innovation. Like robots in the medical field, like this post.

 

In that spirit, the “Fighting Germs” contest is here to not only reward that innovation ─ but also give to other charities for those attempting the same thing! It’s fun, it’s beneficial.

 

They say the best time to plant a tree is thirty years ago. The next best time is today.

 

 

image

Spot allows healthcare workers to communicate with infected patients from a safe distance using an iPad and two-way radio. (Image Credit: Boston Dynamics) 

 

Boston Dynamics is well-known for its four-legged Spot robot, which is capable of performing a variety of tasks, but now they're being put on the frontline to keep healthcare workers safe from the COVID-19 crisis. On April 23rd, Boston Dynamics announced its Spot robots are being used at Brigham and Women's Hospital in Boston, Massachusetts, where they allow healthcare workers to remotely triage patients. The company hopes its open-source tech will be implemented on other mobile robotic platforms around the world.

 

Boston Dynamics' Spot robot is equipped with an iPad, and a two-way radio mounted on its back, which will allow healthcare providers to video call with infected patients as the workers remotely guide the robot through tents. This setup enables doctors to communicate with the patients from a safer area, and possibly in their own homes. For each intake shift completed by a teleoperated robot, at least one healthcare worker can reduce their risk of contracting the virus while preserving the limited supply of protective equipment.

 

In order to provide additional services to healthcare workers, the company stated that Spot still needs to collect vital sign information from infected patients. This includes body temperature, respiratory rate, pulse rate, and oxygen saturation. Boston Dynamics has also been in contact with researchers who use thermal camera technology to calculate respiratory rate and measure body temperature. Additionally, the company has also applied externally developed logic to externally mounted RGB cameras, which can capture blood-vessel contraction changes to measure pulse rate.  They are also testing different methods to measure oxygen saturation.

 

Boston Dynamics hopes to attach a UV-C light or other similar technology to Spot's back, which could kill particles of the virus and disinfect surfaces in spaces that require decontamination like hospital tens or metro stations. A number of mobile robot providers have already developed this tech specifically for hospitals.

 

Even though the Spot robot is being used at Brigham and Women's Hospital, Boston Dynamics also says the software and hardware technology is better suited for tracked or wheeled robots. The company hopes that other mobile robotic platform will use this system to help keep healthcare workers safe. It's also discussing plans with Clearpath, a Canadian firm, to help make the technology available to others.

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • ankur608
    ankur608 over 6 years ago +1
    Great.
  • dubbie
    dubbie over 6 years ago +1
    Well done Spot! Dubbie
  • robogary
    robogary over 6 years ago +1
    Wow ! Open Source !!!!!! I got way over excited, closed my eyes, repeated my wish over and over, while clicking together my ruby slippers. (I wish for a Spot chassis.) The open source files are for spot…
  • robogary
    robogary over 6 years ago

    Wow !  Open Source !!!!!!

    I got way over excited, closed my eyes, repeated my wish over and over, while clicking together my ruby slippers. (I wish for a Spot chassis.)

    The open source files are for spot's medicinal electronic backpack - really really cool, however, the user still needs Spot's Boston Dynamic's robot chassis to build one.

     

    I was hoping the 3D models included Spot's robot chassis - to print a smaller version for demo and teaching classes by my robot club.

    A Spot replicant would be so cool to demo at community STEM exhibits, teaching coding classes at the library using a real life model, take to schools,  robot celebrations, raspberry pi jams, arduino day, etc...

    The Boston Dynamics chassis design is unique and very recognizable.

     

    Catwell - if you know of someone at Boston Dynamics that needs to get rid of a free service unit Spot chassis, please send them my way :-) 

    Or if Spot's chassis is available for open source 3D printing, ........there would be alot of creative people making an army of Spot's with all kinds of Arduino & Raspberry Pi applications on them.

    Can you envision a Spot looking and sniffing the yard for dog poo pickup ?  Searching a garden for weeds and pests ? A robot watchdog ? or walking a human ? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    Well done Spot!

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ankur608
    ankur608 over 6 years ago

    Great.