Fighting Germs
  • Challenges & Projects
  • Project14
  • Fighting Germs
  • More
  • Cancel
Fighting Germs
Blog Neopixel LED Face Mask Lights Up in Any Pattern You Can Program
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Fighting Germs to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 28 Jul 2020 6:09 PM Date Created
  • Views 1853 views
  • Likes 4 likes
  • Comments 3 comments
  • fighting germs
  • diy
  • cabeatwell
  • covid 19
  • face mask
  • innovation
  • fun
Related
Recommended

Neopixel LED Face Mask Lights Up in Any Pattern You Can Program

Catwell
Catwell
28 Jul 2020

image

NeoPixel based face mask. (Image credit: splat238)

 

I think we all thought about this, in some way or another. Good ideas versus great boils down to actually making it happen.

 

What is a design project you’ll get more use out of these days than a face mask? A user on instructables.com has posted detailed instructions for your own DIY LED face mask, which both animates with randomly chosen color and manages to act as any other cloth mask—keeping you and others safe. The project uses an airsoft mesh half mask as the base and WS2812b LEDs, or Neopixels, which allow the user to create almost any effect they can imagine, with the right coding.

 

The project does require some SMD soldering and access to a 3D printer but is otherwise designed to be quick and inexpensive. The instructions even offer two build options: either using a single Wemos LiPo Button Combo board and the other with two different PCBs, a Wemos LiPo Charger Combo board and a Triple Flat tactile button board. The recommended controller for the LEDs is the esp8266, which features more memory and processing speed than most common Arduino boards.

 

The actual construction of the mask is essentially done in a few separate steps—attaching LED strips to the interior of the mask, assembling the controller, securing the control box, wires, and mask straps, and uploading code. All of the steps are outlined in detail, with images, by the designer, who has also uploaded code for 40 different effects. The control box and a few elements used to secure wires within the mask are 3D printed, although the part files are also freely available. The control box itself uses three buttons. When using the provided code, these are used to cycle to the next effect, turn effect rotation on/off, so when off an effect will repeat indefinitely, and to adjust brightness.

 

Both the single- and double-PCB options are posted along with the parts needed for each, although it is noted that single-PCB was a more stable design. It’s also important to know that the power source is an external LiPo battery, which can be dangerous if mistreated. Once the mask is fully assembled, it will cover both nose and mouth and should serve to trap moisture as well as any cloth mask, though you may want to wear a more standard mask for the sake of safety. The LEDs are not particularly visible in direct sunlight but are definitely a fun flare when in the shade or indoors.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Have a story tip? Message me at: cabe(at)element14(dot)com

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • tatoted
    tatoted over 6 years ago +1
    Have you tried experimenting with voice recognition? It would be really cool if it lit up according to how you spoke
Parents
  • tatoted
    tatoted over 6 years ago

    Have you tried experimenting with voice recognition? It would be really cool if it lit up according to how you spoke

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 6 years ago in reply to tatoted

    Rad idea, Teddy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 6 years ago in reply to tatoted

    Rad idea, Teddy.