Fun & Games
  • Challenges & Projects
  • Project14
  • Fun & Games
  • More
  • Cancel
Fun & Games
Forum P-Channel MOSFET High-Side Switch Not Fully Turning Off (ESP32 rail at 2.9V)
  • News
  • Projects
  • Forum
  • Leaderboard
  • More
  • Cancel
  • New
Join Fun & Games to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 50 subscribers
  • Views 1208 views
  • Users 0 members are here
Related

P-Channel MOSFET High-Side Switch Not Fully Turning Off (ESP32 rail at 2.9V)

arvindsa
arvindsa 8 months ago

I’m using a DMP2045U P-channel MOSFET as a high-side switch to control 3.3V power to an ESP32-S3-WROOM module. The gate is driven by an STM32.

image

Connections

  • Source → 3.3V (measured 3.289V)

  • Drain → ESP32 3V3 pin

  • Gate → STM32 GPIO

  • 10k pull-up from gate to 3.3V

Measurements

When gate is LOW (~0.009V):

  • Source = 3.289V

  • Gate = 0.009V

  • Drain = 3.289V

  • Vgs ≈ −3.28V → MOSFET turns fully ON (as expected)

When gate is HIGH (3.287V):

  • Source = 3.289V

  • Gate = 3.287V

  • Vgs ≈ 0V → MOSFET should be OFF

However:

  • Drain measures ~2.89V

I added a 47k pulldown resistor from drain to GND. This reduced the drain voltage to ~2.4V — but not to 0V.

  • All STM32 GPIOs connected to the ESP32 are driven LOW.

  • If I completely remove the MOSFET, the ESP32 3V3 rail stays at 0V (no floating voltage).

Question

Is this expected off-state leakage/floating behavior for a discrete P-MOSFET in this configuration, or is there something wrong with my circuit?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps 8 months ago +1
    Is it possible you have active signals on the digital lines when the ESP32 is off, that seep to the power rail?
  • michaelkellett
    michaelkellett 8 months ago +1
    You have about 50uA leakage through the MOSFET when it's supposed to be turned off - the spec says it should be less than 1uA. Try shorting the MOSFET gate to source (I know its already meant to be at…
Parents
  • michaelkellett
    0 michaelkellett 8 months ago

    You have about 50uA leakage through the MOSFET  when it's supposed to be turned off - the spec says it should be less than 1uA.

    Try shorting the MOSFET gate to source (I know its already meant to be at the same voltage but maybe that only happens when your meter is there - I have seen that before.)

    Then check that it really is turning off.

    Also try a restive load rather than the ESP32.

    I have seen a batch of MOSFETs that were a lot leakier than spec - so it could just be that.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett 8 months ago

    You have about 50uA leakage through the MOSFET  when it's supposed to be turned off - the spec says it should be less than 1uA.

    Try shorting the MOSFET gate to source (I know its already meant to be at the same voltage but maybe that only happens when your meter is there - I have seen that before.)

    Then check that it really is turning off.

    Also try a restive load rather than the ESP32.

    I have seen a batch of MOSFETs that were a lot leakier than spec - so it could just be that.

    MK