Geeky Gadgets
  • Challenges & Projects
  • Project14
  • Geeky Gadgets
  • More
  • Cancel
Geeky Gadgets
Blog Geeky Dalek Project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Geeky Gadgets to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lahey
  • Date Created: 19 May 2017 6:23 AM Date Created
  • Views 2461 views
  • Likes 4 likes
  • Comments 12 comments
  • ggadgetsch
Related
Recommended

Geeky Dalek Project

lahey
lahey
19 May 2017

My geeky idea is a Dalek with object recognition and different behaviors based on what it sees. I have recently acquired two 12'' rc daleks, one functioning and one for spares, and the motor section is actually well built. I will use a RPI3 for the image recognition and an Arduino for the movement and obstacle avoidance, so as not to encumber the RPI too much. Trying to find a viable way to turn an optical mouse into an odometer for motion tracking. Any tips VERY welcome.

 

image

  • Sign in to reply

Top Comments

  • lahey
    lahey over 9 years ago in reply to balearicdynamics +3
    Ciao Enrico, The imaging and object recognition will already use up a lot of processor time for the PI, and the camera and head servos will drain a lot of power. I decided to set up an Arduino so it will…
  • lahey
    lahey over 9 years ago +3
    Update: The motor section is taking shape, what's missing is a gyro to calculate rotation and probably a mouse optical sensor to calculate movement. I hope I have enough pins on the Arduino for all these…
  • lahey
    lahey over 9 years ago in reply to DAB +2
    Hi DAB, yes, the speaker is already in place and I have a whole range of phrases the Dalek will say, based on what it "sees" i have managed to get to get my hands on a couple of these sensors. Thy basically…
Parents
  • barsznica
    barsznica over 9 years ago

    You could use a PCA9685 to increase your outputs.

    Works with Arduino and Pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lahey
    lahey over 9 years ago in reply to barsznica

    I think I need more inputs than outputs. But that PCA board is wicked, daaaaamn!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • lahey
    lahey over 9 years ago in reply to barsznica

    I think I need more inputs than outputs. But that PCA board is wicked, daaaaamn!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • barsznica
    barsznica over 9 years ago in reply to lahey

    You would get the 5 GPIOs, you are currently using as outputs, back as inputs.

    Apparently, the USonic detector can be interfaced with 1 GPIO (trigger AND echo/output).

     

    A heap of IIC (I2C) sensors can be put on the IIC BUS (128, I think) using 2 wire data.

    SPI could also be used for higher speed, but requires 1 GPIO per sensor to "address"/enable it.

     

    Check out a 9DOF IMU.