Geeky Gadgets
  • Challenges & Projects
  • Project14
  • Geeky Gadgets
  • More
  • Cancel
Geeky Gadgets
Blog Geeky Dalek Project
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Geeky Gadgets to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: lahey
  • Date Created: 19 May 2017 6:23 AM Date Created
  • Views 2457 views
  • Likes 4 likes
  • Comments 12 comments
  • ggadgetsch
Related
Recommended

Geeky Dalek Project

lahey
lahey
19 May 2017

My geeky idea is a Dalek with object recognition and different behaviors based on what it sees. I have recently acquired two 12'' rc daleks, one functioning and one for spares, and the motor section is actually well built. I will use a RPI3 for the image recognition and an Arduino for the movement and obstacle avoidance, so as not to encumber the RPI too much. Trying to find a viable way to turn an optical mouse into an odometer for motion tracking. Any tips VERY welcome.

 

image

  • Sign in to reply

Top Comments

  • lahey
    lahey over 9 years ago in reply to balearicdynamics +3
    Ciao Enrico, The imaging and object recognition will already use up a lot of processor time for the PI, and the camera and head servos will drain a lot of power. I decided to set up an Arduino so it will…
  • lahey
    lahey over 9 years ago +3
    Update: The motor section is taking shape, what's missing is a gyro to calculate rotation and probably a mouse optical sensor to calculate movement. I hope I have enough pins on the Arduino for all these…
  • lahey
    lahey over 9 years ago in reply to DAB +2
    Hi DAB, yes, the speaker is already in place and I have a whole range of phrases the Dalek will say, based on what it "sees" i have managed to get to get my hands on a couple of these sensors. Thy basically…
  • barsznica
    barsznica over 9 years ago in reply to lahey

    You would get the 5 GPIOs, you are currently using as outputs, back as inputs.

    Apparently, the USonic detector can be interfaced with 1 GPIO (trigger AND echo/output).

     

    A heap of IIC (I2C) sensors can be put on the IIC BUS (128, I think) using 2 wire data.

    SPI could also be used for higher speed, but requires 1 GPIO per sensor to "address"/enable it.

     

    Check out a 9DOF IMU.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lahey
    lahey over 9 years ago in reply to barsznica

    I think I need more inputs than outputs. But that PCA board is wicked, daaaaamn!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • barsznica
    barsznica over 9 years ago

    You could use a PCA9685 to increase your outputs.

    Works with Arduino and Pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lahey
    lahey over 9 years ago

    Update:

     

    The motor section is taking shape, what's missing is a gyro to calculate rotation and probably a mouse optical sensor to calculate movement. I hope I have enough pins on the Arduino for all these sensors.

     

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lahey
    lahey over 9 years ago

    UPDATE

     

    found a pretty good path planning library on github: https://github.com/elben/kapal and planning to implement it as follows:

    arduino does the basic muscle work, moves and returns position and visible obstacles (ultrasound)

    raspberry gradually builds a map of the area and tells arduino where to move. In case of unforseen obstacles the movement stops and the map is updated.

     

    only problem is the code is poorly maintained & commented and hard to understand how to parse the final path list.

     

    onwards!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>