Hardware Hacking
  • Challenges & Projects
  • Project14
  • Hardware Hacking
  • More
  • Cancel
Hardware Hacking
Blog My Pulse Generator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hardware Hacking to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 9 Jun 2020 1:40 PM Date Created
  • Views 3859 views
  • Likes 13 likes
  • Comments 19 comments
  • pulse generator
  • hardwarehackingch
Related
Recommended

My Pulse Generator

dubbie
dubbie
9 Jun 2020
image

Hardware Hacking

Enter Your Electronics & Design Project for a chance to win a $200 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

Technically this is not a Hack as I haven't done anything to it but it is a bit of reverse engineering and although it is not bus sniffing, I did do a bit of sniffing with my nose. I was inspired by Ralph Yamamoto's Blog on his old Pong game (Pong is Alive ) to dig out an old pulse generator I made, probably over forty years ago.

 

image

 

The construction is much better than I ever remember doing, I must have been training to be an engineer or something, before I gave it all up to become a lecturer. The top and bottom are laminated chip board and the sides are repurposed aluminium sheet. I recognise the plastic coating of the sides from my days at GEC Telecommunications in Coventry when I was on placement, they had skips of old stuff they no longer wanted and you were free to take whatever you wanted. The front is brushed aluminium with Lettraset lettering covered with a plastic film I think.

 

In the video below is a look inside and quick overview of the integrated circuits used.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I'm not particularly attached to this pulse generator so rather than testing it step by step to see if it working I decided to just powered it up and see what is what. If it blows up it blows up.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Surprisingly it still seemed to work so the next step was to see what outputs were still being generated.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

All the outputs still seem to work as desired, albeit with some strange voltages at times. Amazing! After 40 years sitting in cupboards and being moved from house to house, it is still in one piece and still works as it did when I first constructed it. 

 

Still, life moves on. I do not have any sentimental attachments to this pulse generator as I just do not remember making it and I'm not going to use it as it isn't safe and it is very heavy. Plus I am currently in a phase on de-cluttering so this is likely to end up on the rubbish heap somewhere in the not too distant future. I do not want any of these old ICs so I will not keep them. I might keep the 4 mm sockets and maybe the mains plug but that is probably all. If I ever need a pulse generator in the future which does seem unlikely, I will either make one from an Arduino or buy one ready made.

 

Dubbie

  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 6 years ago +7
    Consigned to the rubbish heap! I thought you would put some wheels on it and turn it into a robot that comes scooting across your desk when you declare that you needed a pulse generating. Kind regards
  • beacon_dave
    beacon_dave over 6 years ago in reply to three-phase +5
    Are we talking about some sort of autonomous defibrillator device here ?
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to beacon_dave +4
    beacon_dave wrote: "...No need to change a great design..." One significant improvement Antex made was when they changed the bit design from bifurcated bit plus external spring to a solid bit plus internal…
  • beacon_dave
    beacon_dave over 6 years ago in reply to Jan Cumps

    Yes, could well be the case. I seem to recall it was more of a problem with the smaller 12W irons, so perhaps the narrower diameter element shaft didn't help. Or it may be that originally they shared the 15W bits with the 12W iron and were relying upon the spring to accommodate any difference in element diameters.

     

    I still have an old XS25 iron which was very reliable ( but with the new style bits ) but also now have  the TCS50 model.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to beacon_dave

    beacon_dave  wrote:

     

    "...No need to change a great design..."

    One significant improvement Antex made was when they changed the bit design from bifurcated bit plus external spring to a solid bit plus internal spring. Especially on the older 12W rated irons, they had an annoying tendency to slide off in use when hot.

     

    Mine has the old design. I haven't had the slip-off issue. Maybe because it's still the original tip and has never been removed (it's the 25W model)?

    image

     

    I still use this one when working on older designs that use leaded solder. For lead-free work, the temperture is too low.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to dubbie

    "...No need to change a great design..."

    One significant improvement Antex made was when they changed the bit design from bifurcated bit plus external spring to a solid bit plus internal spring. Especially on the older 12W rated irons, they had an annoying tendency to slide off in use when hot.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to Jan Cumps

    They are distinctive. No need to change a great design.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to dubbie

    Mine from 83 or 84: Antex 25. I thought I recognised it in the video image

    image

    also still in good working order.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>