• Products and Partners
    Products and Partners
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
Hardware Hacking
  • Challenges & Projects
  • Project14
  • Hardware Hacking
  • More
  • Cancel
Hardware Hacking
Blog Pong Game Circa 1978
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hardware Hacking to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 25 May 2020 11:46 PM Date Created
  • Views 2165 views
  • Likes 8 likes
  • Comments 2 comments
  • ay-3-8500-1
  • pong on a chip
  • hardwarehackingch
Related
Recommended

Pong Game Circa 1978

ralphjy
ralphjy
25 May 2020

Sometime in a world long long ago I built a Pong game using a General Instruments AY-3-8500-1 IC (the -1 is for NTSC).

 

I found the unit in one of my junk boxes.  It has survived 3 moves and an earthquake (Northridge 1994).  It was in okay condition considering.  I'm not sure why the case was not screwed together and looks like some components might have been cannibalized and it is missing a controller.  It really looks like something that I would have built 42 years ago image.   If I have time next month I might try to get this to work again as a Hardware Hacking Project.

 

You can see that the homemade paddle controller just used a potentiometer mounted in a used 35mm film canister.  It's odd that there is only one remaining.

image

 

It looks like I used a mix of soldering and wirewrap.  Very messy construction.  I have no idea why there are two 9V battery clips.

image

 

Looks worse from the side but it actually looks like I used a crystal to set the frequency.

image

 

I don't have a schematic and I can't remember if this was still working (not a good sign that the case was open).  But the circuit looks simple enough (due to the IC) and it looks like I didn't use a modulator but drove a composite monitor directly and it also is only monochrome.  I'll probably check to see if the IC appears to be alive and if so it will probably be easiest to rebuild everything from scratch (just can't tell my wife I'm doing it).

 

I did find the AY-3-8500 schematic on the web.  Wouldn't be possible to try this without it.  It does have multiple games and I did put in a multipole switch for selection.

image

image

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 6 years ago +2
    That looks like fun :-) I hope you do get it to work.
  • dubbie
    dubbie over 6 years ago +2
    I remember that circuit for using logic gates to create a crystal oscillator. I can also remember playing Pong on a TV although it cannot have been mine as I never owned one, perhaps it was in a pub. …
Parents
  • fmilburn
    fmilburn over 6 years ago

    That looks like fun :-)  I hope you do get it to work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 6 years ago

    That looks like fun :-)  I hope you do get it to work.