IoT: In the Cloud
  • Challenges & Projects
  • Project14
  • IoT: In the Cloud
  • More
  • Cancel
IoT: In the Cloud
Blog Arduino IoT in the Cloud - Door Alarm
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join IoT: In the Cloud to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsc
  • Date Created: 22 Mar 2019 2:45 PM Date Created
  • Views 2381 views
  • Likes 9 likes
  • Comments 2 comments
  • mkr_1010
  • arduino iot cloud
  • p14 mkr 1010
  • arduino_iot_cloud
  • iotcloudch
  • arduino day 2019
  • arduino mkr1010
Related
Recommended

Arduino IoT in the Cloud - Door Alarm

rsc
rsc
22 Mar 2019
image

IoT: In the Cloud

Enter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I've installed a few of those inexpensive magnetic door and window alarms around the house, but they only make noise, they are not connected.

For this project, I tap into one of the door alarms and send the door status to the cloud.

We start with this:

image

Take it apart:

image

Solder to the V+, Gnd, and trigger input from the reed switch.

image

Then set up the Cloud service.

image

I set up a Thing called "FrontDoorSensor" on the Arduino IoT Cloud Service.

image

Then I set up a parameter called "DoorOpen"

image

image

Code for the Thing:

#include <ArduinoIoTCloud.h>
#include <WiFiConnectionManager.h>


const char THING_ID[] = "asdfjkl-ggfgfgf-200230";


const char SSID[]     = SECRET_SSID;    // Network SSID (name)
const char PASS[]     = SECRET_PASS;    // Network (for WPA, or use as key for WEP)




bool DoorOpen;


void initProperties(){
  ArduinoCloud.setThingId(THING_ID);
  ArduinoCloud.addProperty(DoorOpen, READ, ON_CHANGE, NULL);
}


ConnectionManager *ArduinoIoTPreferredConnection = new WiFiConnectionManager(SSID, PASS);

Main Code:

/* 
  Sketch generated by the Arduino IoT Cloud Thing "FrontDoorSensor"
  https://create.arduino.cc/cloud/things/----


  Arduino IoT Cloud Properties description


  The following variables are automatically generated and updated when changes are made to the Thing properties


  bool DoorOpen;


  Properties which are marked as READ/WRITE in the Cloud Thing will also have functions
  which are called when their values are changed from the Dashboard.
  These functions are generated with the Thing and added at the end of this sketch.
*/


#include "thingProperties.h"


int keyIndex = 0;                 // your network key Index number (needed only for WEP)
int inPin = 6;


void setup() {
  // Initialize serial and wait for port to open:
  Serial.begin(9600);


  pinMode(inPin, INPUT);      // sets the digital pin 6 as input




  // Defined in thingProperties.h
  initProperties();


  // Connect to Arduino IoT Cloud
  ArduinoCloud.begin(ArduinoIoTPreferredConnection);
  
  /*
     The following function allows you to obtain more information
     related to the state of network and IoT Cloud connection and errors
     the higher number the more granular information you’ll get.
     The default is 0 (only errors).
     Maximum is 4
 */
  setDebugMessageLevel(2);
  ArduinoCloud.printDebugInfo();
}


void loop() {
  DoorOpen = digitalRead(inPin);   // read the input pin
  ArduinoCloud.update();
}

 

Next I will add a motion sensor, and have the program email me a message on triggered event.

Scott

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +1
    Nice update. DAB
Parents
  • DAB
    DAB over 7 years ago

    Nice update.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 7 years ago

    Nice update.

     

    DAB