IoT: In the Cloud
  • Challenges & Projects
  • Project14
  • IoT: In the Cloud
  • More
  • Cancel
IoT: In the Cloud
Blog Home Automation Using Raspberry Pi Matrix Voice and Snips
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join IoT: In the Cloud to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ruchir1674
  • Date Created: 24 Mar 2019 10:32 AM Date Created
  • Views 5652 views
  • Likes 13 likes
  • Comments 27 comments
  • matrix labs
  • iotcloudch
  • rpiexpert
  • snips
Related
Recommended

Home Automation Using Raspberry Pi Matrix Voice and Snips

ruchir1674
ruchir1674
24 Mar 2019
image

IoT: In the Cloud

Enter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Updated on 8 May 2019

image

Introduction

Home automation allows us to control household electrical appliances like light, door, fan, and so on. Home automation not only refers to reduce human efforts but also energy efficiency and time saving.

The aim of the project is to implement home automation using Raspberry Pi, Matrix Voice and Snips platform. In this project, Raspberry Pi is connected with Matrix Voice via GPIO pins and all the five lights (such as bedroom, kitchen lights) which we are controlling through voice command are interfaced with expansion GPIO pins of Matrix Voice. We are providing input(voice command) through Matrix voice mic and taking output (response) as light on/off from GPIO of Matrix Voice.

 

Component Needed

1. Matrix Voice ==> $55

image

2. Raspberry Pi 3 B+ ==> $35

image

3. 5V 2.5A Power Supply Adapter ==> $4.78

 

image

 

4. 5V Relay single channel ==> $4

image

5.16 GB SD card ==> $7.68

image

Total cost of the project is around $ 106

 

How to Connect Matrix Voice With RPi 3

The Matrix Voice is a development board for building sound driven behaviors and interfaces. It is an user-friendly tool for simple to complex Internet of Things (IoT) voice app creation. It comes under two versions

1. Matrix Voice version

2. Matrix Voice ESP32 version

Both versions of these boards run the same on a Raspberry Pi, however, the Matrix Voice ESP32 version has the option to run standalone by programming the ESP32 module.

Here I am using Matrix Voice.

 

       imageimage

 

Matrix Voice expansion GPIO

 

DF## pins are equivalent to GPIO## pins.

   imageimage

 

Raspberry Pi GPIO

 

image  image

Note:- The expansion GPIOs on the Matrix Voice are not connected to the RPi GPIOs. The expansion GPIOs mostly come from the FPGA.

 

Before installing Matrix OS make sure you have setup Matrix voice. For that you need

  • Raspberry Pi 3 Model B
  • +5V 2.5A Micro USB Power Supply
  • Matrix voice

1. Insert flashed micro SD card into Raspberry Pi

2. Attach Matrix Voice onto Raspberry Pi GPIO pins

3. Power Raspberry Pi with micro USB power supply

Once done next is installing Matrix OS on your personal computer. You can use Windows or macOS or Linux. In this project I am going to use Linux (Ubuntu) to install Matrix OS

 

Matrix core installation on RPi

 

Before starting installing make sure you have installed NodeJS and npm

1. To install NodeJS, go to NodeJS and download Linux binaries(x64) of version 10.15.1

image

and then extract it with

tar -xvf node-v10.15.1-linux-x64.tar.xz 
cd node-v10.15.1-linux-x64
sudo cp -R * /usr/local/
sudo apt-get update
sudo apt-get upgrade

and check NodeJS and npm version

node -v 
npm -v

 

1. Add the Matrix repository and key.

curl https://apt.matrix.one/doc/apt-key.gpg | sudo apt-key add - 
echo "deb https://apt.matrix.one/raspbian $(lsb_release -sc) main" | sudo tee /etc/apt/sources.list.d/matrixlabs.list

Matrix repository for Matrix HAL

curl https://apt.matrix.one/doc/apt-key.gpg | sudo apt-key add -
echo "deb https://apt.matrix.one/raspbian $(lsb_release -sc) main" | sudo tee /etc/apt/sources.list.d/matrixlabs.list

Update your repository and packages.

sudo apt-get update 
sudo apt-get upgrade

 

2. Install the the Matrix Core packages.
sudo apt-get install matrixio-malos 

image

 

sudo reboot

 

Install the the MATRIX HAL packages.

sudo apt-get install matrixio-creator-init libmatrixio-creator-hal libmatrixio-creator-hal-dev 

Reboot your device.

sudo reboot 

 

3. To install ZeroMQ

echo "deb http://download.opensuse.org/repositories/network:/messaging:/zeromq:/release-stable/Debian_9.0/ ./" | sudo tee /etc/apt/sources.list.d/zeromq.list

wget https://download.opensuse.org/repositories/network:/messaging:/zeromq:/release-stable/Debian_9.0/Release.key -O- | sudo apt-key add

 

4. JavaScript setup

 

Create a node project folder in the home directory of RPi

cd ~/ mkdir js-matrix-core-app (whatever name you want) 
cd js-matrix-core-app
npm init

 

5. Installing npm Packages for ZMQ and Protocol Buffers

 

To install the ZMQ and MATRIX Protocol Buffers npm packages. Make sure you are in directory which you created above (name you give). Here I gave it js-matrix-core-app. This allows you to interact with Matrix Core through Node.js.

npm install zeromq --save
npm install matrix-protos --save

image

 

image

 

To use PWM for external LEDs and servo motor I am using Matrix lite library.

npm install @matrix-io/matrix-lite --save

 

Now you are done with Matrix core and Matrix HAL.

 

What is snips

Snips is an AI voice platform for connected devices. It is an end-to-end solution with Speech Recognition and Natural Language Understanding, enabling anyone to add a customizable voice assistant to their product. Snips is the only deep-learning based voice platform that runs fully on-device. It can run without the need for a server or the cloud. It offers Privacy by Design.

How to install the Snips using SAM CLI tool

For this make sure all the steps mentioned above are working

I. Raspberry Pi

1. To Install the matrix Kernel Modules. Run the following commands in your Raspberry Pi's terminal to add the matrix repository & key and update your repository packages.

 

curl https://apt.matrix.one/doc/apt-key.gpg | sudo apt-key add -
echo "deb https://apt.matrix.one/raspbian $(lsb_release -sc) main" | sudo tee /etc/apt/sources.list.d/matrixlabs.list
sudo apt-get update
sudo apt-get upgrade
sudo reboot

 

2. To Install the Matrix Kernel modules. Use the command below

sudo apt install matrixio-kernel-modules 

  imageimage

 

This allows the microphones on your matrix device to register as an ALSA microphone on your Raspberry Pi.

sudo reboot 

3. Next command will test your microphones by raising your output volume, creating a 5 second long audio recording, and then playing that recording.

Make sure you have select audio jack as output for that

sudo raspi-config 

then blue screen appears, go to advanced option then go to audio and select analog jack.

 

imageimage

image

 

 

amixer set PCM 100% && arecord recording.wav -f S16_LE -r 16000 -d 5 && aplay recording.wav

 

image

 

If you are able to hear the audio then you are done.

Next we are going to install the SAM tool on desktop

 

II.Installing the SAM CLI tool on personal computer(Ubuntu)

 

We are using the SAM CLI tool to create, manage and deploy our Snips assistants, to configure hardware, to view the logs of assistants on the Raspberry Pi, as well as to run your application locally for quick prototyping.

1. Install SAM into your computer with the following command.

sudo npm install -g snips-sam 

2. Installing Snips.ai through SAM

We are going to install Snips.ai on our Raspberry Pi, Snips will be installed through the SAM CLI tool from our personal computer.

sam devices 

This command should log all of the Raspberry Pis on your network with their IP address and host name.

Note:- sam devices not required if you already know your RPi IP address

Connect to your Raspberry Pi using command

sam connect ip address of Pi 

eg :- sam connect 192.168.1.68

you'll then be prompted to insert a username and password of RPi.

 

image

Once you connected use the sudo init command, from your personal computer, to install Snips onto your Raspberry Pi.

sudo sam init 

image

 

III. Configuring Snips.ai on Raspberry Pi

 

Now, edit the snips.toml file for configuring the mics on RPi.

Open terminal and use command to open the snips.toml file

sudo nano /etc/snips.toml 

You can use any editor to do changes.

Scroll down to where you see [snips-audio-server] and replace

# mike = "Built-in Microphone" 
with the following:
mike = "MATRIXIO SOUND: - (hw:2,0)"

image

IV.Testing Snips.ai on personal Computer(Ubuntu)

 

Through your personal computer's terminal, you can use SAM to test the speaker and microphone of your Raspberry Pi.

 

1. To Test Raspberry Pi's speaker

sam test speaker 

image

 

2. To Test the microphones on your Matrix device

sam test microphone 

image

 

If both commands seem to work, you've properly configured Snips.ai on your Raspberry Pi.

If there is some problem use this command

sam setup audio 

Then it will ask whether you are using snips kit or not (I choose no)

Then it will ask you to select the microphone. Here I am using Matrix Voice microphone

Then it will ask you to select the speaker. Here I am using RPi audio jack as speaker.

To test Snips.ai is properly working by installing a demo assistant for the weather or not.

sam install demo 

 

image

 

After installing as you see snips assistant is running.

Now, test the assistant by saying

"Hey Snips!" "What will the weather be like in Madagascar in two days?" 

The response from Snips should be:

"You asked for the weather in Madagascar in two days." 

You can test whether all services are running or not using command

sam status

 

image

 

Congratulations we have successfully installed Snips on RPi.

 

Control lights with Snips.ai

 

1. Creating a Snips assistant & app

Sign into your Snips.ai and create an assistant. After sign in you page will like this

 

image

2. Create a new assistant

 

image

3. Give name to an assistant, select language and then create it.Once created you will see page like this

image

 

4. Then click on add an app and you will see page like this

image

5. Select create a new app and give it a name whatever you want and create it

image

Once created you will see page like this

 

image

 

6. After that open the app, click on edit app.

image

You will see page like this. As you see I already created intent (lights). You will see no intent on your page.

 

image

7. Create a new intent

imageimage

 

After creating you will see page like this. My intent name is lights

 

image

 

8. Give training examples (you can give training examples after creating slots also).

image

9. Then create a new slots and give it name whatever you want. Here I am using four slots

  • switch for on and off state
  • room for different rooms such as bedroom, bathroom etc
  • device for devices such as light, fan etc
  • brightness for setting brightness of light in different rooms.

 

image

 

10. Then give slot type name. Here I am building custom slot type.

  • For room slot

image

 

After that add slot values "bathroom", "bedroom" and "kitchen".

image

 

  • For switch slot

image

 

After that add slot values "on","off","open", and "close".

image

  • For device slot

Give any name whatever you want.

image

 

After that add slot values such as "light", "fan", and "door".

image

  • For brightness slot

Give any name whatever you want.

 

image

After that add slot values 75, 50, 25, 0

image

 

 

11. Close the app, in order to tell the training example which slot is used, double click on off and on and select slot name(switch).

image

 

Double click on room name and select slot name(room).

 

image

 

Double click on light, fan and select slot name(device).

image

 

Double click on values(0, 25, 50) and select slot name(brightness).

image

Then save it and you can test it in window provided right hand side of the page.

 

image

Then deploy it

image

 

Connect SAM to Raspberry Pi on personal computer

 

1. From your computer's terminal, sign in through the Sam CLI Tool

sam login 

Login using your snips account

2. Connect to your Raspberry Pi. When prompted for a username & password, insert the Raspberry Pi credentials.

sam connect YOUR.PI.IP.HERE 

3. Copy the command and paste on your local computer.

image

After deploying on your Pi you will see like this

image

 

Creating Assistant on RPi

 

Assistant will be used to listen and respond to events from your Snips assistant

1. Go to the directory which we made during JavaScript setup in Matrix core. cd ~/js-matrix-core-app and create 4 new JavaScript files.

touch assistant.js pwm.js everloop.js func.js

 

2. Install MQTT to listen in on events from Snips.

npm install mqtt --save

3. Open everloop.js using any editorand paste the code given in program. Code is used to control the LEDs on the MATRIX Creator/Voice.

 

4. Open relay.js using any editor and paste the code given in program. It is used to turn the relay on and off.

 

5. Open assistant.js using any editor and paste the code given in program. It combines all the code from everloop.js & relay.js to control the everloop and relay switch through voice. It shows you how to listen to lightState intents and read slots.

var snipsUserName = 'ruchir'; // username of snips account 
var lightState = 'hermes/intent/'+snipsUserName+':lightState'; // name of intent you give while creating an intent

imageimage

 

Once done now it is time to check.Open your personal computer(Ubuntu) terminal and run

sam watch

On the other hand, open RPi terminal and go to the directory

cd js-matrix-core-app/
node assistant.js  // run it 

 

Training examples

 

turn on bathroom light

turn on the kitchen lights

turn off the bedroom lights

turn on all the light

set bathroom light intensity to 25 percent

set kitchen light intensity to 75 percent

set bedroom light intensity to 50 percent

set bedroom light intensity to 0 percent

open the main hall door

close the main hall door

Webpage

 

I made a page for showing the logs (room, devices, device state, intensity value and date) and gauge showing current intensity value so that I can know which command I used while talking to the snips. Follow the steps giving below for making a webpage.

 

Note - You can use either Node server or Apache server.

 

In this project I am using node server because Apache server is slow and it was not able to update data correctly.

 

Note - If you use code given in this project make sure your all the data is in cd /var/www/html directory or you can change location in the program.

 

First, to install Apache server using command (Not required)

sudo apt-get install apache2 

Apache server is not required if you have node server

                                         or

Node server

Make an empty file name server.js, add program given below and save it.

 

var http = require('http');
var url = require('url');
var fs = require('fs');
var express=require('express');
var bodyParser=require('body-parser');
var nodemailer=require('nodemailer');

var app = express();
app.post('/formaction',function(req,res){
res.writeHead(301,{'location':'http://127.0.0.1:8080/HA.html'});
res.write('<html><script>function newpage(){window.location.href="localhost:8008/HA.html";}</script><body onload="newpage()"></body></html>');
res.end();
var transporter = nodemailer.createTransport({
  service: 'gmail',
  auth: {
  user: '', 
  pass: ''
  }
});
console.log('transporter ready');
var mailOptions = {
  from: '',
  to: '',
  subject: 'Sending Email using Node.js',
  text: Date().toGMTString
};
console.log('mail options set');
transporter.sendMail(mailOptions, function(error, info){
  if (error) {
  console.log(error);
  } else {
  console.log('Email sent: ' + info.response);
  }
console.log('mail on sending');
});
}).listen(8008);



http.createServer(function (req, res) {
  var q = url.parse(req.url, true);
  var filename = "." + q.pathname;
  fs.readFile(filename, function(err, data) {
  if (err) {
  res.writeHead(404, {'Content-Type': 'text/html'});
  return res.end("404 Not Found");
  } 
  res.writeHead(200, {'Content-Type': 'text/html'});
  res.write(data);
  return res.end();
  });
}).listen(8080);

 

 

To run server use command

node server.js 

Next, go to the directory cd /var/www/html and make two folders

1. Make a folder name js using command

mkdir js 
cd js // go to the directory

In /var/www/html/js directory make a file name angular.min.js  and paste data from the link given below

link

In same directory make another file name gauge.min.js and paste data from the link given below

link

required files

 

2. Make a folder name jsonpage using command

mkdir jsonpage
cd jsonpage

In jsonpage directory make a file name info.js. Make it empty

Note:- Json file will be cleared after 50 voice commands

Login page

 

For making login page go to the directory cd /var/www/html and make an empty file name index.html. Add program given below

 

<html>
<head>

<title>Login Page</title>
<meta name="viewport" content="width=device-width, initial-scale=1.0">
</head>

<div align="center">
<p><font color="red"size=5>PLEASE LOGIN TO SEE THE LOGS</font></p> 
</div>

<br>


<form name="loginForm" method="POST" action="http://127.0.0.1:8008/formaction">
<table width="20%" bgcolor="0099CC" align="center" >

<tr>
<td colspan=2><center><font size=4><b>Login Page</b></font></center></td>
</tr>

<tr>
<td>Username:</td>
<td><input type="text" size=25 name="userid"></td>
</tr>

<tr>
<td>Password:</td>
<td><input type="Password" size=25 name="pwd"></td>
</tr>


<tr>
<td ><input type="Reset"></td>
<td><input type="submit" onclick="return check(this.form)" value="Login"></td>
</tr>

</table>
</form>
<script language="javascript">
function check(form)
{

if(form.userid.value == "default" && form.pwd.value == "default")
{    
    var date=new Date();
    date.setTime(date.getTime()+(15*60*1000));<!-- Time 15-->
    document.cookie= 'User=default;expires='+date.toGMTString()+';';
    return true;
    
}
else
{
    alert("Error, Enter valid Username or Password")
    return false;
}
}
</script>

<br><br><br><br>

<div align="left">
<p><font color="brown"size=3>Developed by :</font></p> 
<p><font color="brown"size=5>RUCHIR SHARMA & ADITYA BHARDWAJ </font></p>
<p><font color="brown"size=3></font></p>
</div>

<p><mark><strong>Note: </strong>Supported in Mozilla Firefox & Chromium browser</mark></p>

</body>
</html>

Main page

For making main page go to the directory cd /var/www/html and make an empty file name HA.html(any). Add program given below

(dummy code)

<!DOCTYPE html>
<html lang="en">
<head>
    <meta charset="UTF-8">
    <meta name="viewport" content="width=device-width, initial-scale=1.0">
    <meta http-equiv="X-UA-Compatible" content="ie=edge">
    <title>GUI View</title>
</head>
<style>
    body{
        background-size: 100% 100%;
        align:center;
    }
    table{
        color: white;
        border: ridge 3px yellow;
    }
</style>
<script src = "./js/angular.min.js"> </script>
<script src = './js/gauge.min.js'></script>
<script src = 'index.js'></script>
<body onload = "checkcookie()" background ='./image/i1.jpeg' ng-app="APP" onmouseover="cellcolor()">
    <table border =3 id ='table_id'align="center">
        <tr>
            <td>
                room & devices
            </td>
            <td>
                device state
            </td>
            <td>
                device intensity
            </td>
        <td>
        Time
        </td>
        </tr>
        <tbody ng-controller="ctrl">
        <tr ng-repeat="x in datafile">
            <td>
                {{x.device}}
            </td>
            <td>
                {{x.state}}
            </td>
            <td>
                {{x.intensity}}
            </td>
        <td>
        {{x.time}}
        </td>
        </tr>
        </tbody>
    </table><br><br>
    <div style="background-color:yellow;margin-left:350px;margin-right:350px">
    <center>
    <canvas id='gauge'></canvas><br>
    <div id='demo123'></div>
    </center>
    </div>
</body>
<script>
var app= angular.module("APP",[]); 
app.controller("ctrl",
        function($scope,$http){
            $http.get("./jsonpage/info.json").then(function(response){
                $scope.datafile=response.data;
            });
    });
function cellcolor(){
     set different color of cell based on text }

read();
    setTimeout(function(){draw('demo123');},3000);
    function cookies(){
            var name = "User=";
            var decodedCookie = decodeURIComponent(document.cookie);
            var ca = decodedCookie.split(';');
            for(var i = 0; i < ca.length; i++) {
            var c = ca[i];
            while (c.charAt(0) == ' ') {
            c = c.substring(1);
            }
            if (c.indexOf(name) == 0) {
                    return c.substring(name.length, c.length);
                }
            }
        }
    function checkcookie(){
        var user=cookies();
        if(user==undefined){
            window.location.href = 'index.html'
        }
    }
</script>
</html>

 

For making gauge make a empty file name index.js in cd /var/www/html directory. Program is given below.

 

function read(){
console.log('js started');
var intensity;

var rawfile = new XMLHttpRequest();
rawfile.overrideMimeType("application/json");
rawfile.open("GET", "./jsonpage/info.json", true); 
rawfile.onreadystatechange = function()
{
  if (rawfile.readyState === 4 && rawfile.status == "200" )
  {  
   
  console.log("ready to read");
   
  var data = JSON.parse(rawfile.responseText);
  console.log('json parsed');
  intensity = data[data.length-1].intensity;
  console.log('intensity set to ',intensity);
  console.log('intensity is',intensity);
  document.getElementById('demo123').innerHTML = intensity;
  }
}
rawfile.send();

}
function draw(x){
  var opts = {
  angle: -0.1,
  lineWidth: 0.1, 
  limitMax: 'true', //false
  title:{
  text: 'Intensity'
  } ,
  strokeColor: 'red',
  generateGradient: true,
  pointer: {
  length: 0.5, //The radius of the inner circle
  strokeWidth: 0.03, // The rotation offset
  color: 'red' // Fill color
  },
  staticLabels: {
  font: "90% sans-serif", // Specifies font
  labels: [0, 25, 50, 75, 100], // Print labels at these values
  color: "red", // Optional: Label text color
  fractionDigits: 2 // Optional: Numerical precision. 0=round off.
  }, // just experiment with them
  strokeColor: 'red', // to see which ones work best for you
  staticZones: [
  {strokeStyle: "powderblue", min: 0, max: 25}, // Yellow33
  {strokeStyle: "lightskyblue", min: 25, max: 50}, // Green66
  {strokeStyle: "royalblue", min: 50, max: 75}, // Yellow
  {strokeStyle: "blue", min: 75, max: 100},
  ],
  generateGradient: true
};
console.log(document.getElementById(x)); //
if(document.getElementById(x).firstChild.data == 'zero'){
var inten=0;
}
if(document.getElementById(x).firstChild.data == 'twenty five'){
  var inten=25;
}
if(document.getElementById(x).firstChild.data == 'fifty'){
  var inten=50;
}
if(document.getElementById(x).firstChild.data == 'seventy five'){
  var inten=75;
}

var gauge_value = inten;
console.log(gauge_value);
var target = document.getElementById('gauge'); // your canvas element
var gauge = new Gauge(target).setOptions(opts); // Donut create sexy gauge!
gauge.maxValue = 100; // set max gauge value
gauge.animationSpeed = 40; // set animation speed (32 is default value)
gauge.set(gauge_value); // set actual value  
}

 

Required npm package

 

For sending mail install node package

npm install nodemailer 

Npm package for bidirectional event-based communication

npm install socket.io 

Npm package for express

npm install express 

If you want to hear the words. You can download this node package.

npm install say 

Add these lines in program (example)

const say = require('say')  say.speak('Brightness is set to 75'); 

 

assistant.js for webpage (dummy code)

var fs=require('fs');
var mqtt = require('mqtt');
var client = mqtt.connect('mqtt://localhost', { port: 1883 });
var func =require('./func.js'); 
var everloop = require('./everloop.js');
var pwmlight = require('./pwm.js');
var snipsUserName = 'ruchir';
var wakeword = 'hermes/hotword/default/detected';
var sessionEnd = 'hermes/dialogueManager/sessionEnded';
var lightState = 'hermes/intent/'+snipsUserName+':lights';
var nodemailer=require('nodemailer');
//////////////
//ON CONNECT//
//////////////
client.on('connect', function() {
  console.log('Connected to Snips MQTT server\n');
  client.subscribe('hermes/hotword/default/detected');
  client.subscribe('hermes/dialogueManager/sessionEnded');
  client.subscribe(lightState);
});


//////////////
//ON MESSAGE//
//////////////
client.on('message', function(topic,message) {
  var message = JSON.parse(message);
  switch(topic) {
  // * On Wakeword
  case wakeword:
  everloop.startWaiting();
  console.log('Wakeword Detected');
  break;
  // * On Light State Change
  case lightState:
  // Turn lights On/Off
  try{

// controlling light using PWM
if(message.slots[0].rawValue==='on' || message.slots[0].rawValue==='off'|| message.slots[0].rawValue==='open' || message.slots[0].rawValue==='close'){ 

var room=message.slots[1].rawValue; // room types slot
console.log(room);
var state=message.slots[0].rawValue; // state type slot
console.log(state);
var device=message.slots[2].rawValue;// device type slot
  console.log(device);



switch(room){
// Bathroom light on/off
case 'bathroom':
  if(device ==='light'){
  func.roomtype(0,state);
  console.log("Bathroom light");
  }
  else if(device ==='fan'){
  func.roomtype(5,state);
  console.log("Bathroom fan");
  }
break;


// Bedroom light on/off

case 'bedroom':
if(device === 'light'){
func.roomtype(1,state);
  console.log("Bedroom light");
}
else if(device === 'fan'){
func.roomtype(6,state);
console.log("Bedroom fan");
}

break;

// Kitchen light on/off

case 'Kitchen':
  if(device === 'light'){
  func.roomtype(2,state);
  console.log("Kitchen light");
  }
  else if(device ==='fan'){
  func.roomtype(7,state);
  console.log("Kitchen chimney");
  }

break;


// Living room light on/off
case 'living room':
if(device ==='light'){
  func.roomtype(3,state);
  console.log("Living room light");
  }
  else if(device ==='fan'){
  func.roomtype(8,state);
  console.log("Living room fan");
  }
break;

// Drawing room light on/off
case 'drawing room':
if(device ==='light'){
  func.roomtype(4,state);
  console.log("Drawing room light");
  }
  else if(device ==='fan'){
  func.roomtype(9,state);
  console.log("Drawing room fan");
  }

break;
case 'main hall':
if(device ==='door'){
  func.roomtype(10,state);
  console.log(" Main hall door ");
  }
  else if(device ==='light'){
  func.roomtype(11,state);
  console.log("main hall light");
  }
break;
// for turning all lights on/off
case 'all':func.roomtype(0,state);
  console.log("Bathroom light");
  func.roomtype(1,state);
  console.log("Bedroom light");
  func.roomtype(2,state);
console.log("Kitchen light");
func.roomtype(3,state);
console.log("Living room light");
func.roomtype(4,state);
console.log("Drawing room light");
func.roomtype(11,state);
console.log("Hall room light");

var date=new Date();
  var info=fs.readFileSync('/var/www/html/jsonpage/info.json','utf-8');
  if(info==""){
          write a fresh json file (array of objects in this case)
  }
  else{
          append the data into the json file  
  }
          read the new json file contents
 if(greater than certain length){
          mail it to you and delete the json records
  }
 }

else{

// for controlling light brightness using PWM

var room=message.slots[0].rawValue; // room type slot
console.log(room);
var device=message.slots[1].rawValue; // device type slot
  console.log(device);
var brightness= message.slots[2].rawValue; // brightness value slot
  console.log(brightness);


switch(room){
// set bathroom light brightness 
case 'bathroom':

if (device ==='light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(0);
  console.log('Brightness is set to 75 ')
}
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(0);
console.log('Brightness is set to 50 ')
  }
  else if (device ==='light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(0);
console.log('Brightness is set to 25 ')
  }
else if (device ==='light' && brightness === 'zero'){
  pwmlight.pwmzero(0);
console.log('Brightness is set to 0 ')
}
else if (device ==='light' && brightness === 'hundred'){
  pwmlight.pwmzero(0);
  console.log('Brightness is set to 100 ')
}
break;

// set bedroom light brightness

case 'bedroom' :

if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(1);
console.log("Brightness is set to 100")
}
else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(1);
console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(1);
console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(1);
console.log("Brightness is set to 25")
  }
else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmzero(1);
  console.log("Brightness is set to 0")
  }

break;
// Set Kitchen light brightness

case 'Kitchen' :

if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(2);
  console.log("Brightness is set to 100")
  }
else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(2);
console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(2);
console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(2);
console.log("Brightness is set to 25")
  }
else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmonequat(2);
  console.log("Brightness is set to 0")
}
break;


// Set Living room brightness 

case 'living room':
if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(3);
  console.log("Brightness is set to 100")
  }
  else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(3);
  console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(3);
  console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(3);
  console.log("Brightness is set to 25")
  }
  else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmonequat(3);
  console.log("Brightness is set to 0")
}

break;

//Set drawing room brightness 

case 'drawing room':
if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(4);
  console.log("Brightness is set to 100")
  }
  else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(4);
  console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(4);
  console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(4);
  console.log("Brightness is set to 25")
  }
  else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmzero(4);
  console.log("Brightness is set to 0")
}
break;



  }
var date=new Date();
  read json file info.json
  if(info==""){
          write a fresh json file (array of objects in this case)
  }
  else{
          append the data into the json file  
  }
          read the new json file contents
 if(greater than certain length){
          mail it to you and delete the json records
  }
 }

// Expect error if `on` or `off` is not heard
  catch(e){
  console.log(e)
  }
  break;
  // * On Conversation End
  case sessionEnd:
  everloop.stopWaiting();
  console.log('Session Ended\n');
  break;
  }
});

Once done with all the setup.

Next, Open shell and run

cd js-matrix-core-app 
node assistant.js

Open another shell and run

cd /var/www/html 
node server.js

Open browser

localhost:8080/index.html 

Connections

Relay ==> Matrix Voice

  • 5V ==> 5V
  • GND ==>GND
  • Signal1 ==> GPIO0 (DF0)
  • Signal2 ==> GPIO1 (DF1)
  • Signal3 ==> GPIO2 (DF2)
  • Signal4 ==> GPIO3 (DF3)
  • Signal5 ==> GPIO5 (DF5)
  • signal6 ==> GPIO11 (DF11)

 

Servo Motor ==> Matrix Voice

  • 5V  ==> 5V
  • GND ==> GND
  • Signal ==> GPIO10(DF10)

 

 

 

image

 

image

Program

 

assistant.js

 

/////////////
//VARIABLES//
/////////////

var mqtt = require('mqtt');
var client = mqtt.connect('mqtt://localhost', { port: 1883 });
var func =require('./func.js'); 
var everloop = require('./everloop.js');
var pwmlight = require('./pwm.js');
var snipsUserName = 'ruchir'; // snips username
var wakeword = 'hermes/hotword/default/detected';
var sessionEnd = 'hermes/dialogueManager/sessionEnded';
var lightState = 'hermes/intent/'+snipsUserName+':lights'; // intent name

//////////////
//ON CONNECT//
//////////////
client.on('connect', function() {
  console.log('Connected to Snips MQTT server\n');
  client.subscribe('hermes/hotword/default/detected');
  client.subscribe('hermes/dialogueManager/sessionEnded');
  client.subscribe(lightState);
});


//////////////
//ON MESSAGE//
//////////////
client.on('message', function(topic,message) {
  var message = JSON.parse(message);
  switch(topic) {
  // * On Wakeword
  case wakeword:
  everloop.startWaiting();
  console.log('Wakeword Detected');
  break;
  // * On Light State Change
  case lightState:
  // Turn lights On/Off
  try{

// controlling light using PWM
if(message.slots[0].rawValue==='on' || message.slots[0].rawValue==='off'|| message.slots[0].rawValue==='open' || message.slots[0].rawValue==='close'){ 

var room=message.slots[1].rawValue; // room types slot
console.log(room);
var state=message.slots[0].rawValue; // state type slot
console.log(state);
var device=message.slots[2].rawValue;// device type slot
  console.log(device);



switch(room){
// Bathroom light on/off
case 'bathroom':
  if(device ==='light'){
  func.roomtype(0,state);
  console.log("Bathroom light");
  }
  else if(device ==='fan'){
  func.roomtype(5,state);
  console.log("Bathroom fan");
  }
break;


// Bedroom light on/off

case 'bedroom':
if(device === 'light'){
func.roomtype(1,state);
  console.log("Bedroom light");
}
else if(device === 'fan'){
func.roomtype(6,state);
console.log("Bedroom fan");
}

break;

// Kitchen light on/off

case 'Kitchen':
  if(device === 'light'){
  func.roomtype(2,state);
  console.log("Kitchen light");
  }
  else if(device ==='fan'){
  func.roomtype(7,state);
  console.log("Kitchen chimney");
  }

break;


// Living room light on/off
case 'living room':
if(device ==='light'){
  func.roomtype(3,state);
  console.log("Living room light");
  }
  else if(device ==='fan'){
  func.roomtype(8,state);
  console.log("Living room fan");
  }
break;

// Drawing room light on/off
case 'drawing room':
if(device ==='light'){
  func.roomtype(4,state);
  console.log("Drawing room light");
  }
  else if(device ==='fan'){
  func.roomtype(9,state);
  console.log("Drawing room fan");
  }

break;
case 'main hall':
if(device ==='door'){
  func.roomtype(10,state);
  console.log(" Main hall door ");
  }
  else if(device ==='light'){
  func.roomtype(11,state);
  console.log("main hall light");
  }
break;
// for turning all lights on/off
case 'all':func.roomtype(0,state);
  console.log("Bathroom light");
  func.roomtype(1,state);
  console.log("Bedroom light");
  func.roomtype(2,state);
console.log("Kitchen light");
func.roomtype(3,state);
console.log("Living room light");
func.roomtype(4,state);
console.log("Drawing room light");
func.roomtype(11,state);
console.log("Hall room light");

}
}

else{

// for controlling light brightness using PWM

var room=message.slots[0].rawValue; // room type slot
console.log(room);
var device=message.slots[1].rawValue; // device type slot
  console.log(device);
var brightness= message.slots[2].rawValue; // brightness value slot
  console.log(brightness);


switch(room){
// set bathroom light brightness 
case 'bathroom':

if (device ==='light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(0);
  console.log('Brightness is set to 75 ')
}
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(0);
console.log('Brightness is set to 50 ')
  }
  else if (device ==='light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(0);
console.log('Brightness is set to 25 ')
  }
else if (device ==='light' && brightness === 'zero'){
  pwmlight.pwmzero(0);
console.log('Brightness is set to 0 ')
}
else if (device ==='light' && brightness === 'hundred'){
  pwmlight.pwmzero(0);
  console.log('Brightness is set to 100 ')
}
break;

// set bedroom light brightness

case 'bedroom' :

if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(1);
console.log("Brightness is set to 100")
}
else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(1);
console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(1);
console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(1);
console.log("Brightness is set to 25")
  }
else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmzero(1);
  console.log("Brightness is set to 0")
  }

break;
// Set Kitchen light brightness

case 'Kitchen' :

if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(2);
  console.log("Brightness is set to 100")
  }
else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(2);
console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(2);
console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(2);
console.log("Brightness is set to 25")
  }
else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmonequat(2);
  console.log("Brightness is set to 0")
}
break;


// Set Living room brightness 

case 'living room':
if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(3);
  console.log("Brightness is set to 100")
  }
  else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(3);
  console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(3);
  console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(3);
  console.log("Brightness is set to 25")
  }
  else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmonequat(3);
  console.log("Brightness is set to 0")
}

break;

//Set drawing room brightness 

case 'drawing room':
if (device === 'light' && brightness === 'hundred'){
  pwmlight.pwmfull(4);
  console.log("Brightness is set to 100")
  }
  else if (device === 'light' && brightness === 'seventy five'){
  pwmlight.pwmthreequater(4);
  console.log("Brightness is set to 75")
  }
  else if (device === 'light' && brightness === 'fifty'){
  pwmlight.pwmhalf(4);
  console.log("Brightness is set to 50")
  }
  else if (device === 'light' && brightness === 'twenty five'){
  pwmlight.pwmonequat(4);
  console.log("Brightness is set to 25")
  }
  else if (device === 'light' && brightness === 'zero'){
  pwmlight.pwmzero(4);
  console.log("Brightness is set to 0")
}
break;



}
  }
} 
  // Expect error
  catch(e){
  console.log(e)
  }
  break;
  // * On Conversation End
  case sessionEnd:
  everloop.stopWaiting();
  console.log('Session Ended\n');
  break;
  }
});

 

everloop.js

/////////////
//VARIABLES//
/////////////
var zmq = require('zeromq');// Asynchronous Messaging Framework
var matrix_io = require('matrix-protos').matrix_io;// Protocol Buffers for MATRIX function
var matrix_ip = '127.0.0.1';// Local IP
var matrix_everloop_base_port = 20021;// Port for Everloop driver
var matrix_device_leds = 0;// Holds amount of LEDs on MATRIX device
var methods = {};// Declaration of method controls at the end
var waitingToggle = false;
var counter = 0;
///////////////////
//KEEP ALIVE PORT//
///////////////////
// Create a Pusher socket
var pingSocket = zmq.socket('push')
// Connect Pusher to Keep-alive port
pingSocket.connect('tcp://' + matrix_ip + ':' + (matrix_everloop_base_port + 1));
// Send a single ping
pingSocket.send('');
//////////////
//ERROR PORT//
//////////////
// Create a Subscriber socket
var errorSocket = zmq.socket('sub');
// Connect Subscriber to Error port
errorSocket.connect('tcp://' + matrix_ip + ':' + (matrix_everloop_base_port + 2));
// Connect Subscriber to Error port
errorSocket.subscribe('');
// On Message
errorSocket.on('message', function(error_message){
 console.log('Error received: ' + error_message.toString('utf8'));// Log error
});
////////////////////
//DATA UPDATE PORT//
////////////////////
// Create a Subscriber socket
var updateSocket = zmq.socket('sub');
// Connect Subscriber to Data Update port
updateSocket.connect('tcp://' + matrix_ip + ':' + (matrix_everloop_base_port + 3));
// Subscribe to messages
updateSocket.subscribe('');
// On Message
updateSocket.on('message', function(buffer){
 var data = matrix_io.malos.v1.io.EverloopImage.decode(buffer);// Extract message
 matrix_device_leds = data.everloopLength;// Save MATRIX device LED count
});
/////////////
//BASE PORT//
/////////////
// Create a Pusher socket
var configSocket = zmq.socket('push');
// Connect Pusher to Base Port
configSocket.connect('tcp://' + matrix_ip + ':' + matrix_everloop_base_port);
// Create an empty Everloop image
var image = matrix_io.malos.v1.io.EverloopImage.create();
setInterval(function(){
  // Turns off all LEDs
  if (waitingToggle == false) {
  for (var i = 0; i < matrix_device_leds; ++i) {
  // Set individual LED value
  image.led[i] = {
  red: 0,
  green: 0,
  blue: 0,
  white: 0
  };
  }
  };
  // Creates pulsing LED effect
  if (waitingToggle == true) {
  for (var i = 0; i < matrix_device_leds; ++i) {
  // Set individual LED value
  image.led[i] = {
  red: (Math.round((Math.sin(counter) + 1) * 100) + 10),
  green: (Math.round((Math.sin(counter) + 1) * 100) + 10),
  blue: (Math.round((Math.sin(counter) + 1) * 100) + 10),// Math used to make pulsing effect
  white: 0
  };
  }
  };
  counter = counter + 0.2;
  // Store the Everloop image in MATRIX configuration
  var config = matrix_io.malos.v1.driver.DriverConfig.create({
  'image': image
  });
  // Send MATRIX configuration to MATRIX device
  if(matrix_device_leds > 0) {
  configSocket.send(matrix_io.malos.v1.driver.DriverConfig.encode(config).finish());
  };
},50);
///////////////////
//WAITING METHODS//
///////////////////
methods.startWaiting = function() {
  waitingToggle = true;
};
methods.stopWaiting = function() {
  waitingToggle = false;
};
module.exports = methods;

func.js

var everloop = require('./everloop.js');
var pwmlight = require('./pwm.js');
var methods={};
methods.roomtype = function(pin,state){
  if (state === 'on'){
  pwmlight.lightOn(pin);// passing arguments
  everloop.stopWaiting();
  console.log('light is turned On');
  }
  else if(state === 'off'){
  pwmlight.lightOff(pin);
  everloop.stopWaiting();
  console.log('light is turned Off');
  }
else if(state === 'open'){
pwmlight.dooropen(pin);
everloop.stopWaiting();
console.log('door is open');
}
else if(state === 'close'){
  pwmlight.doorclose(pin);
  everloop.stopWaiting();
  console.log('door is close');
  }

};

module.exports = methods;

 

pwm.js

// PWM functions for controlling lights
var matrix = require("@matrix-io/matrix-lite");
var methods = {};// Declaration of method controls at the end

methods.pwmfull = function(pin){

  matrix.gpio.setFunction(pin, 'PWM');
  matrix.gpio.setMode(pin, 'output');
  matrix.gpio.setPWM({
  pin: pin,
  percentage: 100,
  frequency: 60 
});

};

methods.pwmthreequater = function(pin){


matrix.gpio.setFunction(pin, 'PWM');
matrix.gpio.setMode(pin, 'output');
matrix.gpio.setPWM({
pin: pin,
percentage: 75,
frequency: 60 

});

};

methods.pwmhalf = function(pin){

matrix.gpio.setFunction(pin, 'PWM');
matrix.gpio.setMode(pin, 'output');
matrix.gpio.setPWM({
pin: pin,
percentage: 50,
frequency: 60  

});
};

methods.pwmonequat = function(pin){

  matrix.gpio.setFunction(pin, 'PWM');
  matrix.gpio.setMode(pin, 'output');
  matrix.gpio.setPWM({
  pin: pin,
  percentage: 25,
  frequency: 60 // min 36
});
};

methods.pwmzero = function(pin){


  matrix.gpio.setFunction(pin, 'PWM');
  matrix.gpio.setMode(pin, 'output');
  matrix.gpio.setPWM({
  pin: pin,
  percentage: 0,
  frequency: 60 

});

};

methods.lightOn = function(pin){
   
  matrix.gpio.setFunction(pin, 'PWM');
  matrix.gpio.setMode(pin, 'output');
  matrix.gpio.setPWM({
  pin: pin,
  percentage: 100,
  frequency: 60 
});

};

methods.lightOff = function(pin){


  matrix.gpio.setFunction(pin, 'PWM');
  matrix.gpio.setMode(pin, 'output');
  matrix.gpio.setPWM({
  pin: pin,
  percentage: 0,
  frequency: 60 

});

};

//For controlling doors

methods.dooropen = function(pin){

matrix.gpio.setFunction(pin, 'PWM');
matrix.gpio.setMode(pin, 'output');
matrix.gpio.setServoAngle({
  pin: pin,
  angle: 160,
  // minimum pulse width for a PWM wave (in milliseconds)
  min_pulse_ms:0.8 // 0.8
});

};

methods.doorclose = function(pin){

matrix.gpio.setFunction(pin, 'PWM');
matrix.gpio.setMode(pin, 'output');
matrix.gpio.setServoAngle({
  pin: pin,
  angle: 10,
  // minimum pulse width for a PWM wave (in milliseconds)
  min_pulse_ms:0.8 // 0.8
});

};

module.exports = methods;

Result

imageimage
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
  • ruchir1674
    ruchir1674 over 7 years ago in reply to vimarsh_ +3
    Thanks
  • vimarsh_
    vimarsh_ over 7 years ago +2
    Awesome! Very Detailed Guide!
  • ruchir1674
    ruchir1674 over 7 years ago in reply to ipv1 +1
    Hey If snips audio server not running you can use " sudo sam init " in Linux or "sam init" in Windows and then check it. Please note that if you are deploying assistant first time then first deploy demo…
Parents
  • ipv1
    ipv1 over 7 years ago

    I cant seem to get the snips-audio-server running.

    error log.

    [ x ] Commented out dummy as per https://community.matrix.one/t/matrix-voice-snips-home-assistant-working-together/1519/22

    [ x ] sam test microphone works

    [ x ] recording and playback on the pi using arecorder and aplay works as well.

    Apr 26 00:51:54 raspberrypi systemd[1]: snips-audio-server.service: Failed with result 'exit-code'.

    Apr 26 00:51:59 raspberrypi systemd[1]: snips-audio-server.service: Service hold-off time over, scheduling restart.

    Apr 26 00:51:59 raspberrypi systemd[1]: Stopped Snips Audio Server.

    Apr 26 00:51:59 raspberrypi systemd[1]: Started Snips Audio Server.

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: INFO:snips_audio_server_cli: Starting audio server on mqtt for site default

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: INFO:snips_broadcast_mqtt_server: Starting broadcasting audio on hermes as site "default"

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.front

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.rear

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.center_lfe

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.side

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.surround21

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.surround40

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.surround41

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.surround50

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.surround51

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.surround71

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.iec958

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.iec958

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.hdmi

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.modem

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM cards.pcm.phoneline

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib confmisc.c:1281:(snd_func_refer) Unable to find definition 'defaults.bluealsa.device'

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib conf.c:4528:(_snd_config_evaluate) function snd_func_refer returned error: No such file or directory

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib conf.c:4996:(snd_config_expand) Args evaluate error: No such file or directory

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM bluealsa

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib confmisc.c:1281:(snd_func_refer) Unable to find definition 'defaults.bluealsa.device'

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib conf.c:4528:(_snd_config_evaluate) function snd_func_refer returned error: No such file or directory

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib conf.c:4996:(snd_config_expand) Args evaluate error: No such file or directory

    Apr 26 00:51:59 raspberrypi snips-audio-server[5643]: ALSA lib pcm.c:2495:(snd_pcm_open_noupdate) Unknown PCM bluealsa

    Apr 26 00:51:59 raspberrypi systemd[1]: snips-audio-server.service: Main process exited, code=exited, status=1/FAILURE

    Apr 26 00:51:59 raspberrypi systemd[1]: snips-audio-server.service: Unit entered failed state.

    Apr 26 00:51:59 raspberrypi systemd[1]: snips-audio-server.service: Failed with result 'exit-code'.

    Any clues?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ruchir1674
    ruchir1674 over 7 years ago in reply to ipv1

    Hey

     

    If snips audio server not running you can use " sudo sam init " in Linux or "sam init" in Windows and then check it.

    Please note that if you are deploying assistant first time then first deploy demo one and check sam status and than deploy which you made. Please let me know whether you able to fix that or not

     

    Regards

    Ruchir

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 7 years ago in reply to ruchir1674

    I tried the demo and it shows the audio-server not running. Looks like it can't seem to find the MicArray correctly even with the mike entry in the snips.toml file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ruchir1674
    ruchir1674 over 7 years ago in reply to ipv1

    Please see whether you properly configured mics

     

    edit the snips.toml file for configuring the mics on RPi.

    Scroll down to where you see [snips-audio-server] and replace

    # mike = "Built-in Microphone" 
    with the following:
    mike = "MATRIXIO SOUND: - (hw:2,0)"

    As you said speaker and microphone are working  so no need to use sam setup audio.

     

    Please check and let me know.

     

    Check one more thing is after installing assistant

    test the assistant by saying

    "Hey Snips!" "What will the weather be like in Madagascar in two days?" 

    and see whether it give you any response. Response should be:

    "You asked for the weather in Madagascar in two days." 

    and also run sam status

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ruchir1674
    ruchir1674 over 7 years ago in reply to ipv1

    Please see whether you properly configured mics

     

    edit the snips.toml file for configuring the mics on RPi.

    Scroll down to where you see [snips-audio-server] and replace

    # mike = "Built-in Microphone" 
    with the following:
    mike = "MATRIXIO SOUND: - (hw:2,0)"

    As you said speaker and microphone are working  so no need to use sam setup audio.

     

    Please check and let me know.

     

    Check one more thing is after installing assistant

    test the assistant by saying

    "Hey Snips!" "What will the weather be like in Madagascar in two days?" 

    and see whether it give you any response. Response should be:

    "You asked for the weather in Madagascar in two days." 

    and also run sam status

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ruchir1674
    ruchir1674 over 7 years ago in reply to ruchir1674

    Are you using fresh Raspbian ?

     

    https://docs.snips.ai/additional-resources/troubleshooting

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 7 years ago in reply to ruchir1674

    Tried it and then used netcat to stream from arecord to the service to make it work... Kinda. But it's quite slow in it's response because of that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ruchir1674
    ruchir1674 over 7 years ago in reply to ipv1

    Are you able to run snips audio server

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ipv1
    ipv1 over 7 years ago in reply to ruchir1674

    It does not run automatically and I had to start it up with the --no-mike option and provide a nc  from the arecord application.

     

    It's possible that it cannot find the matrix creator as a valid audio device though it shows up in alsamixer. Everything works as except the audio server. I have given up on it for now and hope someone will come up with a better install method.

     

    I installed the kernel module and can see it as a valid sound device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ruchir1674
    ruchir1674 over 7 years ago in reply to ipv1

    Hey

     

    Do one last thing use command

     

    sam setup audio

     

    Then it will ask whether you are using snips kit or not as you are using matrix so choose no

    Then it will ask you to select the microphone. Here select Matrix Creator microphone

    Then it will ask you to select the speaker. Here select RPi audio jack as speaker

    .

    After that check your assistant and let me know whether this work or not.

     

    Regards

    Ruchir