Making Time
  • Challenges & Projects
  • Project14
  • Making Time
  • More
  • Cancel
Making Time
Blog (Modified) Work Clock
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Making Time to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dwinhold
  • Date Created: 29 Nov 2020 6:28 PM Date Created
  • Views 4303 views
  • Likes 10 likes
  • Comments 13 comments
  • makingtimech
  • work clock
  • dwinhold
Related
Recommended

(Modified) Work Clock

dwinhold
dwinhold
29 Nov 2020

I am presenting the, "(Modified) Work Clock"

 

How often are you at work and feel:

     The time is just dragging on?

     Will this day ever end?

     I wish our lunch break is longer?

 

I would say every one of us feels this way now and then. I have the solution for this!!

 

The (Modified) Work Time Clock

 

Here is how it works: (This is set for my work day)

 

00:00:00 - Midnight - Personal Time (1 second = 1.1666667 seconds)

to

06:59:59

---------------------------

07:00:00 - Work Time (1 second = .6666667 seconds)

to

11:59:59

---------------------------

12:00:00 - Lunch Break (1 second = 1.1666667 seconds)

to

12:29:59

---------------------------

12:30:00 - Work Time (1 second = .6666667 seconds)

to

15:29:59

---------------------------

15:30:00 - Personal Time (1 second = 1.1666667 seconds)

to

00:00:00

 

Work clock math:

 

image

 

So, with the Modified Work Clock you now work only 5.3 hours a day and have 18.7 hours of personal time. This clock still keeps your day at 24 hours but changes the actual time you worked and your personal time.

With Project14's theme being "Making Time Change", this does it!!

 

Below is the Arduino code for the clock:

 

//Digital Arduino Work Clock
//By Dale Winhold
//Project14 Making time change
//Nov 29,2020

#include <LiquidCrystal.h>

LiquidCrystal lcd(12,11,5,4,3,2);

int h; //Hours
int m; //Minutes
int s; //Seconds


const int hs=6; //Hour set pin
const int ms=7; //Minutes set pin

int Hset;
int Mset;

void setup()
{
  lcd.begin(16,2);
  pinMode(hs,INPUT_PULLUP);
  pinMode(ms,INPUT_PULLUP);

}

void loop()
{

 lcd.setCursor(0,0); //Set lcd start print to 0,0
 s=s+1;
 lcd.print("TIME:");
 lcd.print(h);
 lcd.print(":");
 lcd.print(m);
 lcd.print(":");
 lcd.print(s);

//at work 7am to 12pm : 1 second=.6666667 seconds
 if(h>=7 && h<12){
  delay(666.6667);
  lcd.clear();
    if(s==60){
      s=0;
      m=m+1;
    }
    if(m==60){
      m=0;
      h=h+1;
    }
    if(h==24){
      h=0;
    }
  
  lcd.setCursor(0,1); //Set lcd start print to 0,1
  lcd.print("Work Time");
}

//at work 12:30pm to 3:30pm : 1 second=.6666667 seconds
else if((h==12 && m>29) || h==13 || h==14 || (h==15 && m<30)){
    delay(666.6667);
    lcd.clear();
      if(s==60){
        s=0;
        m=m+1;
      }
      if(m==60){
        m=0;
        h=h+1;
      }
      if(h==24){
        h=0;
      }
    
    lcd.setCursor(0,1); //Set lcd start print to 0,1
    lcd.print("Work Time");
}

//off work : 1 second=1.1666667 seconds
else{
  delay(1166.6667);
  lcd.clear();
    if(s==60){
      s=0;
      m=m+1;
    }
    if(m==60){
      m=0;
      h=h+1;
    }
    if(h==24){
      h=0;
    }
    
    lcd.setCursor(0,1); //Set lcd start print to 0,1
    lcd.print("Personal Time");
}

//-------Time
// setting-------//
Mset=digitalRead(ms);
if(Mset==0){
  s=0;
  m=m+1;
  }
  
Hset=digitalRead(hs);
if(Hset==0){
  h=h+1;
  }

}

 

A video of the time changing from personal time to work time. (Notice the difference in the seconds):

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

image

 

Rough sketch of the setup:

 

image

I really hope you like this project on "Making Time Change"

 

Dale Winhold

  • Sign in to reply

Top Comments

  • kmikemoo
    kmikemoo over 5 years ago +5
    dwinhold Boss, you've got it all backwards! The clock is supposed to run faster during the work day! Seriously though, I love the creativity. On some days... it really feels like the clock has two time…
  • dwinhold
    dwinhold over 5 years ago in reply to kmikemoo +4
    It is actually quite funny, I started to go over my chart in detail after I sent the reply. It took me a bit to figure out how that works out, I still am having issues. It looks good, works on paper and…
  • Fred27
    Fred27 over 5 years ago +4
    A really fun project. It reminds me a little of a clock someone wrote back in the day when I used to code as a contractor on an hourly rate. The clock started at £0.00 (or $0.00 or €0.00 as appropriate…
  • kmikemoo
    kmikemoo over 5 years ago

    dwinhold image  Boss, you've got it all backwards!  The clock is supposed to run faster during the work day!  Seriously though, I love the creativity.  On some days... it really feels like the clock has two time constants. image imageimage

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 5 years ago in reply to ajcc

    Thank you for your comment. I totally agree with the variable change to 59 & 23. I was going to use an RTC but it won’t work as it will keep correcting the time. With this clock there is still 24 hours a day. I have the time set buttons for setting the time which can be used whenever.

     

    Ddale W

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ajcc
    ajcc over 5 years ago

    This is an interesting idea and I'm really curious how the variable length seconds worked out for you so far?

    I also noticed your clock counts up to 24:60:60, maybe you could do the test for s > 59 (or s == 60 as its in your code) directly after incrementing the seconds counter instead of waiting until after your variable length one second delay?

    If you want more accurate time keeping you could look into using the onboard real time clock for syncing up your clock every so often. If I'm thinking correctly you'd do that every other second during the work day (2/3 seconds -> 3 seconds every two seconds) or seventh second during personal time (7/6 seconds -> 6 seconds every seven seconds)?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<