Month of Robots
  • Challenges & Projects
  • Project14
  • Month of Robots
  • More
  • Cancel
Month of Robots
Blog NVIDIA Jetson Nano: JetBot Assemble
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Month of Robots to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jomoenginer
  • Date Created: 28 Apr 2019 10:05 AM Date Created
  • Views 5202 views
  • Likes 17 likes
  • Comments 14 comments
  • nvidia jetson nano
  • robotics
  • jetbot
  • robot
  • morobotsch
  • raspberry pi
  • robot project
  • computer vision
Related
Recommended

NVIDIA Jetson Nano: JetBot Assemble

jomoenginer
jomoenginer
28 Apr 2019

Overview

 

In a previous post, and introduction to the NVIDIA Jetson Nano JetBot was given showing the parts required to create the JetBot as per the NVIDIA specs.  In this post, these parts will be used to assemble the JetBot and a basic Motion test will be shown.

 

image

 

Previous Related Posts

NVIDIA Jetson Nano

NVIDIA Jetson Nano: JetBot Intro

NVIDIA Jetson Nano: Collision Avoidance

 

Hardware Setup

 

The Hardware Setup required and tools need to assmble the JetBot are listed on the NVIDIA-AI-IOT JetBot WiKi

https://github.com/NVIDIA-AI-IOT/jetbot/wiki/Hardware-Setup

 

Hardware Required

Part Detail Quantity
M2 Screw 8mm long, self tapping 20
M3 Screw 25mm long 4
M3 Nut 4
Jumper wires Female-Female 4

 

It is suggested to use the M2 Screws listed since the other option is to use #2 standard screws but these do not work as well as the M2.  The M3 can be replaced by 4-40 x 1" screws though.

 

 

WiFi Module Install

To install the M.2 Intel Dual Band Wireless-Ac 8265 W/Bt8mm long, self tapping, the Jetson Nano SoM must be removed from the Carrier board.   This requires removing the 2 mounting screws and releasing the latches on the side of the M.2 socket. There is a screw in the center of the board that needs to be removed which holds the WiFi module in place. Also, the 2 Antennas must be attached at this stage.

image

 

Once the Antennas are installed, gentle insert the WiFi module into the M.2 slot on the carrier board and place the WiFi module screw back in place.

 

image

 

NOTE: Hot Glue was used to hold down the wires and on the mounting screw.

image

 

Place the Jetson Nano SoM back into the slot on the Carrier board and screw it back down.

 

PiOLED

To view the assigned IP Address of the board when it first boots, a PiOLED is attached to Pins 1-6 of the J41 Header.  These pins supply the 3.3 v, Ground and SDL and SCL i2C signals for both the PiOLED and the Motor Board. To attached the Motor Board to these signals, a 6 pin right angle head is added to the PiOLED Display.  A word of caution, the PiOLED is a bit fragile so care must be taken when soldering the pins of the right angle header to the PiOLED head pins.  The first attempt here results in a dead PiOLED.   Also, for the second attempt, jumper wires were used instead of a right angle header since the wires from the Motor board block the header for the Heat Sink Fan.

 

PiOLED before right angle header attached.

image

 

PiOLED after Header attached

image

 

PiOLED Mounted to J41 of Jetson Nano

image

 

NOTE: This image shows the Heat Sink Fan header being block by the right angle header on the PiOLED

image

 

NOTE: If the PiOLED is not connected when booting the JetBot with the JetBot image, the following message will continue to appear in the 'dmesg' output.

Address 0x3c is for the PiOLED

 

tegra-i2c 7000c400.i2c: no acknowledge from address 0x3c

 

 

Motor Driver

The Motor Driver is shipped without the headers and screw terminals attached, so these need to be soldered by the individual.

image

 

The 3 pin header is for the 3.3v and Ground connection for controlling the Motor Driver, the Upper Screw Terminal is used for the Motors via the USB Power Bank.

The 2 pin header is for the SDA and SCL i2c signals and the 2 Screw terminals to the left are for the motor connections.  Note the orientation of the connections.

 

image

 

NOTE: The 2 Type A to Micro, right angle USB cables listed in the BOM are not identical.  The Micro USB Connections are mirror opposites so care must be taken to cut the correct one to attach to the Motor Board otherwise the Power connection to the Nano will interfere with the Ethernet port.

Here the Micro USB connection was removed and the Green and White wires were cut back as well as the shielding.  The Red and Black Wires were stripped back so they can be attached to the Motor Board.

 

Mount the Motor Board using 4 M2 self tapping screws and DC Motors to the 3D printed chassis with 4 M3 screws and nuts .   The modified USB cable is connected to the Screw terminal on the Motor Board and route the cable under the Moot Board and out the side of the chassis.  Attach the Motor wires to the Motor Board.

 

image

 

Connect the 4 Jumper wires to the Motor Board as such:

  • Red       - 3.3v
  • Brown   - Ground
  • Orange - SDA
  • Yellow   - SCL  (White was used in place of Yellow)

 

image

 

 

Camera Module

 

To enhance the filed of view of the camera, a Wide Angle Lens module is used to replace the Raspberry Pi Camera v2 Module.

image

 

The Raspberry Pi Camera module can be pealed off and disconnected from the Camera board and the Wide angle module placed and connected in its place.  This can be performed before or after the Camera board is attached to the 3D printed Camera Mount.

 

image

 

Final Assembly

 

Attached the NVIDIA Jetson Nano to the Chassis using 4 M2 screws.

image

 

Attache the Wheels and the Camera Mount on the chassis, and connect the Motor Driver wires to J41 of the Jetson Nano.image

 

Wire connections

  • Red       - 3.3v
  • Brown   - GND
  • Orange - SDA
  • Yellow   - SCL  (White was used in place of Yellow)

Image from:

https://www.jetsonhacks.com/nvidia-jetson-nano-j41-header-pinout/

 

image

Camera Mount

image

 

Peal the paper from the adhesive Antenna Film and attach one to the underside of the top part of the chassis and the other to the lower part.

Note: It is best to ensure these are as close to the side of the chassis as possible so as to not interfere with the Power Bank placement.

 

Lower attachment

image

 

Upper attachment

image

 

Remove the Power Bank from its protective sleeve and either place double sided adhesive or, in this case, Velcro to the Power Bank so it will hold in place in the chassis..

image

 

 

Slip the Power Bank into the chassis ensuring the 2 USB connections are on the end that aligns with the P41 header of the Jetson Nano. Route the Jetson Nano cable around the Caster Base under the chassis.

image

 

The connections to the Power Bank should like like the following

image

 

NOTE: Since the PiOLED was killed in the header placement, thus it is not attached at this time.

 

The End result of the JetBot assemble in this instance is as follows.

image

 

Face to face with a Parallax cyber:bot with Shield Bot Chassis, the JetBot is quite similar in size to the Parallax Bot.

Interesting, the NVIDIA Jetson Nano JetBot came in at around $250 US and the Parallax Shield Bot with cyber:bot Board, micro:bit board and rechargeable batteries was around  $241 US (or $200 as a complete kit without batteries). However, in the case of the Parallax Bot, the Chassis is provided where the JetBot must be 3d printed or completed by a 3D printing service.

 

 

image

 

JetBot Example Video

In the following Video, the Assembled JetBot is shown as well as a walk through of the Basic Motion Jupyter Notebook that is hosted on the JetBot.  This example shows how to control the JetBot from Python.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • kiri-ll
    kiri-ll over 7 years ago +4
    The machine looks great! I always wanted to see how the training of AI looks like, so I am very curious how this your project will go!
  • jomoenginer
    jomoenginer over 7 years ago in reply to 14rhb +4
    Rod, Thanks. The 3D printer I have is a xyz da Vinci Mini (The orange one) which I picked up for less than $200.00 US. There is an updated one now but I am not sure how well that one performs. The one…
  • 14rhb
    14rhb over 7 years ago +3
    Hi Jon, This is a very well presented build blog which I am really enjoying reading, thank you for taking the time to photograph and write up all the steps. Your 3D printed parts are also very professional…
  • ralphjy
    ralphjy over 7 years ago

    Great progress.  Nice video.  I’m impressed by how comprehensive the documentation is, although you did mention some of it didn’t workimage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to dubbie

    I am not sure where you are located, but you might want to look in your locale to see if there are any Maker Groups or Labs or even a local college or public library that may have 3D Printers you could use.

     

    There is a 3D printing page in the JetBot WiKi where they list possible sources to have the chassis and such 3D printed for you.  There is a cost though.

    https://github.com/NVIDIA-AI-IOT/jetbot/wiki/3d-printing

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    Very nice project!  This is coming along very nicely.  I really like your 3D printed chassis. Nice video demonstration of your robotic movements.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago

    A good build. I wish I could print the chassis.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to kiri-ll

    I've gone through the Collision Avoidance Example where you have to Collect Data on the JetBot via the camera and then go through a Train neural network exercise to run a Live Demo, but there were some issues with some of the instructions in the example so I'll have to go through the process again.  I've posted a few Bug reports on their GitHub repo to correct some of these though. The exercise is a bit involved so it needs a good bit of time to get trough it.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>