Month of Robots
  • Challenges & Projects
  • Project14
  • Month of Robots
  • More
  • Cancel
Month of Robots
Blog NVIDIA Jetson Nano: JetBot Intro
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Month of Robots to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jomoenginer
  • Date Created: 23 Apr 2019 8:33 AM Date Created
  • Views 5123 views
  • Likes 14 likes
  • Comments 18 comments
  • nvidia jetson nano
  • robotics
  • jetbot
  • robot
  • morobotsch
Related
Recommended

NVIDIA Jetson Nano: JetBot Intro

jomoenginer
jomoenginer
23 Apr 2019
image

Month of Robots

Enter Your Project for a chance to win robot prizes for your robot builds and a $200 shopping cart!  The Birthday Special: Robot Prizes for Robot Projects!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Overview

 

It took a bit, but I was able to finally gather the bits and pieces to get started on my version of the NVIDIA Jetson Nano JetBot.  The JetBot is an Mobile Robot Platform that uses the NVIDIA Jetson Nano for its compute power for AI-powered deep learning autonomous navigation.  The Jetson Nano is the latest Single Board computer, or rather System-on-Module in the Jetson line by NVIDIA.   The Nano is a more affordable System at $99 US where the Jetson TX2 runs $299 - $749 and the Jetson AGX Xavier at $1,099, although the Nano does have a scaled down set of features.

 

Related posts

NVIDIA Jetson Nano

https://www.element14.com/community/people/jomoenginer/blog/2019/04/28/nvidia-jetson-nano-jetbot-assemble

https://www.element14.com/community/people/jomoenginer/blog/2019/05/14/nvidia-jetson-nano-collision-avoidance

 

NVIDIA Jetson Nano Developers Blog

https://devblogs.nvidia.com/jetson-nano-ai-computing/

 

NVIDIA Jetson Nano Getting Started Guide

https://developer.nvidia.com/embedded/learn/get-started-jetson-nano-devkit#write

 

 

NANO Specs

https://www.nvidia.com/en-us/autonomous-machines/embedded-systems/

FeatureDetails
GPUNVIDIA MaxwellTm architecture with 128 NVIDIA CUDARegistered cores
CPUQuad-core ARMRegistered CortexRegistered-A57 MPCore processor
Memory4 GB 64-bit LPDDR4
Storage16 GB eMMC 5.1
Video Encode4K @ 30 (H.264/H.265)

Video Decode

4K @ 60

(H.264/H.265)

ConnectivityWi-Fi requires external chip
Camera12 lanes (3x4 or 4x2) MIPI CSI-2, DPHY 1.1 (1.5 Gbps)
Size69.6 mm x 45 mm
Mechanical260-pin edge connector

 

JetBot WiKi

https://github.com/NVIDIA-AI-IOT/jetbot/wiki

 

 

BOM

 

PartDescription
BrainNVIDIA Jetson Nano
Motors2 X Adafruit DC Gearbox Motor -"TT Motor" - 200RPM - 3 to 6VDC (3777)
Motor DriverDC Motor + Stepper FeatherWing Add-on Motor Driver
BatteryINIU 10000 mAh Portable Power Bank LED Display Ultra Compact 2 USB Ports Mobile Charger External Battery Backup Powerbank
uSD CardSamsung 64GB 100MB/s (U3) MicroSD EVO Select Memory Card
USB cableType A to Micro, right angle
Caster Ball1" Inch Delrin Plastic Ball Bearings G1-1 Bearings
WiFi/BTIntel Dual Band Wireless-Ac 8265 W/Bt
CameraRaspberry Pi Camera Module V2-8 Megapixel,1080p
Camera LensWaveshare IMX219 Camera Module for The Official Raspberry Pi Camera Board V2 8MP Sensor 160 Degree FoV
Antenna2 X Molex Antenna Wi-Fi 3.3dBi Gain 2483.5MHz/5850MHz Film
Wheels2 X Thin White Wheel for TT DC Gearbox Motors - 65mm Diameter
OLEDAdafruit PiOLED - 128x32 Monochrome OLED Add-on for Raspberry Pi
Chassis3D Printed
Camera Mount3D Printed
Caster Base3d Printed
Caster Shroud3D Printed

 

JetBot Software Image

https://github.com/NVIDIA-AI-IOT/jetbot/wiki/software-setup

 

  NOTE: Image is 64GB and may need a 128GB Micro SD card

 

  1.  Download the JetBot SD Card image from the software-setup link posted previously.

       The image used in this example is:

       jetbot_image_v0p3p0.zip

  2.  Etcher was used to Load the Image on the SD card in this example.

       NOTE: For uSD cards 64GB or above, the card must be formatted for ExFAT

       a.  On Linux, use mkfs-exfat

       b. If not already installed, in the case of Ubuntu, use apt-get to install the required package

$sudo apt-get install exfat-fuse exfat-utils

 

 

      c. Format the SD card

$ sudo mkfs.exfat -n sdxc64 /dev/sdh
mkexfatfs 1.2.3
Creating... done.
Flushing... done.
File system created successfully.

 

     d. Launch Etcher and select the image to install

image

 

     e. A SD card 64GB or greater will not show automatically in Etcher, so it is necessary to click on Select Drive to select the SD card

  image

 

     f.  Once the card is selected, click Flash to copy the image to the SD card.

image

 

    NOTE: A Warning may appear regarding the size of the image.  Just click Continue

image

     g.  If performed on Ubuntu using Etcher, it is necessary to launch GParted to allocate the allocate space on the SD card.  Otherwise the Nano will not boot.

         Click Fix to complete the process.

 

     h.  Once the GParted process is complete. close the application and safely eject the SD card and insert it back into the Nano

 

 

JetBot Hardware

   The JetBot Hardware listed in the Bill of Materials is sourced from multiple online sources, however some items may not be available. Considering the JetBot image is hardware specific, it is best to sick with what is listed in the BOM or a fair equivalent. In some cases, there are multiple options for a particular item, such as the wheels where the wider and white rimmed wheels were chosen in this instance rather than the skinnier black wheels.  The type of Micro SD card seems to be important to align with the JetBot image size.

image

NVIDIA Jetson Nano

image

 

Chassis

  The JetBot Chassis, Camera Mount, Caster Mount and Caster Shroud were printed on a XYZ da Vinci Mini 3d Printer.

   A 3D printed gripper was added for future use.

 

image

 

   Chassis with Caster attached

image

 

 

 

Wheels and Motor Driver

   The BOM calls out the Adafruit DC Motor + Stepper FeatherWing Add-on Motor Driver which has mounting holes that align with it on the 3D printed chassis.  The motors are standard Hobby Geared DC Motors from Adafruit rated at 200 rpm. The Wheels are Thin White Wheel for TT DC Gearbox Motors that attach to the DC Motors,

image

 

  OLED Display

    The OLED Display is a tiny Adafruit PiOLED that is used to display the system IP Address and related data at boot and during operation.

image

 

Camera and Camera Lens

   The Camera is a Raspberry Pi Camera V2 that will have its camera module replaced with a Waveshare IMX219 Camera Module for 160 Degree Field of View

image

 

WiFi and Antenna

   The WiFi module is a M.2 Intel Dual Band Wireless-Ac 8265 W/Bt that attaches to the carrier board for both WiFi and Bluetooth 4.2 support. There will be 2 Molex Wi-Fi 3.3dBi Gain 2483.5MHz/5850MHz Film Antenna attached to extend the WiFi range.

image

 

 

With the hardware in hand and the 3D printer parts completed, its time to assemble the JetBot which will be covered in the next post.

  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 7 years ago +7
    Very nice. I’m impressed that you got all the parts together so quickly. How much space do you have left on the SD card? Looking forward to see it running. Ralph
  • fmilburn
    fmilburn over 7 years ago +7
    Have to like robots :-). i like the detail you are providing as I have been tempted by this device. As you progress, your thoughts on how well suited it is to someone unfamiliar with AI would be appreciated…
  • shabaz
    shabaz over 7 years ago +6
    Very interesting! It looks like a fun project to get up-to-speed with using the Nano. Also I didn't realize that the Pi camera was usable with the Jetson Nano, that's very cool.
Parents
  • dubbie
    dubbie over 7 years ago

    Just downloaded the STL file foro the jetbot chassis and loaded it into my 3D printer. Regretfully it is about 1 cm too long so I am just not able to print it. Shame, as it looked like a good chassis. I might have to try making something myself that is similar, but smaller. Although I'm not sure TinkerCAD is up to this level of complexity.

     

    Dubbie

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 7 years ago in reply to dubbie

    Hello Dubbie,

     

    I haven't tried TinkerCAD yet, but I can recommend you Fusion360, is becoming more and more popular, there is a free option for makers, updated regularly (maintenance and new features), supports parametric designs and there is a lot of education going on YouTube from users and Autodesk itself.

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to luislabmo

    Luis,

     

    Thanks for this. I did try AutoCAD many years ago plus another called something like 3D something or other, but I just don't seem to be able to get the hang of them. Not sure why, an increasingly solidified brain I expect. I can understand TinkerCAD and how it works.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago in reply to luislabmo

    Luis,

     

    Thanks for this. I did try AutoCAD many years ago plus another called something like 3D something or other, but I just don't seem to be able to get the hang of them. Not sure why, an increasingly solidified brain I expect. I can understand TinkerCAD and how it works.

     

    Dubbie