Movers and Shakers
  • Challenges & Projects
  • Project14
  • Movers and Shakers
  • More
  • Cancel
Movers and Shakers
Blog Walky the Biped Robot - WalkyII gets his legs
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Movers and Shakers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 14 Jul 2018 9:06 PM Date Created
  • Views 2726 views
  • Likes 14 likes
  • Comments 8 comments
  • 3d pritning
  • robotics
  • moversshakersch
  • 3d design
Related
Recommended

Walky the Biped Robot - WalkyII gets his legs

genebren
genebren
14 Jul 2018
image

Movers and Shakers

Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Previous post in the sequence:

Walky the Biped Robot - The prequel

Walky the Biped Robot - Power pack

Walky the Biped Robot - Oops, Walky has an accident!

Walky the Biped Robot - A new hope (actually a new body and battery)

Walky the Biped Robot - WalkyII gets some eyes.

 

Today the 3D printathon has ended.  I finally have some peace and quiet at my desk.  At 2:00 PM, the final piece of WalkyII was printed (final for now?).  After a bit of assembly, WalkyII can now stand on his own.  Things went pretty well.  I needed to clean-up a few holes, tighten this, loosen that...... But in the end, it looks exactly like what I planned.

imageimageimage

Once I assembled him, I decided to see how well he could walk.  I powered the 'original' controller board from the new power pack and hit the switch.  WalkyII did not do too well.  He toddled around like a drunken sailor and would tip over after each step (if not for my helping hand).  I appears that the center of gravity has shifted a bit from the original Walky.  Also some of the joints were a little loose, mostly the 'ankles'.  I did a little rework on the 'ankles' and adjusted the servo linkages a bit to shift feet a little further back.  I also adjusted the front linkages to get the feet a little flatter to the table (the above pictures are post reworks).  I still need to do something to move the feet a little further apart, maybe a slider positioned between the legs and the body, along the bottom edge, to spread the legs out a bit.

 

I did capture a few short clips of WalkyII walking.  While he is not exactly graceful, he can now toddle about without falling over.  I will need to fine tune his gait some, as he has a tendency to walk in circles.  This is all stuff that I can address when I start coding his new controller board.
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
Here are some of the 3D views of his legs, feet and ankles:

imageimageimageimage

All of the pivot points on the legs are done using pressed in nylon shoulder spacer, in an attempt to have a free movement with a minimal amount of wobble.  The majority of the hardware to bolt everything together is 2-56 screws.  On the pivoting leg joints I used nylock nuts to lock the nuts on, without over tightening the joint.

 

So far, so good.  But I do see a lot of work coming up writing the firmware for the controller and finishing up the firmware on the power pack.  (not to mention that I am currently juggling three consulting gigs).

 

Thanks for reading along.  More to come.

Gene

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago in reply to genebren +6
    Hi Gene, What you describe is a principal that I have come to accept as a factor in all repairs and modifications that I make to devices. Always expect and try to anticipate the side effects of any change…
  • jw0752
    jw0752 over 8 years ago +5
    I think he looks pretty good. He almost has to sway to lift the leg that is moving. What would he look like with a rubber sole on his feet? John
  • mcb1
    mcb1 over 8 years ago +5
    I've seen people walking like that ... in the same manner as jw0752 suggests. I wonder if a small rubber strip on the rear edge is enough. It seems the walking motion is to lift the front edge, and then…
Parents
  • three-phase
    three-phase over 8 years ago

    Good to see the progress bing made, I a sure you will make the required improvements in due course.

     

    Kind regards

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 8 years ago

    Good to see the progress bing made, I a sure you will make the required improvements in due course.

     

    Kind regards

    • Cancel
    • Vote Up +5 Vote Down