Movers and Shakers
  • Challenges & Projects
  • Project14
  • Movers and Shakers
  • More
  • Cancel
Movers and Shakers
Blog Walky the Biped Robot - WalkyII is learning to walk again!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Movers and Shakers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: genebren
  • Date Created: 10 Aug 2018 10:52 PM Date Created
  • Views 2109 views
  • Likes 12 likes
  • Comments 6 comments
  • robotics
  • moversshakersch
  • project14
Related
Recommended

Walky the Biped Robot - WalkyII is learning to walk again!

genebren
genebren
10 Aug 2018
image

Movers and Shakers

Enter Your Electronics & Design Project for Your Chance to Win a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Previous post in the sequence:

Walky the Biped Robot - The prequel

Walky the Biped Robot - Power pack

Walky the Biped Robot - Oops, Walky has an accident!

Walky the Biped Robot - A new hope (actually a new body and battery)

Walky the Biped Robot - WalkyII gets some eyes.

Walky the Biped Robot - WalkyII gets his legs

Walky the Biped Robot - WalkyII gets a new brain

 

As I start typing this, WalkyII is recharging his battery.  After a long debug session, WalkyII started getting wacky.  If I started to command the servos, WalkyII's status LEDs would start flashing erratically and then stall mid step.  So it was time to take a break and give WalkyII a little recharge time.  Here is some of his recent photos/videos:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
imageimage

So far, I  have integrated the R/C receiver and front and rear sensors.  WalkyII currently understands the simple commands of Forward and Reverse, with a speed modifier.  Senor wise, WalkyII is using his front and rear I/R distance sensors to avoid table edges and obstacles (he will not start walking if something is in the way and he will stop if something gets in his way while working.

 

Update:  Oops the erratic LED flashes turned out to be a glitch in WalkyII object/edge detection logic (not a near dead battery).  I needed to hold the object/edge detected flag set until the R/C command went back to idle, otherwise WalkyII kept entering and exiting the walking routine.

 

Programming and debugging WalkyII takes a little support and a lot of tools.  Here are some of the tools that I use to teach WalkyII some of his stuff:

image

 

Here WalkyII all connected during a debug session.  The 'red' circle shows the AVR ISP MKII programmer that is attached to WalkyII.  This allows me to 'burn' new firmware, view/modify EEPROM (holding configuration data) and issue a reset, should things go astray.  Below that (in a 'blue' circle) is a old project (IR motion detect/Light switch), that has been re-purposed into a USB to serial bridge.  I used the bridge to send and receive serial commands, used to exercise WalkyII's low level commands or to read/modify variables.  In the background (green circle) is WalkyII friend, who helps out with all the complex math that helps WalkyII to walk.

 

I had also fabricated a sling, that allows WalkyII to be suspended while exercising WalkyII's servos without him flopping all over the desk or toddling off the edge (before his sensors were active.

 

Up next is WalkyII's debug panel.

 

 

 

 

 

 

 

 

 

image

 

The debug control panel allows me to interact with WalkyII's program without interfering with the generation of PWM waveforms and interrupt driven pulse measurements.  From the panel I can control/view the following:

1) set servo positioning pulses on all channels.

2) read I/R distance readings (live, baseline averages, and limit values for obstacle/edge avoidance).

3) read PWM pulse width from the R/C receiver and the command determined from these values.

4) read and modify WalkyII step parameters (Tilt and Stride)

5) Enable override of WalkyII servo settings (as well as filter rate variables)

6) Write current servo positions to default positions (to EEPROM).  This was used to trim out the WalkyII's servo positions.

7) View all data sent/received to/from WalkyII

 

(Note: Oops!, there is some left over startup commands being sent to Walky, which he ignores.  This panel was hacked together from a previous job, or two).

 

 

 

 

 

 

 

One issue that I am still working on is the fact that WalkyII walks like a drunken sailor (not there is anything wrong with that).  I have tried several things to help WalkyII walk the straight and narrow, but so far we are not there yet.  there were several recommendations early on, improvements to WalkyII's feet that might help, thanks jw0752 , mcb1 , ntewinkel and balearicdynamics for the ideas.  So far, I have tried a couple of different pads on WalkyII's soles, but still he is quite wobbly.  Here is WalkyII's latest footwear:

 

image

The black pads are textured vinyl.  They help a little in preventing him from slipping, but I think that he is getting caught up in the side to side momentum of the tilt phase of his gait and generates a bit of a pivot.  I have filtered out some of the fast slew out of the servos, but I think I will need to try a ramp-up, constant velocity and ramp-down servo profile to calm down some of the violent swings to his gait. Also, during testing, WalkyII broke one of his short, lower control rods that drive the stride portion of his gait.  The new control rods that I built, don't move quite as smoothly as the old ones (some binding and such).  I will need to investigate a new lower control arm set (to bad I could not re-solder the brass control arms, darn lead-free solder would not stick, or maybe I should braze it???).

 

Time is getting late, as the deadline is approaching.  I still need to finish up a few thing and produce the remaining documentation, so a couple of my initial goals (like I2C communication to the battery pack to get battery voltage, get mode setting, and perform remote shutdown on inactivity), might fall to side and be addressed later.

 

In the meantime, dinner and a cold beer.....

 

Thanks for following along on this crazy adventure.

Gene

  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 8 years ago +2
    Great progress! > One issue that I am still working on is the fact that WalkyII walks like a drunken sailor I say embrace it and give him a pirate's hat and parrot.
  • jw0752
    jw0752 over 8 years ago +1
    Hi Gene, Have you experimented with only one or two pads on each foot at different corners? John
  • balearicdynamics
    balearicdynamics over 8 years ago +1
    Hi Gene! Thank you for the video, I experienced a small delusion as seeing the video I was expecting to see the guy walking but nothing. To be honest, I think you can also show the not yet perfect milestones…
Parents
  • ntewinkel
    ntewinkel over 8 years ago

    Great progress!

     

    >One issue that I am still working on is the fact that WalkyII walks like a drunken sailor

    I say embrace it and give him a pirate's hat and parrot.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 8 years ago

    Great progress!

     

    >One issue that I am still working on is the fact that WalkyII walks like a drunken sailor

    I say embrace it and give him a pirate's hat and parrot.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to ntewinkel

    Nico,

     

    Thanks!  I think an eye patch would be cool too! Oh, wait that would defeat the I/R sensor.

     

    Gene