NanoRama
  • Challenges & Projects
  • Project14
  • NanoRama
  • More
  • Cancel
NanoRama
Blog TOF Sensor mounted on Laser
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NanoRama to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 25 Apr 2020 8:52 PM Date Created
  • Views 1827 views
  • Likes 6 likes
  • Comments 3 comments
  • nanoramach
Related
Recommended

TOF Sensor mounted on Laser

ralphjy
ralphjy
25 Apr 2020
image

NanoRama

Enter Your Project for a chance to win a Nano Grand Prize bundle for the most innovative use of Arduino plus a $400 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

The next step in my project is to print a mounting fixture for the micro-LIDAR TOF sensor.  I wanted to position the sensor lens in approximately the same plane as the laser lens.  Any small discrepancies will be corrected when I calibrate the offset.

 

The shroud has a press fix onto the spindle/laser mount.  The lower shelf holds the VL6180X and I picked standoffs of the appropriate length to adjust the sensor lens position.

image

 

Bottom view (the addition hole position allows me to mount the VL53L0X).

image

 

While I am prototyping I am just going to mount the solderless breadboard into the upper cavity.  This allows me to continue using the USB programmer.

image

 

The assembly with sensor connections.

image

 

Mounted on the spindle/laser holder.

image

 

When I am done testing I will remove the USB programmer and mount the MicroView in a socket on a small proto PCB.  I'll wire the power and ground from the GRBL controller.  I also need to add the wire to the z-limit input of the GRBL controller.

 

The next step is to do the performance testing with the VL6180X using the averaging program.  I decided to combine a few of the steps from the previous blog and just do all the integration/testing on the cnc/laser machine as I'll need to get wired to the GRBL controller and it's probably better to do the testing in the use environment.

  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 6 years ago in reply to dubbie +1
    This method doesn't have the accuracy/repeatability required for 3D printing or CNC. I find that I adjust my bed infrequently when 3D printing and for CNC the tool variations require me to manually adjust…
Parents
  • dubbie
    dubbie over 6 years ago

    It would seem to be a good idea to do the calibration testing on the real CNC/Laser hardware to get the most accurate environmental conditions. It will be interesting to see if the 3D printed part has any shrinkage/expansion effect over time which affects calibration over time. I use aBS which I think absorbs water over time so I assume that ABS will expand gradually.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 6 years ago in reply to dubbie

    This method doesn't have the accuracy/repeatability required for 3D printing or CNC.  I find that I adjust my bed infrequently when 3D printing and for CNC the tool variations require me to manually adjust.  The laser is a lot more forgiving in focus tolerance and I need to refocus frequently whenever I change material thickness (anywhere from thin cardstock up to about 1/2").  So I'm hoping that this will work for the laser.

     

    Ralph

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 6 years ago in reply to dubbie

    This method doesn't have the accuracy/repeatability required for 3D printing or CNC.  I find that I adjust my bed infrequently when 3D printing and for CNC the tool variations require me to manually adjust.  The laser is a lot more forgiving in focus tolerance and I need to refocus frequently whenever I change material thickness (anywhere from thin cardstock up to about 1/2").  So I'm hoping that this will work for the laser.

     

    Ralph