Open Arduino
  • Challenges & Projects
  • Project14
  • Open Arduino
  • More
  • Cancel
Open Arduino
Blog ArduTrx - a 2-meter-band ham radio transceiver with Arduino
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bernhardmayer
  • Date Created: 12 May 2018 9:45 PM Date Created
  • Views 23245 views
  • Likes 17 likes
  • Comments 18 comments
  • arduinoday18
  • arduino uno
  • ardutrx
  • arduino_leonardo
  • transceiver module
  • arduino_classic
  • openarduinoch
  • arduino
  • ham radio
Related
Recommended

ArduTrx - a 2-meter-band ham radio transceiver with Arduino

bernhardmayer
bernhardmayer
12 May 2018

ArduTrx is a 2-meter-band ham radio transceiver which uses an Arduino as precessor board. I made a Arduino shield with the Dorji DRA818V transceiver module (http://www.dorji.com/docs/data/DRA818V.pdf). Together with an Arduino board and a SainSmart LCD Keypad Shield (https://www.sainsmart.com/products/lcd-keypad-shield-for-arduino-duemilanove-uno-mega2560-mega1280 ) you can build a complete ham radio transceiver and start communicating. This project does not only give some basic functions to communicate with the DRA818V, it moreover has all the fuctions for a completly usable transceiver.

image

 

Features

  • Frequency Range: 134 MHz - 174 Mhz (maybe limited to ham radio bands by software)
  • frequency selection with encoder
  • 1750 Hz tone for repeater operation
  • split rx and tx frequency for repeater operation
  • CTCSS via menu
  • Squelch and volume can be set via display keys
  • Transmit power swtchable from 0.5W to 1W
  • frequency scan
  • all settings are stored in eeprom and recalled after reset

image

 

Planned features

  • support for the UHF version Dorji DRA818U (400 - 470 MHz)
  • DTMF signaling

 

Compatibility

The ArduTrx shield should be compatible with all 5V Arduinos. Compatibility was explicitly tested with Arduino Uno and Arduino Leonardo.

A version also compatible with 3.3V Arduinos is planed.

image

 

Source code

You can find the source code on github: https://github.com/generationmake/ArduTrx

 

Schematics

Here is a link to the schematics: http://blog.generationmake.de/file_download/1/dra-shield.pdf

 

Update March 17, 2019:

 

Project Website

You can find all documents, schematics, links to software and documentation on my project website:

ArduTrx - Open Source Hamradio Transceiver for Arduino

  • Sign in to reply

Top Comments

  • bernhardmayer
    bernhardmayer over 8 years ago in reply to jc2048 +6
    Hi Jon, the DRA818 modules have some problems with the harmonics. So I decided to implement a low pass filter to get rid of them. The filter is a chebyshev low pass with the following parameters: cutoff…
  • heathsmith
    heathsmith over 8 years ago +2
    This is awesome. CW features pretty please!!!!
  • mcb1
    mcb1 over 8 years ago +2
    You may wish to delete the email once it's been done ... You can try sending this sort of information via a PM (Personal message) . It does require the other party to accept your request, but that's easy…
Parents
  • anthonygainsborough
    anthonygainsborough over 6 years ago

    Enjoyed your writeup of this project.

     

    I am also using the DRA818v modules but unable to switch to wideband (firmware issue apparently). Does your module allow wideband mode?

     

    Thanks johnG

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • anthonygainsborough
    anthonygainsborough over 6 years ago

    Enjoyed your writeup of this project.

     

    I am also using the DRA818v modules but unable to switch to wideband (firmware issue apparently). Does your module allow wideband mode?

     

    Thanks johnG