Open Arduino
  • Challenges & Projects
  • Project14
  • Open Arduino
  • More
  • Cancel
Open Arduino
Blog Cyber Chicklet
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 4 May 2018 4:14 AM Date Created
  • Views 4478 views
  • Likes 20 likes
  • Comments 11 comments
  • doug wong
  • ardintermediate
  • caddy hack
  • cyber chicklet
  • arduino_classic
  • ultra precise mouse movement
  • Arduino Day
  • destiny button
  • arduino pro micro
  • openarduinoch
  • perpetuity paradox
  • anduino hid
  • hid conglomerate
Related
Recommended

Cyber Chicklet

dougw
dougw
4 May 2018

The Cyber Chicklet is a mystery device - see how long it takes you to figure out its purpose as you watch the video....

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I am making a blog in honor of arduino day and project14 and element14.

image

This blog is about some arduino applications that tie in to element14.

The next video is about a Destiny Button implemented on a custom PCB.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This video is simply - Happy arduino day!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I have designed a PCB that I call the HID Conglomerate that can perform all the above functions.

image

image

I have been holding off publishing this blog for over a month while waiting for the PCB to arrive.

Unfortunately it has not arrived yet, so I am publishing anyway. The PCB was fabricated over a month ago and I paid extra to have it air mailed here. Apparently it has been in the air for over a month. Canada Post has decided to no longer honor the tracking number systems of other countries, so I can only tell that it left the other country. It is taking longer than if I did not pay for faster delivery. (regular mail) This is the second project in a row that is all messed up by slow PCB mail.

This card can perform any HID function and it has an LCD to display useful information. I can describe a couple of functions I was(am) planning to implement in addition to the examples above:

  • The Volume Commander - my Windows 10 computer is notorious for totally ignoring the volume icon in the tray and the keyboard shortcut makes volume changes in increments of 2, so the HID conglomerate would allow fine control of audio volume without needing the tray icon.
  • The Browser Navigator - my computer at work has a mouse with no "Back" button so the HID Conglomerate would implement a function to go back to the previous browser page (or forward).
  • The Copy Cat - when I am doing a lot of cut and paste, single buttons to perform these functions would be handy.
  • The Caddie Hack - I want to implement precise single pixel mouse moves for my CAD systems and my drawing packages. I am a perfectionist when it comes to graphics and CAD drawings, and moving the mouse accurately to a single pixel can be very tedious. This functionality is going to be worth the price of admission by saving significant time performing accurate mouse movements. Note it can be used at the same time as the real mouse - so one device in each hand works well.
  • The Perpetuity Paradox - this is the original name for the Cyber Chicklet
  • The Destiny Button - described above was really an experiment to see if I could make the mouse fly. I actually wrote a little program that could "handwrite" "Happy arduino day" in a drawing package, but I gave up after writing "Happy" - it was just too tedious. It should be noted that mouse movement is not linear so it is really easy for it to lose track of where the arduino thinks the mouse is.

Update:

The PCBs finally arrived after spending over 6 weeks in air mail limbo, so I got to finish off the project. The finished project photo is added at the top of the blog.

The images below show what is in the module. Note that there are unused connectors that may be used for other projects and applications - because I ordered 10 of these cards (about $1 each).

imageimageHere is a little video of the result:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here is the Cyber Chicklet code:

//Cyber Chicklet
//by Doug Wong
#include <Mouse.h>


void setup(void)
{
  Mouse.begin();
}


void loop()
{ 
    Mouse.move(0, 0, 0);  // move mouse 0 pixels
    delay(120000);        // wait 2 minutes
}

 

Here is a program for the Destiny Button:

//
//Destiny Project
//by Doug Wong
//#include <dht11.h>
#include <Mouse.h>
#include <Keyboard.h>
#define DHT11PIN 20   
#define PIN_SCE   6
#define PIN_RESET 7
#define PIN_DC    8
#define PIN_SDIN  16
#define PIN_SCLK  15
#define PIN_BL  9


#define LCD_C     LOW
#define LCD_D     HIGH


#define LCD_X     84  
#define LCD_Y     48


const int led1 = 17;
const int E14button = 4;
const int Rbutton = 5;
const int Lbutton = 10;
const int Ubutton = 18;
const int Dbutton = 19;


int movx = -400;
int movxx = 50;
int movy = -400;
int movyy = 50;
int movcount = 0;


static const byte ASCII[][5] =
{
 {0x00, 0x00, 0x00, 0x00, 0x00} // 20  
,{0x00, 0x00, 0x5f, 0x00, 0x00} // 21 !
,{0x00, 0x07, 0x00, 0x07, 0x00} // 22 "
,{0x14, 0x7f, 0x14, 0x7f, 0x14} // 23 #
,{0x24, 0x2a, 0x7f, 0x2a, 0x12} // 24 $
,{0x23, 0x13, 0x08, 0x64, 0x62} // 25 %
,{0x36, 0x49, 0x55, 0x22, 0x50} // 26 &
,{0x00, 0x05, 0x03, 0x00, 0x00} // 27 '
,{0x00, 0x1c, 0x22, 0x41, 0x00} // 28 (
,{0x00, 0x41, 0x22, 0x1c, 0x00} // 29 )
,{0x14, 0x08, 0x3e, 0x08, 0x14} // 2a *
,{0x08, 0x08, 0x3e, 0x08, 0x08} // 2b +
,{0x00, 0x50, 0x30, 0x00, 0x00} // 2c ,
,{0x08, 0x08, 0x08, 0x08, 0x08} // 2d -
,{0x00, 0x60, 0x60, 0x00, 0x00} // 2e .
,{0x20, 0x10, 0x08, 0x04, 0x02} // 2f /
,{0x3e, 0x51, 0x49, 0x45, 0x3e} // 30 0
,{0x00, 0x42, 0x7f, 0x40, 0x00} // 31 1
,{0x42, 0x61, 0x51, 0x49, 0x46} // 32 2
,{0x21, 0x41, 0x45, 0x4b, 0x31} // 33 3
,{0x18, 0x14, 0x12, 0x7f, 0x10} // 34 4
,{0x27, 0x45, 0x45, 0x45, 0x39} // 35 5
,{0x3c, 0x4a, 0x49, 0x49, 0x30} // 36 6
,{0x01, 0x71, 0x09, 0x05, 0x03} // 37 7
,{0x36, 0x49, 0x49, 0x49, 0x36} // 38 8
,{0x06, 0x49, 0x49, 0x29, 0x1e} // 39 9
,{0x00, 0x36, 0x36, 0x00, 0x00} // 3a :
,{0x00, 0x56, 0x36, 0x00, 0x00} // 3b ;
,{0x08, 0x14, 0x22, 0x41, 0x00} // 3c <
,{0x14, 0x14, 0x14, 0x14, 0x14} // 3d =
,{0x00, 0x41, 0x22, 0x14, 0x08} // 3e >
,{0x02, 0x01, 0x51, 0x09, 0x06} // 3f ?
,{0x32, 0x49, 0x79, 0x41, 0x3e} // 40 @
,{0x7e, 0x11, 0x11, 0x11, 0x7e} // 41 A
,{0x7f, 0x49, 0x49, 0x49, 0x36} // 42 B
,{0x3e, 0x41, 0x41, 0x41, 0x22} // 43 C
,{0x7f, 0x41, 0x41, 0x22, 0x1c} // 44 D
,{0x7f, 0x49, 0x49, 0x49, 0x41} // 45 E
,{0x7f, 0x09, 0x09, 0x09, 0x01} // 46 F
,{0x3e, 0x41, 0x49, 0x49, 0x7a} // 47 G
,{0x7f, 0x08, 0x08, 0x08, 0x7f} // 48 H
,{0x00, 0x41, 0x7f, 0x41, 0x00} // 49 I
,{0x20, 0x40, 0x41, 0x3f, 0x01} // 4a J
,{0x7f, 0x08, 0x14, 0x22, 0x41} // 4b K
,{0x7f, 0x40, 0x40, 0x40, 0x40} // 4c L
,{0x7f, 0x02, 0x0c, 0x02, 0x7f} // 4d M
,{0x7f, 0x04, 0x08, 0x10, 0x7f} // 4e N
,{0x3e, 0x41, 0x41, 0x41, 0x3e} // 4f O
,{0x7f, 0x09, 0x09, 0x09, 0x06} // 50 P
,{0x3e, 0x41, 0x51, 0x21, 0x5e} // 51 Q
,{0x7f, 0x09, 0x19, 0x29, 0x46} // 52 R
,{0x46, 0x49, 0x49, 0x49, 0x31} // 53 S
,{0x01, 0x01, 0x7f, 0x01, 0x01} // 54 T
,{0x3f, 0x40, 0x40, 0x40, 0x3f} // 55 U
,{0x1f, 0x20, 0x40, 0x20, 0x1f} // 56 V
,{0x3f, 0x40, 0x38, 0x40, 0x3f} // 57 W
,{0x63, 0x14, 0x08, 0x14, 0x63} // 58 X
,{0x07, 0x08, 0x70, 0x08, 0x07} // 59 Y
,{0x61, 0x51, 0x49, 0x45, 0x43} // 5a Z
,{0x00, 0x7f, 0x41, 0x41, 0x00} // 5b [
,{0x02, 0x04, 0x08, 0x10, 0x20} // 5c ¥
,{0x00, 0x41, 0x41, 0x7f, 0x00} // 5d ]
,{0x04, 0x02, 0x01, 0x02, 0x04} // 5e ^
,{0x40, 0x40, 0x40, 0x40, 0x40} // 5f _
,{0x00, 0x01, 0x02, 0x04, 0x00} // 60 `
,{0x20, 0x54, 0x54, 0x54, 0x78} // 61 a
,{0x7f, 0x48, 0x44, 0x44, 0x38} // 62 b
,{0x38, 0x44, 0x44, 0x44, 0x20} // 63 c
,{0x38, 0x44, 0x44, 0x48, 0x7f} // 64 d
,{0x38, 0x54, 0x54, 0x54, 0x18} // 65 e
,{0x08, 0x7e, 0x09, 0x01, 0x02} // 66 f
,{0x0c, 0x52, 0x52, 0x52, 0x3e} // 67 g
,{0x7f, 0x08, 0x04, 0x04, 0x78} // 68 h
,{0x00, 0x44, 0x7d, 0x40, 0x00} // 69 i
,{0x20, 0x40, 0x44, 0x3d, 0x00} // 6a j 
,{0x7f, 0x10, 0x28, 0x44, 0x00} // 6b k
,{0x00, 0x41, 0x7f, 0x40, 0x00} // 6c l
,{0x7c, 0x04, 0x18, 0x04, 0x78} // 6d m
,{0x7c, 0x08, 0x04, 0x04, 0x78} // 6e n
,{0x38, 0x44, 0x44, 0x44, 0x38} // 6f o
,{0x7c, 0x14, 0x14, 0x14, 0x08} // 70 p
,{0x08, 0x14, 0x14, 0x18, 0x7c} // 71 q
,{0x7c, 0x08, 0x04, 0x04, 0x08} // 72 r
,{0x48, 0x54, 0x54, 0x54, 0x20} // 73 s
,{0x04, 0x3f, 0x44, 0x40, 0x20} // 74 t
,{0x3c, 0x40, 0x40, 0x20, 0x7c} // 75 u
,{0x1c, 0x20, 0x40, 0x20, 0x1c} // 76 v
,{0x3c, 0x40, 0x30, 0x40, 0x3c} // 77 w
,{0x44, 0x28, 0x10, 0x28, 0x44} // 78 x
,{0x0c, 0x50, 0x50, 0x50, 0x3c} // 79 y
,{0x44, 0x64, 0x54, 0x4c, 0x44} // 7a z
,{0x00, 0x08, 0x36, 0x41, 0x00} // 7b {
,{0x00, 0x00, 0x7f, 0x00, 0x00} // 7c |
,{0x00, 0x41, 0x36, 0x08, 0x00} // 7d }
,{0x10, 0x08, 0x08, 0x10, 0x08} // 7e ←
,{0x78, 0x46, 0x41, 0x46, 0x78} // 7f →
};


void LcdCharacter(char character)
{
  LcdWrite(LCD_D, 0x00);
  for (int index = 0; index < 5; index++)
  {
    LcdWrite(LCD_D, ASCII[character - 0x20][index]);
  }
  LcdWrite(LCD_D, 0x00);
}


void LcdClear(void)
{
  for (int index = 0; index < LCD_X * LCD_Y / 8; index++)
  {
    LcdWrite(LCD_D, 0x00);
  }
}


void LcdInitialise(void)
{
  pinMode(PIN_SCE, OUTPUT);
  pinMode(PIN_RESET, OUTPUT);
  pinMode(PIN_DC, OUTPUT);
  pinMode(PIN_SDIN, OUTPUT);
  pinMode(PIN_SCLK, OUTPUT);
  digitalWrite(PIN_RESET, LOW);
  digitalWrite(PIN_RESET, HIGH);
  LcdWrite(LCD_C, 0x21 );  // LCD Extended Commands.
  LcdWrite(LCD_C, 0xBA );  // Set LCD Vop (Contrast). 
  LcdWrite(LCD_C, 0x04 );  // Set Temp coefficent. //0x04
  LcdWrite(LCD_C, 0x14 );  // LCD bias mode 1:48. //0x13
  LcdWrite(LCD_C, 0x20 );  // LCD Basic Commands
  LcdWrite(LCD_C, 0x0C );  // LCD in normal mode.
  pinMode(E14button, INPUT_PULLUP);
  pinMode(Rbutton, INPUT_PULLUP);
  pinMode(Lbutton, INPUT_PULLUP);
  pinMode(Ubutton, INPUT_PULLUP);
  pinMode(Dbutton, INPUT_PULLUP);
}


void LcdString(char *characters)
{
  while (*characters)
  {
    LcdCharacter(*characters++);
  }
}


void LcdWrite(byte dc, byte data)
{
  digitalWrite(PIN_DC, dc);
  digitalWrite(PIN_SCE, LOW);
  shiftOut(PIN_SDIN, PIN_SCLK, MSBFIRST, data);
  digitalWrite(PIN_SCE, HIGH);
}


void setup(void)
{
  LcdInitialise();
  LcdClear();
  LcdString("   ARDUNIO  ");
  LcdString("     HID    ");
  LcdString("            ");
  LcdString("     by     ");
  LcdString(" DOUG WONG  ");
  LcdString("            ");
   
  Keyboard.begin();
  Serial1.begin(19200);
  Mouse.begin();
//  dht11.begin();
}


void loop()
{ 


 if (digitalRead(Lbutton) == LOW)
  {
    Mouse.move(-1, 0, 0);  // move mouse
    delay(10);
    while (digitalRead(Lbutton) == LOW)
    {
      delay(1);
    }
    delay(20);
  }
  
 if (digitalRead(Rbutton) == LOW)
  {
    Mouse.move(1, 0, 0);  // move mouse
    delay(10);
    while (digitalRead(Rbutton) == LOW)
    {
      delay(1);
    }
    delay(20);
  }
  
 if (digitalRead(Ubutton) == LOW)
  {
    Mouse.move(0, -1, 0);  // move mouse
    delay(10);
    while (digitalRead(Ubutton) == LOW)
    {
      delay(1);
    }
    delay(20);
  }
  
 if (digitalRead(Dbutton) == LOW)
  {
    Mouse.move(0, 1, 0);  // move mouse
    delay(10);
    while (digitalRead(Dbutton) == LOW)
    {
      delay(1);
    }
    delay(20);
  }


 if (digitalRead(E14button) == LOW)
  {
  LcdClear();
  LcdString("  ELEMENT14 ");
  LcdString("            ");
  LcdString(" Brought to ");
  LcdString(" you by the ");
  LcdString("  DESTINY   ");
  LcdString("   BUTTON   ");





//    Keyboard.println ("HAPPY BIRTHDAY ARDUINO    ");
//    Keyboard.println ("HAPPY BIRTHDAY PROJECT14  ");
//    Keyboard.println ("HAPPY BIRTHDAY ELEMENT14  ");


    movx = -20;
    movy = 10;
    movcount = 0;
    while (movcount < 70)
    {
    Mouse.move(movx, movy, 0);  // move mouse
    delay(5);
    movcount++;
    }
    movx = 5;
    movy = -13;
    movcount = 0;
    while (movcount < 10)
    {
    Mouse.move(movx, movy, 0);  // move mouse
    delay(5);
    movcount++;
    }


    Mouse.press(MOUSE_LEFT);  // click the left button down
    delay(20);
    Mouse.release(MOUSE_LEFT);  // release the left button
    delay(50);
    Mouse.press(MOUSE_LEFT);  // click the left button down
    delay(20);
    Mouse.release(MOUSE_LEFT);  // release the left button


  }


}

 

The project involved 3D printing 2 small cases and designing a custom PCB.

I actually use these HID devices every day, so it has been a very worthwhile project.

The single pixel mouse moves are very handy and I get a surprising amount of use out of the "element14" button.

The software is pretty simple - if you need it, indicate in the comments below and I'll add it here.

Hopefully these ideas are something you can use and have fun with - they are certainly simple to implement and the arduino only costs about $2.

 

This project was one of the lucky ones to be awarded a runner-up swag package.

image

 

Link to contest page:

Open Arduino

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +6
    I guessed it when it did nothing. I think the same HID is one of the tricks the Digispark does. If I recall there were some questions about whether it would breach company policy ... ie a device that kept…
  • 14rhb
    14rhb over 8 years ago +6
    Hi Douglas, What a fun video and thank you for the entertainment (and simple but useful design). My thoughs went along the lines of: Egg timer? ....but ~10 a day....possibly you cook boiled eggs for a…
  • jw0752
    jw0752 over 8 years ago +5
    Hi Doug, Your projects are so well done that I always enjoy looking at them. Thanks for sharing. I was sorry to hear about the mail delay. There is something very strange going on with the mail service…
Parents
  • dubbie
    dubbie over 5 years ago

    Doug,

     

    Very interesting. I may have to try something like this sometime, especially the 3D printed case as mine are much chunkier,

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 5 years ago

    Doug,

     

    Very interesting. I may have to try something like this sometime, especially the 3D printed case as mine are much chunkier,

     

    Dubbie