Open Arduino
  • Challenges & Projects
  • Project14
  • Open Arduino
  • More
  • Cancel
Open Arduino
Blog Wordclock
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Open Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 12 Apr 2018 8:34 AM Date Created
  • Views 2276 views
  • Likes 16 likes
  • Comments 5 comments
  • clock
  • led strip
  • rtc
  • arduinos
  • openarduinoch
  • acrylic
Related
Recommended

Wordclock

mcb1
mcb1
12 Apr 2018
image

Open Arduino

Enter Your Project for a chance to win a grand prize for the most innovative use of Arduino or a $200 shopping cart! The Birthday Special: Arduino Projects for Arduino Day!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I was asked to look at this some time ago.

http://www.dougswordclocks.com/

image

Doug had created a fantastic project, and it was thought that the readers of TheShed may want to have a go.

A deal was struck and a kit was obtained with the intention of detailing how easy it was to put togther.

 

imageimage

imageimage

 

 

 

 

Hardware

The electronics is based on an Arduino, some latches, RTC and LED strip lights.

These are fitted inside a housing to illuminate the various words that spell out the time.

 

It's a rather simple concept, and often the very clever ideas are simple.

 

The enclosure consists of a number of acrylic strips along with a front panel that has a cut graphic that spells out the words.

The front panel can be customised, and can be any language required, so it's a truly global product.

 

 

 

 

Assembly

I started with the electronics first.

I'm not going to bore you with all the details but here are some of the pictures.

 

  imageimage

It's important when bending diodes to not put any pressure on the body. Use pliers to hold the diode lead and bend against the pliers.

 

 

 

imageimage

When soldering ensure you heat the pcb pad and the wire, and then apply solder to the pcb pad/wire junction.

 

 

image

Eventually you end up with a completed item.

 

 

The enclosure is next.

image

Assemble all 4 sides and tape together so they stay put.

 

I used the LED mounting panel to make sure it was square.

I found using Acrylic solvent and applying with a needle and syringe was far more controllable and easier to get in the right place.

This is a near instant stick, unlike the other glues, so use with caution.

 

There are 7 baffles, which stop the light spilling into the next row.

image

The middle is first and then the others.

 

Use tape to hold them in place, and make sure they are square before gluing.

 

 

 

imageimage

There are inner baffles between the words, and you need to add the LED strips behing each word, so I marked these by illuminating the front panel.

 

 

imageimage

The LEDs get laid out, stuck down and then soldered.

 

 

 

imageimage

Eventually the rear looks something like this

 

 

 

imageimage

Some screw holes to hold the front and rear panels in place, pushbuttons and power, and a means of mounting it on the wall and the enclosure is assembled

 

 

 

Software

Doug has been very generous and made the code Open Source.

He has also provided the schematic and pcb layout.

 

He does ask that you credit him if you're going to change it, which is only fair.

 

I've attached it and the other bits of the information at the bottom.

 

 

 

Video

It's hard to imgine the clock without seeing it in action.

image

 

 

For the video I found a 9v power pack, so that the camera didn't flare out.

I'm adjusting the time setting to show a time sequence ... otherwise it would be a very long or highly sped up video.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

 

 

Large versions

I was amazed when I saw the pictures of this one.

http://www.dougswordclocks.com/wordclocks/wp-content/uploads/2013/01/Brisbane-2.jpg

We tracked down the Brisbane Apartment block it was in, but couldn't get inside to take some photos ... unfortunately.

 

 

 

However I'm thinking a spare wall, CNC router, and it might suit home. image

 

 

In the meantime it is surprising what the humble Arduino can do.

 

 

Mark

 

The guys at Wyolum made a version that had individual leds.

I saw some images but I did manage to grab a copy of the instructions.

Attachments:
imagever3_Schematic.pdf
imageC3jr_Manual (1)-1.pdf
  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +4
    Fun build there. I really do like the clock concept. Given the limited word set, it seems like you could add a voice to the project in addition to the displayed words. Gene
  • mcb1
    mcb1 over 8 years ago in reply to genebren +4
    Given the limited word set, it seems like you could add a voice to the project in addition to the displayed words. You have a month ... best you get cracking then You could, but I won't be. How often do…
  • shabaz
    shabaz over 8 years ago +4
    It is really nice. I love these things. Also a nice opportunity to choose a favorite font, I like the one Doug has picked. Need to build something like this one day : )
Parents
  • genebren
    genebren over 8 years ago

    Fun build there.  I really do like the clock concept.  Given the limited word set, it seems like you could add a voice to the project in addition to the displayed words.

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to genebren

    Given the limited word set, it seems like you could add a voice to the project in addition to the displayed words.

    You have a month ... best you get cracking then image

     

    You could, but I won't be.

    How often do you have it speak the time, ten minutes, half hour, on the hour.?

    Then do you really want something on the wall blabbing out the time all the time.?

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago in reply to mcb1

    Good points.

     

    I am blabbing all the time and I haven't heard any complaints.

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago in reply to mcb1

    Good points.

     

    I am blabbing all the time and I haven't heard any complaints.

    Gene

    • Cancel
    • Vote Up +3 Vote Down