Photography
  • Challenges & Projects
  • Project14
  • Photography
  • More
  • Cancel
Photography
Blog Raspberry Pi HQ View Camera - From the roof to the Moon.
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Photography to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 18 Jul 2021 12:12 PM Date Created
  • Views 6317 views
  • Likes 16 likes
  • Comments 16 comments
  • camera lens
  • photographych
  • raspberry pi 4b
  • photography
  • raspberry pi
  • camera
  • sinar
Related
Recommended

Raspberry Pi HQ View Camera - From the roof to the Moon.

javagoza
javagoza
18 Jul 2021
image

Photography                                               Submit an EntrySubmit an Entry

 

Monthly Themes   | Monthly Poll   |  Back to homepage image

 

Raspberry Pi HQ View Camera

The Raspberry Pi HQ View Camera is a camera with a Raspberry High Quality CameraRaspberry High Quality Camera module and a Raspberry Pi 4BRaspberry Pi 4B attached to an old large-format mono-rail view camera. For now powered by a Raspberry Pi power supplyRaspberry Pi power supply until I find a suitable powerbank to power both the raspberry and the raspberry HQ camera module

 

image

 

The story of the project

 

Many years ago I ran the IT department of a local newspaper. That included, in addition to an IBM AS400 computer, software development, electrical maintenance, air conditioning systems, prepress, Web-fed offset lithographic press PLC programming, photo composition and photographic processing. I became fond of photography and decided to get lessons for learning product photo. I bought a second hand Sinar Norma camera to learn and for my first jobs, jewelry photography. Then digital photography appeared, I changed my profession, I registered as a kodak digital developer and that's when my passion with photography ended, it became an employee job.

I had seen how other members of the element14 community were using the Raspberry Pi HQ Camera and was curious, so I bought one and tried to resurrect the Sinar Norma. It has been a very pleasant experience, rediscovering myself with photography so many years later.

 

Advantages and limitations

Advantages

Great control over the image provided by the swings, tilts, and other camera view adjustments.

Limitations

The camera must be used on a tripod and there is a delay between the image is composed and focused and when the final image is taken.

The Raspberry Pi HQ Camera sensor is too small. Any lens you can find for an old view camera turns into a powerful telephoto lens.

 

 

Raspberry Pi HQ View Camera Parts

 

image

 

Basic view camera adjustments

 

image

 

1. Focusing. Changing  the distance between lens and ground glass.

 

2. Back Tilt. Rotation of the camera back around a horizontal axis. To control the convergence of parallel vertical lines.

 

3. Front Tilt. Rotation of the lens board around a horizontal axis. To control the angle of the plane of sharp focus from top to bottom.

 

4. Front Vertical Shift. Moves the image the same distance in the same direction on the ground glass.

 

5. Back Vertical Shift. Moves he image in the opposite direction the same distance on the ground glass.

 

6. Back Swing. Rotation of the camera back around a vertical axis. To control the convergence of parallel horizontal lines.

 

7. Front Swing. Rotation of the lens board and lens around a vertical axis.To control the side to side angle of the plane of sharp focus.

 

8. Front Horizontal Shift. Moves the image the same distance in the same direction on the ground glass.

 

9. Back Horizontal Shift. Moves the image the same distance in the opposite direction on the ground glass.

 

 

 

 

 

 

Additionally:

10 . Pan-and-Tilt Head: Allows the entire camera to be tilted up and down, rotated clockwise and counterclockwise ad panned 360º circle around a vertical axis using the tripod.

 

11. Reversible and revolving back: The ground glass and the back can be placed in either a vertical or horizontal format position.

 

 

The Sinar Norma

The Sinar Norma is a monorail large format camera. The Sinar Norma used has a set up for 9x12 cm photography, a format widely used in Europe. It was made by the Swiss company Sinar.  It is a great and versatile large format camera.

 

image

Camera parts

 

image

 

The lenses

  • Schneider - Kreuznach Angulon 1:6,8/65
  • Schneider - Kreuznach Angulon 1:6,8/90
  • Schneider - Kreuznach Symmar 1:5,6/135
  • Schneider - Kreuznach Tele - Arton 1:5,5/270

 

 

 

Attaching the Raspberry Pi High Quality Camera

Adaptation for attaching the Raspberry Pi 4 B and the Raspberry Pi High Quality Camera

 

image

 

All glossy parts should be covered with a matte black color to prevent glare from reflecting off the lens system. The flare noticeably decreases the quality of the image.

image

 

 

 

Attaching the Raspberry Pi 4B board

 

Front View: The module stands upright on the case of the raspberry pi 4B

 

image

 

Back View: The box has a fan to prevent the module from heating up.

image

 

Lateral view:

image

Camera attached taking the first shot with a Schneider -Kreuznach Angulon 1:6,8/65 f/6,8

image

 

First shot: It works!

I try with the most angular lens that I have a 65 mm focal length lens that for 9x12 is a wide angle lens but for the small 6 x 4 mm sensor of the Raspberry Pi HQ Camera it becomes a powerful lens telephoto. I take a photo of a very distant object.

It was windy and the sycamore's leaves were constantly moving. The effect on the camera sensor is curious.

 

image

 

 

And with the same settings I take a photo of a closer object. And with the same settings I take a photo of a closer object. I still do not know the options of the raspberry pi hq camera well. I hope to improve the next shots.

It is grainy but the result is surprising because the photo is taken in the shade without additional lighting.

 

 

image

 

Let's compare with a photo taken with a Samsung A20 mobile

This is the reference photo taken from where we are going to place the Raspberry Pi View Camera:

 

image

 

Schneider -Kreuznach Angulon 1:6,8/65 f/11

 

 

image

 

Schneider - Kreuznach Angulon 1:6,8/90 f/11

 

image

 

Schneider - Kreuznach Symmar 1:5,6/135 f/11

I really am in love with this lens

 

image

 

Schneider - Kreuznach Tele - Arton 1:5,5/270 f/11

 

This telephoto lens is really a big guy and it turns our camera almost into a telescope.

 

image

 

Yes I said telescope, where is the moon?

Schneider - Kreuznach Tele - Arton 1:5,5/270 f/11

 

 

image

 

Last photo is a bit overexposed, let's try at f/16

 

image

 

At these focal lengths the moon is a very fast object image

 

Full Moon 2021/07/23 Spain

image

References

  • View Camera Technique by Leslie Stroebel, Routledge; 7th edition (March 31 1999)
  • The Camera by Ansel Adams, New York Graphic Society, 1982
  • Life Library of Photography: The Camera, Photography as a Tool, Special Problems, Photographing Nature, Frontiers of Photography.

 

 

Raspberry Pi HQ View Camera Blogs
Raspberry Pi HQ View Camera - From the roof to the Moon.
Raspberry Pi HQ View Camera - From the Moon to the PCB.
  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 5 years ago +6
    Great write-up! Putting a sensor on the back of a view camera is something I have wanted to do as well. I am envious of your camera and lenses
  • genebren
    genebren over 5 years ago +5
    Very cool blog. The images were very crisp and clear.
  • shabaz
    shabaz over 5 years ago +5
    Hi Enrique, Great work with the camera, and the results look really good!! Thank you for showing how to properly use such a sensor with the alignment capabilities in all the dimensions as you have shown…
Parents
  • shabaz
    shabaz over 5 years ago

    Hi Enrique,

     

    Great work with the camera, and the results look really good!!

    Thank you for showing how to properly use such a sensor with the alignment capabilities in all the dimensions as you have shown. It's really neat how you managed to use the existing camera to adapt to such a purpose.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 5 years ago in reply to shabaz

    Thanks shabaz! I have expanded the section of the camera adjustments explaining briefly what each one does, although the use is somewhat more complex since they all also influence something in the sharp focus plane.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 5 years ago in reply to shabaz

    Thanks shabaz! I have expanded the section of the camera adjustments explaining briefly what each one does, although the use is somewhat more complex since they all also influence something in the sharp focus plane.

    • Cancel
    • Vote Up +3 Vote Down