Photonics
  • Challenges & Projects
  • Project14
  • Photonics
  • More
  • Cancel
Photonics
Blog Simple light flicker meter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Photonics to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 8 Mar 2020 4:44 PM Date Created
  • Views 7079 views
  • Likes 18 likes
  • Comments 11 comments
  • esp32
  • light
  • led
  • photonicsch
  • flicker
  • m5stick
Related
Recommended

Simple light flicker meter

kk99
kk99
8 Mar 2020

image

The basic idea was to create a simple device which allow to compare the quality of light sources e.g. LED bulbs. I have used TSL250R IC containing photodiode and operational amplifier with configured feedback loop. This IC is optical sensor which output voltage is proportional to light intensitivity. I have put this sensor inside to M5Stick case and connected directly to ESP32 module. Output from sensor is connected to GPIO with number 35. Below there are images with mounted sensor:

image

image

Output data is sampled by ADC which is triggered by hardware timer of ESP32 board.

After sampling there is calculated FFT. After that there is obtained frequency for maximum peak.

Additionally there is displayed a plot with input data, so we could see amplitude of input signal.

All data are presented on OLED display.

Below there is diagram with flow:

 

image

Program was written in C with usage of ArduinoFFT and U8g2 libraries. Below there is source:

#include <Arduino.h>
#include <U8g2lib.h>
#include <arduinoFFT.h>

#ifdef U8X8_HAVE_HW_SPI
#include <SPI.h>
#endif

U8G2_SH1107_64X128_F_4W_HW_SPI u8g2(U8G2_R1, /* cs=*/ 14, /* dc=*/ 27, /* reset=*/ 33);

arduinoFFT FFT = arduinoFFT();
hw_timer_t *timer = NULL;
bool getSample;
const byte maxSamples = 128;
const word samplingFrequency = 2000;
double vReal[maxSamples];
double vImag[maxSamples];

void timerInterrupt() {
  if (!getSample) {
    getSample = true;
  }
}

void setup() {
  u8g2.begin();
  u8g2.setFont(u8g2_font_5x7_tr);
  analogReadResolution(12);
  getSample = false;
  timer = timerBegin(0, 80, true);
  timerAttachInterrupt(timer, &timerInterrupt, true);
  timerAlarmWrite(timer, 1000000/samplingFrequency, true);
  timerAlarmEnable(timer);
}

void loop() {
  word adcData[maxSamples];
  byte sampleCount = 0;
  bool adcDataReady = false;
  do {
    if (getSample && !adcDataReady) {
      adcData[sampleCount] = analogRead(35);
      sampleCount++;
      if (sampleCount >= maxSamples) {
        adcDataReady = true;
        sampleCount = 0;
      } else {
        getSample = false;
      }
    }

    if (adcDataReady) {
      char displayText[16];
      for (byte i = 0; i < maxSamples; i++) {
        vReal[i] = double(adcData[i]);
        vImag[i] = 0;
      }
      FFT.Windowing(vReal, maxSamples, FFT_WIN_TYP_HAMMING, FFT_FORWARD);
      FFT.Compute(vReal, vImag, maxSamples, FFT_FORWARD);
      FFT.ComplexToMagnitude(vReal, vImag, maxSamples);
      word peak = FFT.MajorPeak(vReal, maxSamples, samplingFrequency);
      adcDataReady = false;
      getSample = false;
      u8g2.clearBuffer();
      snprintf (displayText, 8, "%dHz", peak);
      u8g2.drawStr(65, 10, displayText);
      word r = 1 << 12;
      r = r / 54;
      for (byte i = 0; i < maxSamples; i++) {
        u8g2.drawPixel(i, 54-(adcData[i] / r));
      }
      u8g2.sendBuffer();
      delay(100);
    }
  } while (true);
}

 

Below there is short video presentation. We could see here a two different LED light sources with different flicker (high and low).

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

More details about light flicker in LED lamps you could find in this document:

LED flicker

 

The interesting improvement could be added measurement of light spectrum with additional sensor.

Attachments:
lightFlickerMeter.zip
  • Sign in to reply

Top Comments

  • genebren
    genebren over 6 years ago +5
    Awesome project. I worked in the lighting industry for a while and we did a lot of testing on our Zigbee mesh light controllers (and the attached luminaries, with their own driver/controller) to measure…
  • three-phase
    three-phase over 6 years ago +4
    Interesting project and works really well. I never really thought of LEDs have any flicker to their light output. Kind regards.
  • dougw
    dougw over 6 years ago +3
    Very nice project. What would it show for a fluorescent bulb?
Parents
  • dubbie
    dubbie over 6 years ago

    A very interesting and useful project. I have often thought it would be good to be able to measure the actual flicker in lighting. This is eomthing I might have to come back to and try myself, sometime.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago

    A very interesting and useful project. I have often thought it would be good to be able to measure the actual flicker in lighting. This is eomthing I might have to come back to and try myself, sometime.

     

    Dubbie