Portable Electronics Kit
  • Challenges & Projects
  • Project14
  • Portable Electronics Kit
  • More
  • Cancel
Portable Electronics Kit
Blog Control an relay from web server using NodeMCU
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Portable Electronics Kit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 11 Feb 2018 9:04 PM Date Created
  • Views 3417 views
  • Likes 8 likes
  • Comments 4 comments
  • portableekitch
Related
Recommended

Control an relay from web server using NodeMCU

kk99
kk99
11 Feb 2018

image

I would like to present simple circuit which allow to control device via relay with usage of web server running on ESP8266 board. The main component is ESP8266 board which allow to run script in LUA language. This ESP8266 board is connected with relay module via pin headers. Here is relay module:
image

Coil of relay is driven by NPN transistor from GPIO16 pin (PIN0) of ESP8266 board. Here is schematic of relay module:

image

To ESP8266 board was uploaded code (init.lua) which do following things:
- creates WiFi software access point with static IP address,
- sets PIN D0 as output and proper state,
- creates web server with simple HTML page which allow to control relay remotely.

 

Here code of LUA script:

cfg={} 
cfg.ssid="WiFiSwitch" 
cfg.pwd="Password" 
wifi.ap.config(cfg) 
cfg={} 
cfg.ip="192.168.1.1"; 
cfg.netmask="255.255.255.0"; 
cfg.gateway="192.168.1.1"; 
wifi.ap.setip(cfg); 
wifi.setmode(wifi.SOFTAP) 
gpio.mode(0, gpio.OUTPUT) 
gpio.write(0, gpio.LOW) 
srv=net.createServer(net.TCP) 
srv:listen(80,function(conn) 
conn:on("receive",function(conn,request) 
print(request) 
_, j = string.find(request, 'switchState=') 
if j ~= nil then 
command = string.sub(request, j + 1) 
if command == 'on' then 
gpio.write(0, gpio.HIGH) 
else 
gpio.write(0, gpio.LOW) 
end 
end 
conn:send('HTTP/1.1 200 OK\n\n') 
conn:send('<!DOCTYPE html>') 
conn:send('<html lang="en">') 
conn:send('<head><meta charset="utf-8" />') 
conn:send('<title>Remote switch</title></head>') 
conn:send('<body><h1 align="center">Remote switch</h1>') 
if gpio.read(0) == gpio.HIGH then 
switchValue = "ON" 
else 
switchValue = "OFF" 
end 
conn:send('<p>The switch is ' .. switchValue .. '</p>') 
conn:send('<form method="post">') 
conn:send('<input type="radio" name="switchState" value="on">ON</input><br />') 
conn:send('<input type="radio" name="switchState" value="off">OFF</input><br />') 
conn:send('<input type="submit" value="Switch" />') 
conn:send('</form></body></html>') 
conn:on("sent",function(conn) conn:close() end) 
end) 
end)


Here is view of this HTML page:
image

Attachments:
code.zip
  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +3
    Pretty cool project. One step closer to controlling the world via WiFi . What are you planning on controlling with your relay? Gene
  • kk99
    kk99 over 8 years ago in reply to genebren +2
    I would like to use this module to control 12 V output from regulator from solar system. In future I would like to add to this module possibility to set timer to control how long this relay is in ON or…
  • rcaste53
    rcaste53 over 8 years ago +1
    The connection of 1N4148 diode es wrong. Its cathode must be connected to VCC
Parents
  • genebren
    genebren over 8 years ago

    Pretty cool project.  One step closer to controlling the world via WiFiimage.  What are you planning on controlling with your relay?

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Pretty cool project.  One step closer to controlling the world via WiFiimage.  What are you planning on controlling with your relay?

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kk99
    kk99 over 8 years ago in reply to genebren

    I would like to use this module to control 12 V output from regulator from solar system. In future I would like to add to this module possibility to set timer to control how long this relay is in ON or OFF state.