A Question of Scale
  • Challenges & Projects
  • Project14
  • A Question of Scale
  • More
  • Cancel
A Question of Scale
Blog Jumbo LED
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join A Question of Scale to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 2 Feb 2019 11:30 PM Date Created
  • Views 6370 views
  • Likes 19 likes
  • Comments 24 comments
  • questionofscalech
Related
Recommended

Jumbo LED

Workshopshed
Workshopshed
2 Feb 2019

Since creating the Jumbo Servo I've been thinking about what else I could make in a jumbo size. The LED seemed the obvious choice.  I started by looking at pictures of LEDs up close. I then went on the hunt for different parts to help me along. Luckily I'd seen in the local IKEA some glass domes. I put one of those in the trolly and headed to the checkout, stopping to check the "junk" area before left. There I found a plastic dome with some LED lights, it had a better height to width ratio so I swapped my glass one for that. I also ordered some 10W LEDs and some gold and silver filament. I waited until those LEDs had arrived before committing to the project.

image

 

CAD

I modelled the LED using Fusion360, and put large holes down the middle of the legs for the wires. I exported the parts I would need to print as STL files.

image

 

Electronics

The electronics for this project are exceedingly simple. Just a 3W Red LED, resistor and a 12v power supply. I used copper wire from some "twin and earth" to replicate the tiny wires you see going from the semiconductor to the legs.

 

Printing

I did have some challenges printing this. Firstly I printed the legs in draft mode on my printer. Because of the thin wall size the printer omitted some of the walls! So I stopped the print then printed it again mirrored so that I could stick the two halves together. This worked quite well as it means I did not have to thread the cables through the legs. I used hot glue to hold the wires and halves in place.

 

For the base of the dome I used clear PLA, I realised that I did not have either the filament or the time to print it at the thickness I desired so cancelled the print after the first 3 layers so I had a nice solid disk to work with. I also spotted that there was no way to post the legs through as I'd modelled them with the wider section used to stop the LED going through the PCB. So I sawed my base in two and glued it to the dome. It's a bit flimsy so probably best to print or saw myself a thicker base at some point.

 

Resistor

No sophisticated constant current supplies for this project. Just an inline resistor. That was hidden inside a jumbo version of the resistor made from some pipe lagging and electrical tape.

 

Demo

The bit you've all been waiting for, the demo!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

{gallery} LED Gallery

image

Circuit: Here's a shot of the LED and the resistor that was just out of shot in the video. A 10mm LED for scale.

image

Legs: Printed in 2 parts then glued together

image

Top: LED from the top

image

Side: LED from the side

image

Lit LED: The limiting resistor is quite large, the device can go a lot brighter than this

image

LED Lit: Here it is lit up from the side.

  • Sign in to reply

Top Comments

  • gecoz
    gecoz over 7 years ago +11
    Perfect fit for this board!
  • baldengineer
    baldengineer over 7 years ago +7
    Nice job man! I appreciate that you added the current limiting resistor. Big props to you.
  • Workshopshed
    Workshopshed over 7 years ago in reply to balearicdynamics +7
    Fixed that and added a + and -
Parents
  • kk99
    kk99 over 7 years ago

    Awesome and eye catching project. Congratulations.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kk99
    kk99 over 7 years ago

    Awesome and eye catching project. Congratulations.

    • Cancel
    • Vote Up +4 Vote Down