A Question of Scale
  • Challenges & Projects
  • Project14
  • A Question of Scale
  • More
  • Cancel
A Question of Scale
Blog Tiny24hourMoBot #2 : 5 Hours in
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join A Question of Scale to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 7 Feb 2019 5:09 PM Date Created
  • Views 1229 views
  • Likes 7 likes
  • Comments 1 comment
  • mobile robots
  • tiny24hourmobot)
  • tiny24hourmobot
  • robotics projects
  • questionofscalech
Related
Recommended

Tiny24hourMoBot #2 : 5 Hours in

dubbie
dubbie
7 Feb 2019
image

A Question of Scale

Enter Your Electronics & Design Project for a Chance to Win a Cartridge-Sized NES Portable or a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Five hours after starting my 24 hour design of a Tiny Mobile Robot (tiny24hourmobot) I have managed to 3D print a rectangular band that will hold two continuous rotation servo motors. I did think of using the DC motors from inside two broken micro servo motors but I thought they would be rotating too fast, plus I would have had to include a dual H bridge DC motor drive as well. I do have one but it seemed an unnecessary complication when I could just use two continuous rotation servo motors. I did check that the two servos would fit inside the red spray can top I intended to use before printing the rectangular holder. Unfortunately I forgot to include the diameter of the wheels. The micro servo motors come with 24 mm diameter circular fixings which I thought would make great wheels and save me 3D printing them. Unfortunately this makes the motor - wheel combination 51.5 mm wide at its widest point, whereas the inside diameter of the spray can top is only 50.0 mm wide. I could try reducing the diameter of the wheels by a couple of mm but then there might not be enough clearance between the bottom of the servo motor and the ground.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Hay oh. Nothing much to be done there so I've now changed to 3D printing the equivalent of the spray can top.It does mean that I will be able to design it so that the motor unit fits into it nicely fixes together. I may not be using the exact spray can top I wanted but it is pretty close and I can probably find a slightly larger spray can sometime in the future if I still want to use recycles can tops.

 

Dubbie

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +2
    Nice demo. DAB
  • DAB
    DAB over 7 years ago

    Nice demo.

     

    DAB