A Question of Scale
  • Challenges & Projects
  • Project14
  • A Question of Scale
  • More
  • Cancel
A Question of Scale
Blog Tiny24hourMoBot #5 : Post Script - Making it even Tinier
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join A Question of Scale to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 13 Feb 2019 11:25 AM Date Created
  • Views 1364 views
  • Likes 8 likes
  • Comments 4 comments
  • mobile robots
  • tiny24hourmobot
  • 3d printers
Related
Recommended

Tiny24hourMoBot #5 : Post Script - Making it even Tinier

dubbie
dubbie
13 Feb 2019
image

A Question of Scale

Enter Your Electronics & Design Project for a Chance to Win a Cartridge-Sized NES Portable or a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Although I managed to create a just about working Tiny Mobile Robot in 24 hours I did not quite achieve my initial aim of getting to fit inside some read shiny spray can tops that I have been collecting. Having looked at the design to see if it was ever possible to get it to fit I decided to have a go at redesigning the motor assembly part to see if it could be made smaller. Obviously it could, as it is nearly always possible to improve on something that already exists. I identified that I could make the servo motor band holding the two motors together smaller and reduced it from 10 mm wide to 6 mm wide. By cutting off the mounting tags on the servo motors I was also able to reduce the wheel size from 24 mm to 20 mm. This might not seem very much but the combined effect is to reduce the motor unit diameter from 55 mm to 48 mm which is just enough so that it fits into the spray can cap.

 

image

 

I used TinkerCAD to design some new small wheels that have a grove for a rubber band to make a non-slip wheel. I found some suitable elastic bands in my LEGO in a packet I had never opened so fortunately they were still rubbery. I had to use glue (first time ever) to fix the servo horn (also cutdown in size) to the new wheels as the self-tapping screws I had originally used were too large.

 

Unfortunately I did not have time to reduce the size of the electronics so that now takes up too much room in the spray can lid and I cannot yet get the motor unit to fit nicely and there just isn't any room for the battery. Too many wires and too large a PCB. I did try using a 3.7V LiPo battery which just fits into the spray can lid but it just didn't have the voltage to run the Nano and the servo motors, it will need a boost converter so I am going to look at that next.

 

image

 

However, when everything except the batteries was stuffed into the top, it just about worked.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Future steps will be to reduce the electronics and the batteries in size.

 

Dubbie

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago +4
    That's very cool - love the idea of aerosol can cap robots : )
  • dubbie
    dubbie over 7 years ago in reply to shabaz +3
    Shabaz, Thanks, although I have not yet managed to get it all inside this specific spray can top. I may have to think about a slightly larger spray can top if I want to get everything inside. Dubbie
  • ntewinkel
    ntewinkel over 7 years ago +3
    Great progress, Dubbie! You could save a bit of space by using a Digispark or Pro-Mini board insteady of the Nano, some of which are available in 3.3v models too. Squeezing the battery in will be tricky…
Parents
  • ntewinkel
    ntewinkel over 7 years ago

    Great progress, Dubbie!

     

    You could save a bit of space by using a Digispark or Pro-Mini board insteady of the Nano, some of which are available in 3.3v models too.

    Squeezing the battery in will be tricky, but maybe using a little pack from a toy helicopter would give enough run time.

    I've also seen LifePo4 batteries in AA (and AAA I think) format with a nominal voltage of 3.2v and a fully-charged voltage less than the maximum allowed on those boards - meaning you wouldn't even need a boost or regulation circuit.

     

    You might end up having to 3D print an internal skeleton to neatly fit all the pieces!

    Before you design that, play a few rounds of Tetris image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to ntewinkel

    Nico,

     

    Thanks for the suggestion. I'm already thinking about using a LiPo battery with a booster PCB which will be considerably smaller than just AAA batteries. I've never seen a LiPo in AA or AAA format, I might have to have a look for those as two of them would produce the voltage needed.

     

    I've already started designing an internal 3D printed structure so that the outer shell can just drop onto it. We'll have to see how that goes.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago in reply to ntewinkel

    Nico,

     

    Thanks for the suggestion. I'm already thinking about using a LiPo battery with a booster PCB which will be considerably smaller than just AAA batteries. I've never seen a LiPo in AA or AAA format, I might have to have a look for those as two of them would produce the voltage needed.

     

    I've already started designing an internal 3D printed structure so that the outer shell can just drop onto it. We'll have to see how that goes.

     

    Dubbie