Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog Operator?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mfetting
  • Date Created: 1 Nov 2020 9:43 PM Date Created
  • Views 2817 views
  • Likes 11 likes
  • Comments 9 comments
  • google aiy
  • recycle
  • recycleretrofitch
Related
Recommended

Operator?

mfetting
mfetting
1 Nov 2020
image

Recycle & Retrofit

Enter Your Electronics & Design Project for a chance to win a $200 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

Convert early 1900's crank wall phone to a voice activated assistant.

image

The phone is called "the cathedral top and picture-frame type wall phone" because of the shape of the top and the rectangular groove in front of the box. The small black cylinder at the center of the top was a lightning arrestor. When the line was struck by lightning, this would divert the high voltage to a wire connected to the ground, protecting other wires and coils in the telephone from being burned by the excessive current.

 

Estimated value of this vintage phone is between $125.00 to $250.00.

 

Recyle & Retrofit Project:

 

Modify the Google voice AIY code to repond to the prompt "Operator", for example:

 

Question: "Operator, How do you make lemonade?"

Response: "One, In a small saucepan combine sugar and one cup water. Bring to boil and stir to dissolve sugar. And two, remove seeds from lemon juice but leave pulp."

 

There are no markings or labels on the phone to indicate the manufacturer.  There is a metal tag on the voice transmitter that contains "L41775".

A review of the components resembles the following wiring diagram, common to the Kellog Wall Phone of similar design.

 

imageimage

image

 

Action Plan:

 

1. Investigate current construction and design:

     - Search the web for any information on internal design.

     - Disassemble as necessary to further your understanding (avoid destroying any useful parts for upcycling).

     - Understand how and why it currently functions as designed.

2. Identify the means to update the design:

     - Using knowledge from prior investigation make modification decisions.

     - Test and verify the modifications.

3. Enable connection via Wi-Fi or Bluetooth:

     - Extend the modifications to allow greater accessibility.

 

Project will include the following items:

 

  1. Wall Crank Phone - Purchased at second hand store for $40 (Aug, 2018)
  2. Raspberry Pi 4 - Supports the Google Voice AIY Hat
  3. Google Voice AIY Hat - Enable Google Voice AIY Version 1 functionality
  4. Headphone speaker - replace existing internal component of the candlestick receiver
  5. Microphone - Use two I2S ISS MEMS Microphones (ICS-43432) for the voice transmitter
  6. New cloth covered wire for candlestick reciever.
  7. 3D printed internal parts for the candlestick receiver and transmitter
  8. 3D printed Raspberry Pi 4 mount
  9. Construct new wiring harness

 

Important Note for DIY.

 

With a manufacture date in the early 1900's, the wire insulation likely contains asbestos. If you spray the wire with a clear craft spray the asbestos will be less likely released into the air.  The spray is a temporary encapsulation of the asbestos, allowing it to be removed safely. It is best to replace the old wire with new safe wire.

 

Stretch goal:

 

  • Allow the bell to ring as an alarm/timer controlled through the voice activated assistant.

 

Research:

 

Google Voice AIY V1 Schematic

image

imageimage

Microphone Board (due to size it will need to be modified to fit in the voice transmitter)

image

Current Tasks:

 

1. Enabling Google Voice to use a custom hotword "Operator"

2. Layout circuit for relay to control bell ring (decide if the raspberry will control pattern of ring or ring circuit with timer"

3. Find an old headset to get a speaker

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 5 years ago in reply to Workshopshed +4
    www.youtube.com/watch
  • DAB
    DAB over 5 years ago +3
    In high school, I worked at a local grocery store and they still had one installed and working. They used it to connect directly to the owners house rather than use and open phone line. I do not know if…
  • Workshopshed
    Workshopshed over 5 years ago +3
    I remember trying to get the Google AIY respond to a custom word and it completely failing to recognise my accent. We tried "Marty Walk" and it got very confused so we swapped to "Activate Robot".
  • neilk
    neilk over 5 years ago in reply to Workshopshed

    A couple of years ago I bought my mother a Google device. Her problem wasn't her accent; it was her inability to remember that the trigger was "Hey Google"!

     

    She would try "Hello Google", "Mr Google", "Help Google", etc etc. Despite all my efforts, she never got to grips with itimage

     

    Neil

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 5 years ago

    I remember trying to get the Google AIY respond to a custom word and it completely failing to recognise my accent. We tried "Marty Walk" and it got very confused so we swapped to "Activate Robot".

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mfetting
    mfetting over 5 years ago in reply to DAB

    My uncle worked for a rural telephone company in MN and I remember him storing old crank phones up in the attic of my grandparents’ home.  He was a bit of a horse trader so somewhere along the line he likely traded them for something else.  He passed away many years ago, so I have no idea of what finally happened to them.  I know the old switchboard is in the town's museum.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    In high school, I worked at a local grocery store and they still had one installed and working.

     

    They used it to connect directly to the owners house rather than use and open phone line.

     

    I do not know if they still have it up and working, but it was fun to use.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<