Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog The Disinfectinator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yesha98
  • Date Created: 1 Dec 2020 3:25 PM Date Created
  • Views 3564 views
  • Likes 9 likes
  • Comments 6 comments
  • recycleretrofitch
Related
Recommended

The Disinfectinator

yesha98
yesha98
1 Dec 2020
image

Recycle & Retrofit

Enter Your Electronics & Design Project for a chance to win a $200 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

UV-C Based Germs Disinfecting Machine using vintage flatbed Scanner (Acer) and an old CPU

A touch-free germs disinfecting device that can disinfect anything from masks, wallets to mobile phones, killing maximum germs using UV-C.

image

Things used in this project:

Hardware:

S.NoComponentsQuantity
1Arduino MKR WiFi 10101
2Arduino UNO1
3MG90S Micro Servo1
4PHPoC Bread Board1
5Jumper wires (generic)1
6UVC Lamp1
7Adafruit RGB Backlight LCD - 16x21
8Digilent IR Proximity Sensor2
9Ultrasonic Sensor - HC-SR04 (Generic)1
10SparkFun Stepper motor driver board A49881
11ControlEverything.com 1-Channel Signal Relay 1A SPDT I²C Mini Module1

 

Software:

Arduino IDE

 

Tools and consumables used:

SnoTools
1 Soldering iron (generic)
2Solder Wire, Lead-Free
3Solder Flux, Soldering
4Drill / Driver, Cordless
5Multitool, Screwdriver
6Hammer
7Poker
8Hacksaw with Blade

 

Story:

Motivation:

I always wanted to build something useful to society and the world. Having been experienced in doing several science projects in electronics and IoT, I wanted to utilize my skills in such a way that most of the front-line workers are benefited from that. Due to the ongoing pandemic, things have changed a lot. We need to wear masks everywhere, sanitize our hands from time to time, etc. One such issue that I found was, after using our mobile phones or other things outside, we often forget to sanitize them or we do it with liquid disinfectant. Thus, I wanted to build something that could help people stay away from germs by disinfecting their essentials without touching the disinfecting machine itself.

In the current era, e-Waste has been a major threat to the environment. Therefore, this project mainly relies on using e-Waste effectively as much as possible.

Theory:

UV-C kills the germs by rupturing their cell membrane and altering their DNA/RNA

Source: lightstec.com

 

Source: lightstec.com

So this was the main idea in doing this project. UV disinfecting chambers have already hit the market, but one of the main features that they all lacked was, the 360-degree all-surface disinfection. This project overcomes those limitations and disinfects all the surfaces by flipping the items automatically after disinfecting one surface.

Key Features:

  • Completely Touch-Free
  • 360-degree disinfection
  • Kills coronaviruses also
  • UV-C based
  • Interactive display
  • Adjustable Timer up to 12 Hrs.
  • Emergency stop

Working:

  • The micro-controller continuously monitors for any obstacles in the proximity of the IR sensors. Once there is an obstacle in the close proximity, for required amount of time (1.5 seconds in this case) an event is triggered, based on what's displayed in the LCD.
  • When the open tray event is triggered, the stepper motor is driven the required number of steps to open the tray.
  • The same way when the close tray event is triggered, the stepper is driven until the limit switch shows a red-flag (the switch changes it's state) so that the tray is closed.
  • The timer is set either to default or by measuring the distance between the ultrasonic sensor and the hand.
  • After choosing the disinfect option, the relay is turned ON, thus turning on the UV-C lamp. After disinfecting one surface, the items are automatically flipped with the help of servo motors while the UV is still ON.
  • Lastly, after disinfection, the tray is again opened by the stepper motor.

Procedure:

Step 1: Gathering Things

Since this project is made from e-Waste, you need to first gather the parts. Things you would need:
  • An old flatbed scanner / embedded scanner (from the printer)
  • An old CPU Case
  • Geometry box
Then, you would need all the parts listed in the previous section.

Step 2: Building the Case and Tray

  • Dismantle the scanner and take out the lower part of the scanner that would have the scan head and the stepper motor attached with it. This would be used to take the items inside and outside the disinfecting machine.
  • Solder wires to the stepper motor, so that they're lengthy enough to connect to the breadboard.
  • Fix a limit switch at the end of the base, so that we can determine the position of the scan head while starting the MCU.

 

The base with the scan head of an old flatbed scanner, with the stepper motor and limit switch attached.

 

The base with the scan head of an old flatbed scanner, with the stepper motor and limit switch attached.
  • Remove the lamp that's there inside the scan head, you can re-use it later. Fix a firm base (tray) to the scan head. The things to be disinfected will be placed on the tray.
  • Now take the geometry box and separate the lid and the base. Attach these two to the servo motors, the servo motors will be used to flip these items.
  • Now fix the servo motor set up with the tray such that they can lift items and flip them. Make sure you use a powerful enough servo like a metal geared one, ex. MG90S servo.
  • Now mount the tray to the scan head. You should end up something like this:

 

The tray fixed to the scan head with the servo set-up

 

The tray fixed to the scan head with the servo set-up
  • Remove the front part of the CPU case such that it's completely open in one side.
  • Now attach the lower part of the scanner with CPU case using screws. Drill holes if necessary.

 

The base and tray mounted to the CPU case.

 

The base and tray mounted to the CPU case.

Step 3: The circuitry and sensors

Schematic:

image

  • The primary Micro-controller board will be the Arduino MKR WiFi 1010, and the secondary Micro-controller board will be the Arduino Uno. Give the connections as per the circuit given in the Schematics section below.
  • Fix the IR sensor in front of the top panel and the ultrasonic sensor in the middle, the display should be in the corner and clearly visible to the user.
  • The UV-C light should be placed beneath the top panel, in a reasonable position such that max. amount of light falls on the items placed on the tray.
  • Test each and every part including the motor and sensor as you connect them to the MCU.
  • Make the wires connecting the servo lengthy enough such that it doesn't stop the tray from coming out completely.
  • The completed circuitry looked like this for me, but make the connections as neat as possible.

 

The finished circuit should look something like this

 

The finished circuit should look something like this

Step 4: Uploading the code

  • The code that is provided is completely modular, call the functions that you need to execute while checking the circuitry.

Code:

You can find the full code here: https://github.com/yeshvanth-m/uvc

The final model:

image

Full Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Thank you for reading! imageimage

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 5 years ago +3
    Hi Yeshvanth, Very cool and well engineered. I like it and enjoyed your presentation. John
  • BigG
    BigG over 5 years ago +2
    Nooooooooooo! I've only just scrapped me old Epsom printer/scanner machine. Your demo of reusing a flatbed scanner is brilliant. Well done.
  • dixonselvan
    dixonselvan over 5 years ago +1
    Nice work yesha98
  • yesha98
    yesha98 over 5 years ago in reply to dixonselvan

    Thank you so much dixonselvan!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 5 years ago

    Nice work yesha98

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yesha98
    yesha98 over 5 years ago in reply to BigG

    Thank you so much BigG!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 5 years ago

    Nooooooooooo! I've only just scrapped me old Epsom printer/scanner machine.

     

    Your demo of reusing a flatbed scanner is brilliant. Well done.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • yesha98
    yesha98 over 5 years ago in reply to jw0752

    Thank you so much John!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>