Remote Monitoring & Control
  • Challenges & Projects
  • Project14
  • Remote Monitoring & Control
  • More
  • Cancel
Remote Monitoring & Control
Blog Big Petro Maker Magic:  $100 Datalogger That Can Save Millions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Remote Monitoring & Control to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Sean_Miller
  • Date Created: 17 Jul 2019 2:42 AM Date Created
  • Views 6362 views
  • Likes 20 likes
  • Comments 15 comments
  • remotemonitoringcontrolch
  • industrial control
  • sean miller
  • modbus
  • arduino
Related
Recommended

Big Petro Maker Magic:  $100 Datalogger That Can Save Millions

Sean_Miller
Sean_Miller
17 Jul 2019

This blog is in support of the Remote Monitoring & Control Project14 Challenge:

"So that is my challenge - make a datalogger of 24 sensors logging data every one minute that could run without mains power or human intervention for 7 days with no wires to avoid a million dollar a day loss"...

-Sean

PROJECT VIDEO

Below is are best attempt at edutainment detailing our project and the working Arduino Mega Modbus Datalogger:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

BILL OF MATERIALS

Arduino MegaArduino Mega

LCD 2x 16, I2CLCD 2x 16, I2C

Real Time ClockReal Time Clock

Arduino SD/Ethernet Shield

3D Files on Github

 

INTRODUCTION

The Energy, Petroleum, Chemicals, and Materials industries drive a lot of business for tech companies, IT companies, construction companies, consultants...the list goes on and on.  But sometimes, a fast, practical, and economical solution just hasn't been made yet in your "space".  Being a non-electrical engineer with a career in fixed equipment/mechanical engineering, this led me to my Remote Monitoring & Control Project:  Ad Hoc, Freaky Intense, Fixed Equipment Vital Health Monitoring.

 

To put this into context, let's look at a recent event.  If you live on the east coast, you probably heard about the 2019 Philadelphia refinery explosion.

 

Fortunately, no one was hurt:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

It is said to be the east coast's oldest refinery.  With Refining already over 100 years old, the industry is tasked with ensuring their assets keep their mechanical integrity.  In other words, making sure they can "keep it in the pipes", as we say at work.  With the age of assets and higher environmental standards, monitoring the fixed assets for erosion, corrosion, and cracking mechanisms that could lead to catastrophic failure and loss of containment has never been at a higher peak.  For Refining, when it gets out of the pipes, it usually means a fire or explosion comes with it.

 

For reference in this blog, "Fixed Equipment" refers to non rotating, non sensing assets such as piping and vessels.  This is opposed to the engineering fields of "Rotating Equipment" (pumps and compressors) and "Control Systems".  They too need monitoring, but compared to those tech savvy disciplines, someone that works on Fixed Equipment doesn't have a voltmeter or wire snips in their tool bag.  When you say Java, we say "don't mind if I do" and head to the break room.  That's what is cool about the Maker phenomenon - some very unique developments can occur as I hope you will find below.

 

KEEPING IT IN THE PIPES

The American Petroleum Institute has developed codes over the last century that serve as the industry's REGAGAP.  This acronym stands for Recognized and Generally Accepted Good Engineering Practices.  The US government's OSHA 1910 considers API 510, 570, and 579 codes as REGAGAP for fixed equipment (among others).  These codes provide specific asset condition requirements to trigger repair or increased monitoring.

 

One of the most common thing that is monitored is thickness of piping and vessel walls.  Over time, all metal slowly migrates into the process steams due to erosion or corrosion.  It does this to the point that pinholes occur or even a fish mouth rupture (not good).  Carbon steel rusts away when oxygen is present to form iron oxide on the surface and then water comes and washes it away.  Most folks have seen that with cheaper outdoor furniture and grills.  It's a process called rusting away.

 

However, carbon steel will also corrode away without oxygen present such as when used to transfer a liquid containing sulfur.  That corrosion process is called sulfidation.  It will eat the pipe from the inside out even if the pipe is beautifully painted once a year.  In addition to corrosion, you can have other metal damage mechanisms called cracking.  For example, if you go to Lowes, you'd think Stainless Steel is the end all metal need of the planet.  Just try to run some chlorides through it like found in crude oil and then heat it up.  It cracks and ruptures catastrophically!  So, you have to keep things under check.

 

The US didn't take over the top spot of petroleum product production by shutting down for every nick and scratch.  No refinery anywhere could stay in business if it had to shut down due to a thin spot of pipe.  But it also couldn't stay afloat if it had a fire every other day.  So, the code API 579 provides REGAGEP for operating under Fitness for Service (aka FFS).  This is a term applied when a defect is found on fixed equipment such as for pipe walls that have become thin enough to require more frequent inspection or vessel shells that have developed a crack on the surface that hasn't gone all the way through.  Shutting down could result in millions of dollars of sales loss, could present a local consumer fuel price crisis, and also presents many safety challenges for securing the equipment that normally contains hazardous materials for human interaction and work.

 

Now, at first read, this may seem shocking to someone outside of this 100 year old industry.  Don't worry, though - FFS calculations have a significant safety factor built in.  All of this is to just trigger proper attention way ahead of true physical limitations.  Thus, Insurance and Process Safety Management auditors and state code fully adopt API 579 for REGAGEP.

 

So, applying a lot of math, an engineer can allow the site to confidently operate with the defect under Fitness for Service (FFS) to make the run until the next major scheduled turnaround - which could be two or more years away.  However, the math is contingent that operating conditions (typically temperature, pressure, and flows) are generally the same and that corrosion rates, vibration, and any other damage mechanism isn't introduced.  Here is where I've challenged myself - I want ad hoc freaky, intense fixed equipment vital health monitoring.  (I made that phrase up.  Just now.  Feel free to use it.).  API code just requires inspecting at the half life calculation.  For instance, take a 3 year end of life calculation to an 18 month next inspection.  But like Freddy said, I want it all and I want it now.

TRADITIONAL MANUAL MONITORING OF MECHANICAL INTEGRITY

In the last 20+ years, various techniques to monitor fixed equipment have emerged.  In the earlier years, they'd just drill a hole partway through pipe and vessel walls.  If that shallow, tell-tale hole leaked, you knew it was time to replace it.  Sounds like commons sense, right?  Weeeeeeeelllllllll....common sense is actually "hindsight bias".  Fast forward 50 years, and hindsight (and injury) proved that tell-tale holes were no longer the common sense approach.  It assumed that the system would erode or corrode evenly on every face of its geometry.  It didn't account for cracking mechanisms or localized damage due to how the process flowed in the vessel or pipes.

 

Today's techniques are phenomenal at predicting problems without even having to shutdown the process.  However, many of them require expensive scaffolding to be built so humans can perform the inspections.  With that comes safety concerns and high costs.  Scaffold erection alone cost five figures.  Dependent on the process service, a business may do the monitoring anywhere from 3 to 10 years.  You could have process upsets that lead to corrosion in between that totally confuse you.

 

Below is an example of an inspection technique called Radiography (x-ray).  It is used to measure the wall thickness.

 

image

Radiography (aka X-ray) is a frequently used manual
technique for measuring pipe thickness.
Other techniques are Ultrasonic Thickness. 
Both can be costly, manual processes.

 

If the wall loss surpasses the thickness alert rate, it goes under Fitness for Service.  Once a piece of equipment goes under Fitness for Service (aka FFS), monitoring has to be increased.  Here comes the Maker project.  Instead of just settling on the present era method of doubling the frequency of inspection (say from every 3 years to every 18 months), one could make a device to monitor every minute!

 

AD HOC FREAKY, INTENSE FIXED EQUIPMENT VITAL HEALTH MONITORING

 

Now don't get me wrong - there are some big players in this market to measure thickness all the time.  However, it is very expensive to pull cable in the field for ad hoc desires.  Typically, permanent installations only have a few locations covered to provide an indication of general thinning.  This project is about allowing one to put out a temporary monitoring system to deal with a one off issue found in a remote area that doesn't have a permanent monitoring system installed.  Which is most of the industry.

 

Luckily, some other technology has emerged:  wireless industrial transmitters.  They can be used to automate the monitoring needed as well as make it easy to install without a major capital project.  The transmitters meet all the electrical classification requirements of Class I Div II Areas - which means their enclosures can contain an explosion inside of them if they were to spark - and they would keep out external gases that could ignite.  So, one would never have to worry about the atmosphere around the devices or require a Low Energy permit as long as the enclosure stayed closed - just as any control box in the field.

image

Rosemount 648 Industrial Sensor Transmitter - Loving to Meet the Arduino

 

By taking Rosemount 648 Wireless Transmitters used for normal internal process condition monitoring, one can establish an adhoc strategy to measure the fixed equipment vital conditions where the hurt is:

  • Surface Temperature
  • Strain
  • Vibration
  • Thickness

 

They just need to pair with sensors made for permanent installations as shown below.

image

Top Left:  Permasense Thickness Monitoring

Top Right: Strain Gage

Bottom Left: RTD temperature sensor

Bottom Right: vibration sensor

 

 

Normally, control systems monitor what is in the pipes and vessels - not the assets themselves (with the exception of large furnace tubes and rotating equipment).  As stated before, inspection technicians are sent out with hand held devices to take X-rays, shoot IR guns for temperature, and measure thickness with UT meters.

 

To automate such monitoring for ad hoc freaky, intense fixed equipment vital health monitoring, Rosemount Wireless transmitters can link together and repeat their wireless network to a Emerson 1410 Gateway.  You can daisy chain the transmitters such that you can get the sensor data in the remote location all the way back to your office.

image

Rosemont Auto-organizing Network

Capable of hopping 120ft between transmitters

all the way to your office

 

Here's the big bummer - the gateway doesn't store data!  For permanent installations, versus this project's adhoc freaky increased monitoring, it would normally be hardwired into a site's Distributive Control System (DCS ) to allow its data historian to do the logging.

 

image

Emerson 1410 Gateway:  Pretty Much a Boss for Industrial Wireless Data Brokering

 

The Wireless version of the Rosemount Wireless Transmitters make for a great solution for ad hoc freaky, intense fixed equipment vital health monitoring.  But, you have to have a way to collect the data, not just monitor it.  In walks good ole' Arduino.

 

DESIGNING A FIXED EQUIPMENT VITALS ARDUINO MEGALOGGER

The idea of going from every 18 months of human based monitoring to every minute of mega awesome monitoring is an easy sell.  But what good is monitoring if you don't record the data!

 

Rather than just use this in my office, I'd also like to have the gateway mobile as well.  So, when powering the Emerson 1410 Gateway with a practical amount of batteries, I got about 7 days.  So that is my Project 14 challenge - make a datalogger of 24 sensors logging data every one minute that could run without mains power or human intervention for 7 days with no wires.

 

Looking at the Arduino Mega, an SD/Ethernet Shield, a Real Time Clock, the math worked out:

image

A Spreadsheet to Estimate How Often The Datalogger Would Need Attention

 

One could get 1002 days of data every minute for 24 sensors and 2004 days with 12 sensors.  Also, using the Real Time Clock approach to shut off the Arduino in between datalogs, one could get 18 days of run time versus just 7.  With just a couple more 12V batteries in the suitcase, one could basically only have to check on it twice a month.  Now we're talking true ad hoc freaky, intense fixed equipment vital health MEGA monitoring!

 

Of course, one could acquire a control system datalogger at the expense of 5 figures of costs and services - but then I wouldn't be able to present this Project 14 Maker Remote Logging challenge solution, would I? image

 

EMULATING A MODBUS SERVER

Since 1979, an open source protocol for serial transmission has been in use called ModbusRegistered owned now by Schneider Electric.  Its original company developed it for their process control hardware so that manufacturers of automated valves and sensors could use it to communicate with their controllers.  It's like I2C, SPI, and the rest of the Master-Slave serial communication protocols.

 

To develop the Arduino code to poll the gateway for data, I needed to emulate a ModbusRegistered device for development at the house.  The device is considered the server or slave in the ModbusRegistered protocol.  I elected to use my PC to host such an emulator.  So, first I needed to install Python for Windows.  I retrieved it from here:  https://www.python.org/downloads/

 

I then found this nice little Python Modbus emulator named uModbus:  https://umodbus.readthedocs.io/en/latest/client/tcp.html#api

 

Here is the server side code that would emulate my Emerson 1410 setup:

#!/usr/bin/env python
# scripts/examples/simple_data_store.py
import logging
from socketserver import TCPServer
from collections import defaultdict
from umodbus import conf
from umodbus.server.tcp import RequestHandler, get_server
from umodbus.utils import log_to_stream
# Add stream handler to logger 'uModbus'.
log_to_stream(level=logging.DEBUG)
# A very simple data store which maps addresses against their values.
data_store = defaultdict(int)
# Enable values to be signed (default is False).
conf.SIGNED_VALUES = False
print("Starting Server...")
TCPServer.allow_reuse_address = True
app = get_server(TCPServer, ('localhost', 502), RequestHandler)

@app.route(slave_ids=[1], function_codes=[1, 3], addresses=list(range(7000, 7010)))
def read_data_store(slave_id, function_code, address):
    """" Return value of addresses. """
    return data_store[address]

@app.route(slave_ids=[1], function_codes=[6, 15], addresses=list(range(7000, 7010)))
def write_data_store(slave_id, function_code, address, value):
    """" Set value for address. """
    data_store[address] = value
if __name__ == '__main__':
    try:
        app.serve_forever()
    finally:
        app.shutdown()
        app.server_close()

 

(If you have trouble getting this to work, try opening port 502 on your firewall.)

 

I needed some data to pull from the server by my Arduino code.  To first seed the data at register 7001 and 7002 of the Modbus server, I made a client emulator to push over some values that are similar to what I expect from the Rosemount 648 wireless transmitters to land on the gateway.

 

#!/usr/bin/env python
# scripts/examples/simple_tcp_client.py
import socket
from umodbus import conf
from umodbus.client import tcp
# Enable values to be signed (default is False).
conf.SIGNED_VALUES = True
sock = socket.socket(socket.AF_INET, socket.SOCK_STREAM)
sock.connect(('192.168.1.239', 502))
# Returns a message or Application Data Unit (ADU) specific for doing
# Modbus TCP/IP.
message = tcp.write_single_register(slave_id=1, address=7002,value=30000)
#message = tcp.read_holding_registers(slave_id=1, starting_address=7001,quantity=2)
#you can un comment line 13 and comment line 12 to read back from the server
print("About to send message...")
response = tcp.send_message(message, sock)
print(response)
sock.close()
print("Completed successfully")

 

THE ARDUINO MEGA DATALOGGER SOLUTION

I first prototyped my solution with an Arduino Uno.  I found an existing Arduino library that handled all the heavy lifting of communicating using ModbusRegistered using TCP/IP.  I used a common shield (W5100) to handle the SD card logging, ethernet communication, and a Real Time Clock triggering a MOSFET to provide a deep sleep cycle.

image

Left to Right:  DS3231 Realtime Clock, Arduino UNO with W5100 SD/Ethernet Shield, 2x16 LCD Screen

 

Here was the code used in prototyping:

#include <SPI.h>
#include <SD.h>
#include <Wire.h> 
#include <LiquidCrystal_I2C.h>
#include "DS3231.h"
unsigned int param_value_int[7];
#include <Ethernet.h>
#include <ArduinoRS485.h> // ArduinoModbus depends on the ArduinoRS485 library
#include <ArduinoModbus.h>
byte mac[] = {0x90, 0xA2, 0xDA, 0x0E, 0x94, 0xB5 };
IPAddress ip(192, 168, 1, 94);
IPAddress server(192, 168, 1, 239); 
IPAddress gateway(192, 168, 1, 1);
IPAddress subnet(255, 255, 255, 0);
EthernetClient client;
ModbusTCPClient modbusTCPClient(client);
LiquidCrystal_I2C lcd(0x27,16,2);  // set the LCD address to 0x27 for a 16 chars and 2 line display
RTClib RTC; //real time clock
void setup() {
  Serial.begin(9600);
  Ethernet.begin(mac, ip, gateway, subnet);  
  
  lcd.init();
  lcd.backlight();
  lcd.setCursor(0,0);
  lcd.print("  PHILLIPS 66");
  lcd.setCursor(1,1);
  lcd.print("JJ8 Megalogger");
  pinMode(4, OUTPUT);
  digitalWrite(4, HIGH);                      // To disable slave select for SD card; depricated.
  delay(2000);
}
void loop() {
  lcd.display();
  lcd.clear();
  lcd.setCursor(0,0);
  lcd.print("Working...Please");
  lcd.setCursor(0,1);
  lcd.print("Stand By...");
  ethernetLoop();
  
  lcd.clear();
  lcd.setCursor(0,0);
  writeToFile(getTime());
  lcd.clear();
  lcd.print(getTime());
  delay(3000);
}
String getTime() {
  DateTime now = RTC.now();
  return (String)(now.year()) + '-' + (String)(now.month()) + '-' + (String)(now.day()) + " " + (String(now.hour())) + ":" + (String)(now.minute()) +":" + (String)(now.second());
}
void writeToFile(String the_string) {
  // Open serial communications and wait for port to open:
  File myFile;
  if (!SD.begin(4)) {
    lcd.clear();
    lcd.print("FAILED CARD!");
    while (1);
  }
  // open the file. note that only one file can be open at a time,
  // so you have to close this one before opening another.
  myFile = SD.open("JJ8.txt", FILE_WRITE);
  // if the file opened okay, write to it:
  if (myFile) {
    myFile.println(the_string);
    // close the file:
    myFile.close();
    lcd.clear();
    lcd.print("Write success!");
    lcd.setCursor(0,1);
    lcd.print("You may power down.");
    delay(5000);
  } else {
    // if the file didn't open, print an error:
    lcd.clear();
    lcd.print("error opening test.txt");
    while (1);
  }
}
void ethernetLoop()
{ long response;
  if (!modbusTCPClient.connected()) {
    // client not connected, start the Modbus TCP client
    Serial.println("Attempting to connect to Modbus TCP server");
    
    if (!modbusTCPClient.begin(server)) {
      
      Serial.println("Modbus TCP Client failed to connect!");
      Serial.println(modbusTCPClient.lastError());
      return;
    } else {
      Serial.println("Modbus TCP Client connected");
    }
  } else   Serial.println("Modbus TCP Client connected");
  
  Serial.println("About to read holding registers...");
  response=modbusTCPClient.holdingRegisterRead(1,7001); //https://www.arduino.cc/en/ArduinoModbus/ModbusClientholdingRegisterRead
  Serial.println("complete ");
  
  if (!response) {
    Serial.println("Could not read register! ");
    Serial.println(modbusTCPClient.lastError());
  } else {
    Serial.println("Register Value=" + String(response) );
    lcd.clear();
    lcd.print("Did it:" + String(response));
    delay(3000);
  }
  // wait for 1 second
  modbusTCPClient.stop();
  delay(100);  
}

 

As you can see, there is a lot of code and libraries.  I surpassed the UNO dynamic (RAM) memory.  The UNO couldn't handle the load of an LCD, SD card, ethernet port, and Real Time Clock all under one board.  In my 8 years of using Arduino, I finally had a project that outgrew it!

 

So, based on the math above...and the overall RAM I needed for my code to pull it off, I selected an Arduino Mega 2560 Rev 3 to pull it off.

image

Arduino Mega 2560:  Selected it for its Low Power and High RAM to handle all my code

 

 

Using the Arduino, I can hit a Modbus controller of any brand through the gateway's TCP/IP port to read the current values of its registers. All I need to know is the slave id (typically 1) and the address of the registers I want to read.

 

You may think, how do you know you don't have bad data coming in?  Well, they thought of that all the way back in 1979 when they developed the ModbusRegistered protocol.  At the end of its bit packet is a checksum.  If the prior bits don't sum up to the checksum value, we trap and handle it.  So far, I've never lost a bit.

 

After uploading the code to the Mega and adjusting for my particular registers and SD write timing, I powered it by batteries and achieved the goal of 1 week datalogging.

ASSEMBLY OF THE FINAL PROJECT

I used Autodesk Fusion 360 to design the case.  Fortunately, all the devices in my project had already been modeled and found on grabcad.com.  This site is a great place to look for off the shelf models to save you hours of time establishing "obstruction models" for your own designs.

 

image

Autodesk Fusion 360 Design

 

 

image

Fully Assembled Arduino Mega Datalogger

 

image

Running the Code

 

You can find the Autodesk Fusion 360 file along with the Arduino .ino file at our Github repository:  https://github.com/RaisingAwesome/Arduino-Modbus-Mega-Logger

 

PROJECT CONCLUSION

This was a great project to show how the lines have blurred in Engineering disciplines in recent time.  The Maker revolution over the last 10 years has changed the university approach to engineering and I'm glad to find that graduates are coming in with Arduino experience and coding skills regardless of discipline.  We still have a lot of barriers to break down between IT, Electrical Engineering, and Mechanical Engineering, but I see it happening every day.

 

There is no doubt that code is what will change the world to come as the hardware is already available and very inexpensive.  I hope this blog tieing age old industrial communication protocols to modern maker magic provides insight that will inspire others to embrace code and the hardware and change the world!!

 

-Sean

 

PS.  Although you see a lot of products here - I have no affiliation with those companies or any endorsement from them - they are just industry standards I have worked with over the years.

  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 7 years ago +4
    Good explanation of the problem and the background information. The great thing with Rosemount equipment is they can operate in a wide range of temperatures and last for decades because they are so well…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to mp2100 +4
    Because the network gateway is wireless, it can be 120 feet from the nearest wireless transmitter. One can install multiple wireless transmitters as "wifi" repeaters every 120 ft between the suitcase and…
  • neuromodulator
    neuromodulator over 7 years ago +3
    This is very interesting! What sensors are you using? How do you measure strain and thinkness?
Parents
  • neuromodulator
    neuromodulator over 7 years ago

    This is very interesting!

    What sensors are you using? How do you measure strain and thinkness?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to neuromodulator

    For thickness, Permasense (offered by Emerson) is what I consider the most prevalent brand.  They came out of the UK.  Their batteries last 10 years!

     

    Strain is more of a commodity matched to the application - most often directed by temperature of the asset.  The kicker is using it with the Rosemount 648 wireless so that it is paired to its sensitivity.

     

    -Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to neuromodulator

    For thickness, Permasense (offered by Emerson) is what I consider the most prevalent brand.  They came out of the UK.  Their batteries last 10 years!

     

    Strain is more of a commodity matched to the application - most often directed by temperature of the asset.  The kicker is using it with the Rosemount 648 wireless so that it is paired to its sensitivity.

     

    -Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • neuromodulator
    neuromodulator over 7 years ago in reply to Sean_Miller

    There is an herox challenge (https://www.herox.com/astinspection ) to find ways to automate corrostion and cracking measurement of tanks, apparently they still do it manually (with guys with sensing equipment). Also in my country (Chile) BASF was looking for ways to measure/predict corrosion rate, as they were also doing it manually. Why aren't all these companies using this technology (permanently attached ultrasound sensors)?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to neuromodulator

    My thoughts on why it appears they are not using ultrasonic sensors to inspect tanks:

    • They may actually have some installed on the tank walls, but that doesn't paint the entire picture needed to satisfy the tank inspection.
    • The bottom of the tank, a leading region of concern, is inaccessible from the outside.  They are most likely looking for a retrofit solution since excavating and chipping out foundation wouldn't be favored.  There is an open space for a venture capitalist here yet unexplored for new tank installations.  You have an opportunity to design in a sensor grid before you lay the bottom.  It'd take some head scratching so that the sensors could periodically be replaced and to get the necessary coverage.
    • A leading cause of wall and bottom corrosion is deterioration of its coating inside.  If they knew the coating was in good condition, then they could lower their risk rank, and per API 580 (Risk Based Inspection), extend their interval between inspections.  UT won't detect deteriorated coatings.  XRay won't either.  As of now, you have to visually inspect from the inside.  So, perhaps the first trick would be to have a submersible high res camera that can blow away crude and record a map to support visual inspection.  They have such camera robots with magnetic wheels that go up large columns - but for clean inspection only - not on the fly or non-decontaminated service.

     

    My thoughts on why everyone isn't using permanently installed UT for pipes and vessels:

    • It's just starting to come into vogue in the fixed equipment world among inspired leaders.
    • Fixed Equipment Engineers aren't known for their tech pursuits.  hey typically aren't in the same room or building with Control Systems Engineers.  They tend to write weld repairs plans, review knew projects for standards compliance, and perform torque specification calculations.  Not a lot of room for tech exploration without it being a push from the top.
    • If the Control Systems Engineers have not yet implemented a wireless infrastructure for their sites, then there is a huge hurdle to climb - IT will voice concern on security and electricians may voice concern on becoming network experts.
    • If the Control Systems Engineers are still using pneumatic controllers and transmitters, they are really behind.  This is still the case for a lot of the small guys.
    • Fixed Equipment inspection and repair contractors are typically two wings of one company.  Their business model is labor and material cost plus.  Eliminating manual inspection eliminates profit, so they have no reason to pursue it.  In fact, there are many that still manually log on paper using hand held devices that are automatically capturing the data ready for upload into the corrosion management system (such as Ultrapipe, Meridium, and PCMS).  They will continue to do so until the owner catches on that this could have stopped 20 years ago.

     

    If its just lack of knowing about it, an engineer can google Permasense and probably get a corporate award and lifetime membership to the Jelly of the Month Club.  They will bring in a game changer.

     

    See ya',

    Sean

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neuromodulator
    neuromodulator over 7 years ago in reply to Sean_Miller

    I learned about this corrosion issue a few months ago when the local BASF talked about it. Without any knowledge of the current state of the art, I thought it could be in some way solved using an ultrasonic sensor connected to an MCU wirelessly connected to a server, which would through statistics estimate the corrosion rate and when the pipe could fail. After checking online I sadly found there were already a couple of such implementations so I abandoned the idea as I didn't think it would be worth to reinvent the wheel.

    Is piping technology working on solving the corrosion issue? Maybe through the use of fiberglass, plastics or other materials that don't corrode at all?




    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to neuromodulator

    I do think there is space for competition in remote corrosion monitoring and one could make a better solution than what is on the market.  The prices definitely reflect lack of competition.  The designs appear to be in their "first gen" look and feel.

     

    As for solving the corrosion issue - there definitely is an entire industry around living with it:

    • Universities sell Material Science BS and Masters degrees for it
    • Third Party Corrosion Control companies such as Nalco exist to sample chemistry and sell/operate additives that inhibit corrosion
    • Companies make probes that corrode and measure the rate in the process stream (I never recommend them)
    • Companies have NDE technicans to detect thinning of pipe and vessels
    • Engineers like me manage around it
    • Craftsman repair it.
    • etc.

     

    Depending on your culture in the industry, you may focus on handling it, or you may have long ago gone to alloys that are compatible.  The Chemical Industry tends to "alloy up" and it not be as much of a concern.

     

    For other materials, Plastic can't hold up to the longevity needed.  There are vessels from the 40's still around.  Plastic tends to embrittle in 10 years and not be applied in pressures greater than 80psi.  There are processes that operate at 2000psi and even 10000psi such as Tyvek.

     

    For fiberglass, its strips of material can start delaminating.  Often a new tank is internally inspected within its first year just to make sure compatibility with the process.

     

    Cost drives the metal choice as well.  For example, its cheaper to epoxy coat a carbon steel tank every six years than make it out of Hastelloy once.

     

    The bummer with many solutions is that there are conditions that one can create a cracking mechanism such as if the process is taken down too quickly or chlorides are introduced.  So, you can't totally get away from inspection.

     

    However, those companies that still have carbon steel and require chemical treatment need to "alloy up" if they want to reduce the entourage of services required to keep it in the pipes.

     

    Great questions,

    Sean