RF Radio Frequency
  • Challenges & Projects
  • Project14
  • RF Radio Frequency
  • More
  • Cancel
RF Radio Frequency
Blog Arduino Mini RDF Fox
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RF Radio Frequency to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kmikemoo
  • Date Created: 13 Jan 2020 4:57 AM Date Created
  • Views 8654 views
  • Likes 11 likes
  • Comments 3 comments
  • rfradiofrequencych
  • arduino
  • ham radio
Related
Recommended

Arduino Mini RDF Fox

kmikemoo
kmikemoo
13 Jan 2020

As part of Project14 | RF (Radio Frequency): Win a Spectrum Analyzer for the Most Innovative RF Project!, I wanted an automated transmitter for my Antenna Radiation project.  Amateur radio folks use such a device for "fox hunting", a radio direction finding event where the transmitter is hidden and one has to find it.  I decided to go with one where an Arduino controls a handheld radio and plays a little segment that the radio broadcasts.  My inspiration came from Fox Hunt Transmitter – Whitecourt Amateur Radio.

The version I used for testing antenna radiation patterns was good enough - but I did want to improve it (sooner or later).  The schematic from Whitecourt had two wires reversed (dark brown and purple on the smaller plug).  The "schematic" below is correct.

imageimage

Yes, that's a Velleman box.  The rubber band was to keep the lid on during the snow and sleet.  The blue thing is a 2000mAh cell phone charger for power and the whole system plugs into a $35 Baofeng UV-82 radio.

The relay controls the Push-To-Talk circuit.  When closed, the radio transmits.

D5 is the Arduino output to radio microphone input. The darker brown wire is also common / radio ground.

A0 allows for DTMF (Dual Tone Multi Frequency) input, but I'm not using that yet.

 

With the antenna radiation pattern testing complete, I wanted to upgrade the packaging of my fox - to make it more field ready.  The circuit did need to be modified slightly and I needed to change my Arduino code slightly.  The relay board above was active low and the relay used below will be active high.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
image

Slides

1.  Protoboard that will fit in the project box

2.  Add headers and ground jumper

3.  Add relay

4.  Add relay driver circuit

5.  Add wiring that will connect to radio

6.  Add terminal connector for radio wiring & install Arduino

7.  Connect radio plug

8.  Project box

9.  Antenna jumper and installation hole

10.  Antenna jumper in hole

11.  Antenna installed

12.  Arduino fox with relay installed in project box, radio and battery added

13.  Arduino Mini Fox transmitting.  Not very flashy but will hide well.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I will need to add a notice on the side before I place it somewhere to test its range.  It wouldn't be good for someone to think it a nefarious device.  That is all for another day.

 

Forgot to add the files.

Attachments:
Fox.ino.txt.zip
pitches.h.txt.zip
  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +1
    Nice build. DAB
Parents
  • durandal734
    durandal734 over 4 years ago

    Hi, for some reason this, and pretty much all the different variations of this DTMF detection code just don't work on my arduino. When I load it, it'll push out an empty carrier wave for about 30 seconds and then it won't acknowledge any DTMF codes. I'm at my wit's end here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • durandal734
    durandal734 over 4 years ago

    Hi, for some reason this, and pretty much all the different variations of this DTMF detection code just don't work on my arduino. When I load it, it'll push out an empty carrier wave for about 30 seconds and then it won't acknowledge any DTMF codes. I'm at my wit's end here.