RF Radio Frequency
  • Challenges & Projects
  • Project14
  • RF Radio Frequency
  • More
  • Cancel
RF Radio Frequency
Blog Project to design RF friendly Switching Converters
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RF Radio Frequency to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: station240
  • Date Created: 14 Jan 2020 5:40 AM Date Created
  • Views 1726 views
  • Likes 7 likes
  • Comments 3 comments
  • rfradiofrequencych
Related
Recommended

Project to design RF friendly Switching Converters

station240
station240
14 Jan 2020
image

RF (Radio Frequency)

Enter Your Project for a chance to win a Spectrum Analyzer for the Most Innovative RF Project!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Strange Bedfellows - RF and digital switching

I was wondering how the Spread Spectrum option in some Computer Motherboard BIOS actually works, at the time I couldn't find an explanation.

It sounded a lot like a FM modulator, only connected to some form of sweep or white noise generator instead of an audio input.

After much searching, I found this is exactly how it works.

image

 

This opens further questions, just how much RF technology has made it's way into computer and Switch Mode Power Supply (SMPS) design ?

Then you have things like modern digital radios, and Software Defined Radio (SDR), where technology has crossed in the other direction.

 

In the RF field, spread spectrum broadcasts use any of the following technologies:

Frequency-hopping spread spectrum (FHSS), direct-sequence spread spectrum (DSSS), time-hopping spread spectrum (THSS), chirp spread spectrum (CSS)

 

The Projects

So my projects are to design, and hopefully build, RF friendly Switchmode Power Supplies.

These could be anything from a 5W LED driver, to a 5000W offgrid solar inverter.

To the best of my knowledge none of this exists.

 

First we need to understand the problem why is a simple squarewave such a huge problem for radio, TV and RF in general.

If you look at a 1kHz squarewave with a Spectrum Analyzer you get this.

image

 

Every second harmonic is skipped, so 1kHz gets harmonics of 3kHz, 5kHz, 7kHz etc. This skipping is the result of the 50% duty cycle, the even (divides by 2) frequencies are cancelled out.

However, SMPS work by varing the duty cycle to get a stable output voltage, so what frequencies are cancelled alter varies.

In addition, a second main frequency is generated, as ontime is time, and frequency = 1 / time.

An FM signal looks like this on a Spectrum Analyzer, note the peak is -12dB lower.

image

Nothing is perfect, this will create more wideband noise, and may raise the noise floor on some RF recievers.

 

 

I happened to find this document on TI's website, the PFC chip was mentioned in one of their recent videos.

Frequency Dithering with the UCC28180 and TLV3201

https://www.ti.com/lit/an/slua704/slua704.pdf March 2014

The UCC28180 is a dedicated Power Factor Correction controller, a type of boost converter for charging a capacity with DC from AC as a continuous load.

 

 

 

 

So we have an external circuit that can vary the frequency of a PFC controller, just need to apply it to a generic PWM controller.

Simple right ?

 

Looking at the standard PWM controllers (including the ones I have lying around), they all use a RC oscilator to set the frequency and the UCC28180 just makes do with a single resistor.

It's not the same, so we need to find PWM controllers with the same single resistor to set frequency input.

 

So far I've found LM5020, LM5021, LM5025 using the search term "Single Resistor Programmable Oscillator" together with "PWM". There will be others, but not found them so far.

In detail the specs are:

LM5020 <630kHz

LM5021 <1MHz

LM5022 <2.2MHz 6-60V input, 1A mosfet gate drive

LM5025 <1MHz  13-90V input, 1A mosfet gate drive

 

LM5022 describes itself as having "Single Resistor Oscillator Frequency Set", *sigh* standards TI.

It's suitable for Boost Converters.

 

The frequency pin on the LM5022 is around 2V, so need to increase the voltage to the Frequency Dithering circuit to 4V.

May also need to alter R5, to alter the magnitude of the output. Not looked yet at changing the amount of Frequency Dithering, as 7kHz may not be enough.

 

Another thought, can this approach also work with a traditional RC network where a resistor charges a capacitor ?

I theory it should be possible, some experiments and component changes will be needed.

 

 

Another idea

Skip pulses, rather than varying the duty cycle.

eg 50% duty cycle, ignore every second pulse by not generating it.

 

Problems I see with this idea:

1. More lumpy output voltage on SMPS.

2. Requires higher frequency and voltage to make up for the reduced transfer in some situations.

3. Possibly less efficient.

4. The intermittent RF emmissions might be more problematic to filter/ignore in RF equipment.

 

However if the SMPS has multiple parallel converters, for increased power output, there is another option.

Disable individual sections (phases) to control the output voltage.

 

 

More complex RF friendly controllers

 

A Microcontroller using Fourier Transform and a table of known frequencies to avoid, to create RF safe PWM signals.

 

Use SDR (Software Defined Radio) methods to create a more complex frequency control.

 

A further idea, allow external input to one of the Microcontroller or SDR controller, from a RF device itself.

So the frequency(s) being transmitted/received can be avoided by the SMPS controller.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 6 years ago +2
    Linear Technology (Analog Devices) make Spread Spectrum Oscillators: eg LTC6908 They have a good article on the web: https://www.analog.com/en/technical-articles/spread-spectrum-frequency-modulation-reduces…
  • station240
    station240 over 6 years ago in reply to michaelkellett +1
    I didn't have time to look up all the possible chips from different companies, as briefly mentioned they sometimes use different terms. I choose the LM5022 early in the search, as it's capable of taking…
Parents
  • michaelkellett
    michaelkellett over 6 years ago

    Linear Technology (Analog Devices) make Spread Spectrum Oscillators:

    eg LTC6908

     

    They have a good article on the web:

     

    https://www.analog.com/en/technical-articles/spread-spectrum-frequency-modulation-reduces-emi.html

     

    which mentions these and several complete spread spectrum capable regulator chips.

     

    The LTC3251 is an interesting part - it's a spread spectrum capable inductorless step down switcher.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • station240
    station240 over 6 years ago in reply to michaelkellett

    For my purposes, The sawtooth generator circuit I got off TI, is better than the Linear Technology parts you mentioned.

    As I wanted to experiment with how altering the frequency variation changes the spectrum response.

    Neither of those LTC ships have control over that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • station240
    station240 over 6 years ago in reply to michaelkellett

    For my purposes, The sawtooth generator circuit I got off TI, is better than the Linear Technology parts you mentioned.

    As I wanted to experiment with how altering the frequency variation changes the spectrum response.

    Neither of those LTC ships have control over that.