Rube Goldberg Device
  • Challenges & Projects
  • Project14
  • Rube Goldberg Device
  • More
  • Cancel
Rube Goldberg Device
Blog Rube Goldberg Machine to Turn On a Light
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Rube Goldberg Device to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 16 Aug 2022 11:40 PM Date Created
  • Views 27728 views
  • Likes 9 likes
  • Comments 9 comments
  • rubegoldbergch
  • Braccio
  • rube goldberg machine
  • robot arm
Related
Recommended

Rube Goldberg Machine to Turn On a Light

ntewinkel
ntewinkel
16 Aug 2022

I've always wanted to build a Rube Goldberg Machine, but I had no idea how tedious - and painful - the process would be! Laughing

It also took a LOT more pre-thinking and figuring out just to plan what was possible and how each step could trigger the next step. And oh boy is this thing ever finicky on exactly where each item has to be!

So without further ado, here is my Rube Goldberg Machine!

Nico's Rube Goldberg Machine

It turns on the light in the top corner, and all you have to do is simply touch the little bird on the post to start the machine.

I'm hoping to get proper government funding so that I can shrink down this machine into something that will fit into a standard electrical box that can be mounted in place of a regular light switch Stuck out tongue winking eye

Here's my intro video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

And here is the final machine in action!!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Full disclosure: I had to use a little bit of film-maker magic to get the full final sequence Laughing
Each step actually (surprisingly!) worked very well by itself and most of the time it did trigger the next action, but having ALL steps work ALL the time is not something I was able to achieve.
Some was to get better camera angles - I was able to quite reliably have the bird trigger the robot arm, and the robot arm very reliably delivered the marble, and the marble somewhat reliably triggered the robot-worm, and the robot-worm always reliably crashed into the excavator, but the stylus didn't reliably press the button in the app to start the Elegoo car (it's a TINY button!). After adding a few supports and by using sticky-tacky, and after much effort and trial and error, the car crash somewhat reliably would press the button to turn on Mr. Robot who then very reliably uttered the command to tell Alexa to turn on the light.
And, sigh, Alexa refused to listen to an inferior robot saying her name - it does actually turn on the light if I say her name first just before the robot says the command. I should've recorded my own voice for the keyword.

All in all I'm pretty happy with how it all came together!

Enjoy!

  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 4 years ago in reply to beacon_dave +1
    >" The bird on a stick that I had used to have had a bit of a tendency to rotate around the pole" Oh it did that here too! and it failed a lot at first because of it. I was able to compensate somewhat…
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    "...I've always wanted to build a Rube Goldberg Machine, but I had no idea how tedious - and painful - the process would be!..."

    But worth it in the end  Slight smile

    The bird on a stick that I had used to have had a bit of a tendency to rotate around the pole on its way down, so it would probably have failed at the first step ! 

    Any plans of going for the record ? Just a couple of more hours should do it... Slight smile

    5000+ Hours to Break A Guinness World Record?!
    https://www.youtube.com/watch?v=3wwJl7ZG9Q4

    300 Step Rube Goldberg Machine - all Built Within a 6ft CUBE?!! | (Guinness World Record Breaker)
    https://youtu.be/Namgsx6I7Us

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 4 years ago in reply to beacon_dave

    >"The bird on a stick that I had used to have had a bit of a tendency to rotate around the pole"

    Oh it did that here too! and it failed a lot at first because of it. I was able to compensate somewhat by moving the reed switch closer to the base and starting the bird rotated away a bit. Every step was kind of like that - compensating for the real-life movements and aligning the next steps carefully. Very finicky business Laughing

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 4 years ago in reply to beacon_dave

    >"The bird on a stick that I had used to have had a bit of a tendency to rotate around the pole"

    Oh it did that here too! and it failed a lot at first because of it. I was able to compensate somewhat by moving the reed switch closer to the base and starting the bird rotated away a bit. Every step was kind of like that - compensating for the real-life movements and aligning the next steps carefully. Very finicky business Laughing