Simple Music Maker
  • Challenges & Projects
  • Project14
  • Simple Music Maker
  • More
  • Cancel
Simple Music Maker
Blog Old fashioned Japanese Music Box
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Simple Music Maker to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 4 Jun 2018 4:50 PM Date Created
  • Views 24814 views
  • Likes 16 likes
  • Comments 6 comments
  • musicmakerch
  • musictimech
Related
Recommended

Old fashioned Japanese Music Box

Workshopshed
Workshopshed
4 Jun 2018

Today you can put a Rasperry Pi Zero or PocketBeagle in a project and have the resources of a whole computer to control your project.

 

When I was a lad, all we had were a few chips and transistors. One of my favourites was the 555 timer so I decided to use two for this little project which was origionally created for a tutorial in Hackspace Magazine.

 

A mechanical music box is controlled with 556 chip (dual 555), a transistor and a few discrete components. It is triggered by a capacitive touch module which has an active high output.

A simple transistor switch inverts the signal and triggers the first 555. This is configured as a monostable and runs for a few seconds. The second 555 is configured as an astable with a diode in the timing circuit to make it perform as a PWM generator. This allows speed control of the motor which is driven by a transistor.

image

image

The motor was a modified microservo, the mechanics were adjusted so that it could run continuously and the control circuit was removed and replaced with a simple capacitor, with the above circuit providing the control.

imageimage

A simple wooden box was made for the housing and a tune from a popular Japanese animation was played on the hand cranked music mechanism.

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +3
    Hi Andy, I really liked your use of the 556 timer chip. For some reason using basic chips appeals to me as opposed to microprocessors for everything. Thanks John
  • Workshopshed
    Workshopshed over 8 years ago in reply to jw0752 +3
    Cheers John, when I grew up the 555, CMOS 4000 series logic and a 741 were what I had. Many variations of a 555 + 4017 were created.
  • genebren
    genebren over 8 years ago +2
    Clever design. I really like the servo motor crank approach to drive the music box mechanism. Very cool! Gene
Parents
  • genebren
    genebren over 8 years ago

    Clever design.  I really like the servo motor crank approach to drive the music box mechanism.  Very cool!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Clever design.  I really like the servo motor crank approach to drive the music box mechanism.  Very cool!

    Gene