Simple Music Maker
  • Challenges & Projects
  • Project14
  • Simple Music Maker
  • More
  • Cancel
Simple Music Maker
Blog Tube headphone amplifier
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Simple Music Maker to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 10 Jun 2018 1:37 PM Date Created
  • Views 6427 views
  • Likes 12 likes
  • Comments 11 comments
  • musicmakerch
  • acousticsch
Related
Recommended

Tube headphone amplifier

kk99
kk99
10 Jun 2018

image

I would like to present a simple headphone amplifier based on PCC88 tubes. This construction was made a around a year ago. This amplifier gives a very fun from listening of music.

Main construction based on the White's cathode follower. Here is schematic of this part:
image

Here you could find more information about White's follower with equations for e.g. gain: http://www.tubecad.com/october99/page4.html

As power supply I have used a boost converter which gives around 180V with 40 mA of current. Here is schematic of boost converter:

image

Values of elements:

R1 = 0.47 Ω

R3 = 10 kΩ

R4 = 681 kΩ

L = 1mH

T1 = IRF840

D1 = BYV29-500

C5 = 470uF + 100nF

Case was made from old box for transformer which was polished.


imageimage

Here is short video presentation:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago +6
    Interesting circuit and a nice project built around it. I can sort of understand the operation, indirectly, by substituting FETs for the tubes. The top tube is a follower and the bottom one an active pull…
  • rachaelp
    rachaelp over 8 years ago +5
    Very nice project! I used to have a valve amp as part of my hifi setup, maybe I will build one of these headphone amps one day just so I can have some excuse to mess with valves
  • DAB
    DAB over 8 years ago +4
    Brings back memories. I used to build these back in the 1960's. DAB
Parents
  • DAB
    DAB over 8 years ago

    Brings back memories.

    I used to build these back in the 1960's.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago

    Brings back memories.

    I used to build these back in the 1960's.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down