Solar Power Devices
  • Challenges & Projects
  • Project14
  • Solar Power Devices
  • More
  • Cancel
Solar Power Devices
Blog Project 'GiraSol' - Oliver Schalles
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Solar Power Devices to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oliverschalles
  • Date Created: 24 Jul 2018 2:37 PM Date Created
  • Views 4837 views
  • Likes 15 likes
  • Comments 15 comments
  • parabolmirror
  • photodiodes
  • oled
  • ntc
  • windowlevermotor
  • last
  • i2c bus
  • girasol
  • solarpwrdevicesch
  • ardruino
Related
Recommended

Project 'GiraSol' - Oliver Schalles

oliverschalles
oliverschalles
24 Jul 2018

oliverschalles 24.07.2018 16:05

Project 'GiraSol' - Oliver Schalles

 

Calle Calvario 15
04288 Bédar / Almeria
Spain
0034 664025031

 

 

 

 

**********************************

11th. Update,  from 10. 2. 2020 @ 19:21

A real help  from a  friend:
An Electronic Device  Producer  offered  me  samples  from a highly  precisely Lux 'meter  -  basically  a  one  pixel  camera with programmable  exposure  time  and aperture' ...   and all to talk over  the  I2C bus   ( VEML 6030 )

 

Here I  won in the  contest  for  sun energy  collecting things'- the possibility to choose  from ' precise  electronics and  stumbled over the VEML 7700, a  precise luxmeter - but as I  found out  all devices  have the same  I2C address ( to communicate  with  it) - so  the need to find out a possibility to manipulate  them , to be  able to talk  with one of them 4 - so I asked by  email the Producer, if there  any  posibilities' exist, to switch them devices - with the same  address ?? ..
for  a  single  device of it (VEML7700)  a adafruit library with  an example  program for Arduino, exists. so far  so good .
an hour later I got a  response - "yes, it is true -  you, one cannot readout' individual - devices  with the  same  address,  on the  same  bus ...!"


became  interrupted  -   so  next  time  more  to it...

now:
11.2.2020.

so . what  to do ?  browsing around  and  found  some ideas  -  I2c  switching  devices - switching the  sda lines,   cutting off the vdd to the  devices ...  wow .
and  but  - they   put me on a  different path:  the  VEML 6030 -  a similar  device  to the  7700, but has  additional pins: interrupt  and :  Address'assign!

when that  pin is  tied to gound - you have  a certain -  fixed adress ( 0x10 )  - and when that pin is  tied  to Vdd - than the address  changes  to  0x48.. !

wow . so one  could  communicate  with 2  devices - addressing theirs individual  address - ok ,

but  still the  need of 4 devices -  west, east, horizont  and  zenith  - so again,  switching ??
not so  good .
browsing  again, until I found in a Arduino Forum: https://forum.arduino.cc/index.php?topic=466617.0    THAT idea:

to explain I need to upload  a fast drawn schematic : 

the sensors:  # 1, 2, 3, 4  are  connected  paralell, I2C Bus - sda  & scl, and the power to each device -
and  the  adress input pin of each device is  connected to the  out of the  decoder or  the GPIO pin of the  arduino_  - : when switched high' the address of the device ' switches over to   0x48,  and  the arduino can address / comunicate /  read out ' the  datas..

when that line is  low, (0Volts ) it has  a different address in that array - and  just not listening to',
  when  the  arduino wants  to talk  to someone  who listen to 0x48,  ( like  a telephone  number(!) ) .
.. the  genial thing is:
- for every  I2C device RTC clock, a Oled  Display ;  here, the  light sensores, and its unique features  -  to program' it, has to have a different, unique Library   (in where  is  written the different addresses, often ! )   2  adresses ?   - two libs !!   ( it adds up more  bytes to store in the final program, that sports the arduino... )
- here we just need to communicate with only one  device  at a time  -  and so it will work  to support / communicate with a device that listens  to 0x40 -
- and that will be - all of them 4, here,   (or  10 - if  you 'want') so: when selected, by an high signal from the  arduino  ( by a GPIO Port ) , 
THAT device  will be  able  communicate with the Arduino.
so  only  one lib, only one  program that  has to run 4 times,  after addressing the sleeping (better said  listening to an other address ) device - to establish communication - to stet the parameters  and  to read out,  than switching to other device _ high to the address pin - and  the  same thing over again. ....
I could   use  4  digital out pins  of the arduino - but  for  why - when I can have 2 ?
, just need to - bin'code - the two out lines and a decoding  device  2:4 ( 74'138 ) : it's  out's are connected to the device address pins (after a 5 to 3.3 volt  shift..)  as above in the schematic .. <

for  why  that all ?
I  build up a Photo'diode / tansistor  Array - to get ' infos  about where  at the  sky is brightest  point ? - to track the sun.. yes.

so at fist again a schematic form that array  -  a note  from my  analoge notebook,  a photo from it :

as  we  can see  -  we have  4  PD,  and  a center one  - the  center is intended  to  just  measure  the amount of overall light_   to detect   the   night / day  difference -
  while the 2  pairs, crosswise  - for to detect  the  rotation of the sun -  from east to west over the  day  -  and  the elevation angle  from  morning - horizont  to   noon,  at zenith  and  back to  horizont,  at evening..
so them 2 pairs  deliver ots  analoge  signals  to the  arduino, which detcts the  amount of light  form each, calculate the / a difference  from a  pair ( rotation /  elevation) and gives the  diifference, and the direction  to fire the motors  - high difference  - motor(s)  fast, small difference, motor slow,  and - at no difference:  motor  stop - the mirror is alligned...

Ideas  and  Praxis :
first tests, connecting, test on stability  and sensivity: ( i experimented  quite  a while  to find out  the values  to the correct resistors  and  capacities' .. )

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

by  aproaching the light to one of the PD in the array - one  can see how the indicating LED  responds to it...

here, the idea  - to ' a  functioning PD Array. :
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


and the  final ' aperture:
now the PD's  are 'coated  with black heat'shrink tube  - to prevent light coming  from aside ... imageimage

And  the pcb, is  coated  with  a laquer  to prevent to 'enter atmospheric  influences to the board...

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

so it will be attached to the parabolic  dish:

an overview' :

The 'camara' tilt and pan thing' - is is intended  to 'fine-adjust the 'mechanics  to the  electronics...
so, that the focus is  really  there , where the heat collecting element  is   mounted on !! image

imageimage

so back to the ' help from a  friend -
Vishay ( I am not  in any'ways ' connectet,  '$$' to them ' )  -
but I asked them what to do when some devices , have same  address, blah, blah,
  and long story  short _ they  sent me  - within  4  days  ( Germany/ Spain )
10 samples of their VEML 6030, for free.
but these  devices'  so to name', are as big as  2 by 2 milimeters ,
and  when one of them  will fall on the  floor  - it will be  for ever lost .
..
BUT - they  are  super precise, the datas  one  can read out,  will do  make  sense,  and  one' (Arduino  GiraSol Program') can 'work highly  accurate with it:
to detect:

Where is the sun ???


"... or use manual soldering method ...!"      ( aiiii )

2 by 2 millimeter, each...   mmm . 'image

think, it  will be a big challenge...
Ok..  image image

Thank  you  for  your  time  to read, for  your interest_ image

Sunny  Greetings  from Bedar', Andalucia.

Oliver

**********************************

10th. Update,  from 5. 2. 2020 @ 15:50:

Some of the secret works behind the 'curtain:
(optical) Switches, RS Flipflop, Arduino lead to a State-Machine...

 

The  'State Machine'  - the model I made  from an  old  cd rom drive - and mounted on the carrier one of the switches - the other one  was already attached to the  frame at the other end'point... the  switches triggers the R or the S input of the  flipflop, so that the out of the FF either has  'high': going to 'west', or 'low': going east, depending on the  direction the  carrier  moves..
That model (to get the code for the Arduino, and to see if any obstacles may  occur', BEFORE I  would  let that Program  'sport'  the  real big motor for the  GiraSol... I attached the optical endswitchs to the GiraSol X axis 'recently ', so now, the 'need  for the model... made  some  videos from it :  but I want to start  with the  layout  from the RS FlipFlop,
(drawn in Eagle, exported the design via Lasertoner'transfer on a real, double sided' pcb, etched, drilled  and 'populized it) -  and - was already  build into the  GiraSol -Box, so I needed to simulate on  a breedboad - the FF, for that State Machine 'model... 
The  Arduino detects the low/ high change on one digital input pin, and drives accordingly to it the 2 PMW out lines' - reversing the - one PWM, the other, to ground  - so the motor  spins with its PWM speed this way or the other (clockwise / anti'clockwise) ...

Directly  after power'up these  RS-FF's goes in a  un'definite state (due to components differencies -  small, but...)
So to prevent the toggel'ing to an indefinite  state - there is this build-in condensator (C1, 100nF) - it takes  a 'bit' longer to get completely charged, so that input  (at pin 6) is  a bit longer torn to ground' - long  enough,  to trigger the RS FF, to a definite  state ... 
Here  two channels in the  design, exactly 1:1  - one  for the X axsis - rotation  and one  for the Y axsis - elevation.. 
(in the  final PCB I have 1K to all inputs, the pullup's are 100K,  and the IC is finally a '4093,  a quad CMOS S
chmidTrigger NAND..
I do really  like them cmos digital  ic's , for  you can run them, make them work  on  3  to 15 Vcc !) 
and   - in the JP1  - 1 & 2 are the input pins  for the optical switch signals, and in JP2 you find the out's of the FF..
one of them 2 is  enough to detect  the direction: high or low - (  for the second is  just reversed to the first )
so  i decided to  define: logical '1', 5 volts  =  goWest; and logical '0', 0 Volts -  means  goEast...


image

 

the CD Rom drive..


image

 

the modified drive  - endswitch installed:


image

 

beedboard  FF, motor-driver, while attaching to the model' ..

image


here   you can see that  'model' running - in the background  the breedboard, on witch I built  the  RS FF (one  channel)
nice  to see the outs  from the FF indicated by the 2 LED's - which lits according to the direction the slider 'moves ...
the other switch is a bit hidden under the pcb, for it was  already  installed - I just  used it - as one endswitch.. 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image



the core part of the state-machine  program :  (azimuth =  rotation -  from  east to West, at daytime ,  and  from west, at  evening, back to East , to the morning start position... )

  // read the state of Azimuth input pin:, signal from output of  the RS FF //
  ffAzimuth = digitalRead(ffAzimuthPin);
  if (ffAzimuth == HIGH)                        // if FF Q Azimuth = HIGH => goWest
  {
    goWest();
    // delay(2000);
  }
  else
  {
    while (ffAzimuth == LOW)
    {
      goOst();
      // delay(2000);
    }
  }
}
// --------------------------------
void goWest()
{
  analogWrite(mot_Xb, 0);             // first: Ground
  analogWrite(mot_Xa, speed);
}
// --------------------------------
void goOst()
{
  analogWrite(mot_Xa, 0);               // first: Ground
  analogWrite(mot_Xb, speed);
}

 

all wired, Arduino Nano Driven:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

the  setup  with the  real machine'  via the GiraSol Box; motor drivers and optical endswitches..


no smoke ?  ..  no... image

image

the rotation axis and one optical switch...

image

 

That optical Switch in ' Action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image




the State  Machine in full action. Program uploaded to Girasol Arduino Nano, executing..  image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

L'adar ? image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

so far  for today ...
thank  you  for  your interest, for  your  'patience ...

greetings to you all -  from beautiful (today, not so sunny)  Andalucia...
Oliver







 

**********************************

9th. Update,  from 5. 2. 2020 @ 11:50:

News:

 

still alive - working on and on secretly ...
I am sorry  for  so  long  being on silence  - currently buisy to care for  an elderly man, ( 82 ) and that takes  pretty  time ...

the  dish i wanted to directly  metallize - is  now  covered'  with highly reflective mirror  foil,  and a free'hand test - to the  direct sunlight, was  able  to set a wooden stick on fire  within 3-to 4  seconds when held directly  to the  focus... that, was pretty impressive for me ... image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image






 

 

**********************************

8th. Update,  from 23. 11. 2018 @ 17:30:

The  optical endswitches...

 

 

the  End-Switches…

 

as recognized - the mechanical switches I  wanted to use and installed them already one year ago - they start to rust, to oxidize - so a more durable solution was in need.

image

 

I  googled around in my pile of electronically parts  and  found - some  pair of optical  devices:

an infrared diode mounted in opposite  to a  phototransistor - so the light beam opens the  collector-emitter path.. ( so  a ‚ positive logic‘ )

But, to toggle the electronic in the Girasol -Electronic Box  - it's expecting  a  signal that goes logic 'low', '0‘, so the signal had to be inverted…

 

The final 'switch' is to toggle the entrance (an RS Flipflop ) - the active path - an 'open-collector' draws the input to ground, to trigger ..

 

I need to build 2 pair optical end switches - one pair for the elevation axis, and one pair for the rotation’ ..

 

first schematic:

mimage

 

The detecting electronic works on breed board:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

At right the  'interrupt to the 'light beam device'

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The led indicate 2 channels, and one I grabbed by the oszi..

Its a bit lame, but it works perfect for my small issues - and was 25$..  (!!)

You can see, that the logic level changes from high, ( about 4.2  volts, ) to low, about, 0.7.. 0.8   volts..

Its set that one step on the screen represents 2 volts..

 

Normal ' MHz oscilloscope - one channel, starts at 200$; good ones, with two or even 4 inputs - at _500,  digital storage, too, 1000$,

( talking about hi-end,  - than open end..  goes up at  6000.. (! )

So that device ' I have is a super cheap one, digital, stores as well, all basic functones available.

And I do not megahertz, just to see if that signal chances, and how !   You can see roughly the power supply, if the power is clean '

And that's basically you need for the hobby

 

breadboard,  one pair:

This little board is the soldered version of the breed board ...

I need 2 of them  - one for rotating east/west and the other for the elevation - horizon/zenith:


image

When running it shows the state of the optical switches

Green - no interrupt, Red - beam is blocked, (device is at end point..)

image

image

 

 

 

the  second device,but now with ic socket.

I removed  unnecessary pins and left over  the 'active pins in the socket' s

 

the TD62503 consists of 5 transistors - the base as open 'input, and an open collector 'output, basically - 
and all emitters are connected internally to pin 8..
Only  4 of the transistors I used : the 4 inputs -  and 4 open collectors (200 mA each) - and the common emitter:
image



image

 

 

connected  to :

image

The yellow/green gives the signal; Red - positive for IR Led, black  - commune negative, ground...

So have  2 pairs of  detecting boards with the 4 sensors -the return points at east, west, horizon  & zenith

 

When the machine runs 'into'an (optical) switch at its  end'point, it has to stop and do reverse (by the GiraSol - Program ):
these are the detectors, to tell the program and 'it asks - is there, at that pin, connected to Arduino -  a high ( 5 volts,) or low' - logic, = 0 volts ??

 

The following electronic, directly after, is to store the way  (direction where to go )  - a toggle - RS FlipFlop tells', stores the state - if east  or west switch is ' triggered, it changes its output state:  on its tour to west = high', going to east = low'..

West tour ends' up  - at that detector when it runs into, 'triggers‘ the switch, and the prior high signal now goes low ... = now, go east,  - until you' hit the other end - the east switch..

 

The signal cooking, signal shaping' and toggling, does the hardware before the arduino..

The whole action is focused on - if one of them 4 reaches the switch, the toggle action is performed - the toggle line is connected to arduino, and the other toggle signal - as well to the Arduino. One of these signals ( high/ low) triggers the 'Service Interrupt Routine', ( at pin D2/3 )  witch calls a routine, wto look what state that toggle signal has:
all members in the program is now informed, that the 'goto-west' direction has changed - now it shall 'go east'.

 

for having 2 motores, all has to be double, so 2 interrupt pins, and 2 toggle signal pins..

So the need of 4 detectors…

***

so far,  theoretically …

 

Next day I found out, that the strange behaviour (sometimes a randomly’  triggering)  of one pair I recognized - at test phase with them big' ones, -

was due  a mistake I made:

I assumed that the devices were build up similar, consisting just one  IR LED and a Phototransistor - but after a check and download the data sheets -

I saw that the bigger ones were completely  ready image  - no need for a resistor for the IR LED:
just to  connect to  Vcc, Ground  -  and having than, the open collector to use ( iCE  @ 40 mA ) …. image

 

The 'small' one from sharp is the simple version, diode / photo transistor.. 


- the big one has it's electronic' already built-in:image

So I needed to skip, simply, just short out' the 350 ohm resistor, to sufficiently power up the device.

 

The resistor - limited the power, the device needed to run fully: so that strange behaviour is/was 'caused by not sufficient supply voltage..:


imageimage

 

 

the cables  have  to be  well 'isolated -  not prior against electricity  - but against moisture..
to identify: the + pole is the shorter one .. image

image

now, than: measuring cable' length, attached some jacks, designed the PCB where the two pairs of signals have to go in,

to be shaped and amplified, to go to the GiraSol-Box'

 

A spiralchord from an telephone gives free movement for the senselevation detectors, of course, they are moving with the mirror, so there the rotation'..
image

 

Now, the last 3 days  ‚in’ to build a lil board that does, in fact, trigger the switch inputs of the GiraSol-Box,

Had to open the box to see if my cable to them devices having the same color-lines connected throu'..

 

And that thing, the attempt’ was OK, but did not work to trigger:


image

So I've had to change the design, and found a even better solution :

 

now the final’ switch/trigger/contact to the  RS FlipFlop -  will be done with optocouplers ( its  IR Diode  in series  with the visible LED) The open collector,   draws the input 'low, perfect to trigger !!!

It does it’s  work,now,  yesterday evening until this  morning  -  reliable, all states  were fast and well recocnized and super stable':



Right, bottom, the cable jacked in'to the GiraSol.box...


imageimage

the  6 wire cable  to the output pins have to have a socket’ to the cable to push-in to the jack of the  GiraSol Box…:

image

Red is Vcc ( +5V)

white is ground,

Black - west

Yellow - east

Green - horizont

Blue - zenith

(Lakota colours to the directions)

 

 

 

It works like a charm...

Set & reset,  by 2 devices, 4 sensors, - connected to the GiraSol.Box:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A one year task: now ready, done ..

These sensors I found in a big copy machine and  had them all in my ‚scrap box‘

 

2 months ago, the optocoupler I used  here (4 in one) came from Farnell, from the price I won on here, on Element14 !!  ( Huuuurraaaayyyy !!!!)

So all came together at the right time..

 

These optical switch devices - now - has to be mount to the real machine..

Next steps lead to new updates… image

 

 

warm greetings, despite from pretty fresh and wet weather, now, in Andalucia..

Oliver

 

 

 

**********************************

7th. Update,  from 23. 11. 2018 @ 14:30:

reorganizing the 'blog, for better radar'bility:


now the  updates  are  ordened chononogically:

 

actual...

...

...

...

oldest ...

 

Oliver

 

 

 

**********************************

6th. Update,  from 19. 10. 2018 @ 23:06:
a biig 'Thank You' to the Element14 community :

 

The resistors and the ic's.. :


image

It's just a small part of it, the other electronics I received 4 days later, after choosing from all  their  components from Farnel

 

I did not expect them any more - for, due to the high shipping prices, I e'mailed to Tariq - who finally did the order for me, that he should skip the resistors  -
but as I saw today,  he must have 'ignored' it, and so, the resistors were sent to me..

so  again - Thank  you  so much image

Oliver

 

 

 

**********************************

5th Update,  from 17. 10. 2018 @ 20:08:
the cleaning, polishing action, with abrazive whitening toothpaste - and the diy - polisher..

 

the  material to polish  image :


the tool to it  image :

image

 

And, the result from today.. ( better as I thought )  - the 'reflectivity' - after1-hour polishing  -
I even could hear the different areas where it was dull while polishing'..

 

After working on, the sound legalized to other already done areas:

the better, finer, smoother, the better the reflective layer, every fanit scratch, or dullness, one can see, alike magnified on the result.

They say that silver layer one can add-on, thicker, to legalize scratches, but have no experience, practical, until now..  ( as it would behave as a 'filler.. I've to see )

After the polishing action, I sprayed, cleaned at first with tab-water, then with distilled..

of course - with my sprayer ...


The weather was nice, no wind, not too hot or cold and a clear sky, perfect working conditions.
Hope the weather will be good tomorrow, so I can do the final polish...

greetings to  you all - from Andalucia -
Oliver

 

 

**********************************

4th Update,  from 16. 10. 2018 @ 22:06:
the working double-spray-on-air-pistol' ...

 

as I promised I took a 'clip (this  afternoon)  from the  working' pistol' - here water - and a dry wooden board to show. :

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


 

The best - ok, it works like a charm, too - it takes from the two bottles the same amount of liquid (!!!) as intended:

image

Next step's:

The last two polishing action - a toothpaste which whitens the teeth, abrasive, soft, and the last polish with normal toothpaste - even finer the abrasive,

- for not able to get here cerium dioxide, or titan dioxide as a fine powder, thought about to use talcum powder, but it has different, coarse grains in it.

So thinking about car polish liquid, but that is waxed or has silicone in it, and - looks nice, but as a bonding to the silver layer? Catastrophe.
Need to remove any faint of silicone than, and that would be more work, and disappointing, for it is not a real polish, but a masking, filling to the fine grooves in the lacquer, the dull, abrazed surface...

So I ended up with toothpaste, for its water-soluble and so for removable from the dish, no fillers, just real fine polishing action...

After the dish is finally polished, I need to clean with all I've in hand, fluoride, from the toothpaste, shall be removed with sulfuric acid - on the surface, after the acid, I'll remove, neutralise

with a strong base, then a water de'tensifier, and distilled water to clean all up...

I can see how the molecules work to each other !! image


the last two days  - a lot of rain, here...
greetings  from Andalucia image

Oliver

 

 

 

***************************************************************
3rd Update,  from 12. 10. 2018:
how to 'mirrorize', to make the dish 'highly' reflective -
the  need  for  a double-spray-on-air-pisol' - and the DIY build:

 

 

................................................................................

At first:

I have to, want wholeheartedly' say a  biiig "THANK YOU" to all here, in the community,  for the price I won - and for the help I received ...

I could choose the electronics - and all came to my hands -  and it felt like having Christmas!

It was  really  thrilling for me  image 
..................................................................................

I will go on with the updates - likewise logical - the last entry, down'under' was:  - how to silverize that dish-  and found out, that I do need a finer mist to spray on. -
this garden-pump-sprayer - they made too big drops, and the handling was pretty challenging.. (the liquids from each bottle has to be sprayed on, simultaneously ! ) 
so I looked for an other, better solution since than.

My neighbour Christobal lend me his air compressor - with a dust blower pistol, from which I unscrewed the tip -  and looked around in my boxes of material' and ended up with some  connectors and rings  - from the garden hose. The connector, to attach the end of the hose - fitted ' accidentally ' perfect in the pistol: I even could screw it on'- with a ´bit of force, so - it was perfectly tight.

image


now - I could use the pistol it to fit anything on it!  (a ' female' connector)
after that 'important step'  - I looked further on - the male connectors to it - found two -  which I could screw-on each other.
One of it I extended the outlet - with a PVC tubing,  some  8 centimetres - to have the outlet for the air.


My idea - then: letting end fine tubings at the outlet, so the air will take the liquid out and form the spray...
to add in 2  little tubings from a  venofix butterfly (the med-doctors use them to get a blood sample from off your vein') .
I just wanted to let them end, in the endpiece...

image


but how to get them in that housing?
I drilled  2 little holes on each side of the endpiece - oppositional' than I cut off the needles and pushed the little tubings into the housing - one left, one to the 'right -

and long enough to end up in the nozzel. A drop' of CA glue, tightend the drillings... :

image

 

the end-piece:  all parts in place:

image

But, that 'construct' worked - for just around 5 minutes:
The air stream forced the ends of the fine tubings to vibrate -  and so the ends destroyed themselves by hitting to each other ...

MMMMM... image

 

The need to reconstruct  the entire 'end-tip':
A concrete airflow, a housing for the end of the fine tubings. Form metal. Glued, fixed together - like a pack of three.. :

wow - and again,  hovering the house, was looking in all boxes, cartons. And I found' a radio antenna. The last end part was fine,  but was it thin enough to fit?

image

 

tube,  red shrinktube, metal tube,  the end of the flexible, a toothpic in the lumen' :

image


Cutting, measuring, recutting, until all the 3 ends were in place - the tubing outlets for the liqids and the air tube. Before glueing the fine flexible tubes, the ends - into the fine metallic tubes, I pushed in the ends, in the lumen a tip of a waxed toothpick - to prevent that any glue would clog up the fine outlet.

image

 

airtubing and the 2 liquid dispenser tubings - that tiplet - to get in place:

image

 

here in the housing, starts the airtube:
image

After the ends were fine and cured I added the longer air tube - fixed altogether by shrinktube, some epoxy to the triplet and all at, in' the end of the PVC nozzle...

 

shrink tube forms the triplet :

image

 

a bigger shrink tube all around, to tighten all up and to stabilize. - the shorter tip is  the air nozzle (red) :

image

 

all in place, ready to connect:

image

That construct works like a charm. It draws about 1 ml every second to nebulize...  image

Now,  how to attach the little tubings to the liquid bottles, and a holder for the bottles -  to that pistol ?
browsing the house, an empty 5-litre demin water canister would do it ':

cutting away the half of it from top to down, cutting away the unused parts -

at top of that construct a big hole to fit on to that pistol, to the garden hose connector... :

into the open syringes I can add some filter material, and they guarantee that the tubings will be well 'supplied, always submerged in the liquid..
the bottleholder, 2 x 0.5 liters:

image

 

the center drilled caps with the superflexible liquid-tubings:

image

after all testing all has to be cleaned, all, the working marks...  yes... image

next step - waiting on good weather, to clean the whole dish thoroughly, to give last polish on it, and than, the setup of new  silverize-fluids -

the  activator - ( tin chloride );

the  silversolution itself  (silver ions  bound in 'aminoacid-complex')

and the  recductor - (glucose and a vitamin C, organic  acid image )

further above, in the previous update, I posted the more complex receipt to it.
the tin chloride, the activator,  -  I will spray on with the pump-sprayer. 
and for the reductor and the  silver solution, I will use that new -

Double-Spray-On-AirGun

image

so long - i ll keep you updated !!
with nice  regards and  greetings  from Andalucia -

 

Oliver

 

 

 

**********************************

2nd Update: from 23.09.2018
the history  about  to choose  the dish, and  - how to 'mirrorize', making  it 'highly' reflective:

All them 'parabols' I had im my hands were coated, of course - the one I used here, shown in the video, has a core from aluminium with is massive 'coated'  glass fibres X epoxy (structures on the backside)  and a  fine layer of it on the front..

I wet-sanded the front, with 150, 300, 500, 800, 1000  up to 1.500 - the parabol' was  laid up ward, and I filled the parabolic gap with water and some drops  of a  dishwasher, detergent'

My grinding tool was a 30 cm round tap from a small rubbish bin...and I just followed softly (!!) the form, curve -  not to change the geometry...

than the question:  which way to use - to make that parabolic area highly reflective?

:

Aluminiumfoil ? , space blankets ( mylarfilm, golden and silver reflective )? adhesive reflective foil? silverize by chemics?  wow.

a loot of ways,  one as bad and unpractical, as cutting the foil in stripes, glueing them, step by step, to cover the entire area, (glueing?  - with what? - a glue that contains thinner in order to evaporate to cure'  - how will that solvent go through mylar, a tight foil ?  - no way. , so 2  components epoxy?
Idea good' (no thinner need to evaporate) - but:
Wow, what a procedure  - to get the glue on, in a fine coat? You see every irregularity in/of the geometry of reflexion: even the faint layer of epoxy ruined the surface... 
And, additionally  - after a  year, the entire work starts to get dull on the cut edges, and the mylar film 'brittled' loose, and leaving the metallization randomly on the surface: very, very bad. - Frustrating-No-Way. ...

Than, finally, I found a 'patent' to silverize 'ANY surface'  as they claim - it made sense to me - and I started to achieve all the stuff I needed for...

Made the liquids, and tried'out  - on a  glass plate, to see if the chemismus worked - and it did.

The liquids need to be adjusted in concentration, and I found that the pump spray devices (garden center) do spray, work - but the produced drops are too big, so I need finally an air-compressor  - for a finer mist ...

The silverizing solution and the reductor liquid has to be sprayed on, simultaneously and while meeting on the surface, it forms pretty immediately a fine reflective silver layer -  from 10 µm to ...150 , 200 µm, depending on low long you treat the area.

On the  glass plate, I found areas, where the  silver layer was tightly  bound to the  surface - and  areas,  where  I could  just wipe the  layer off, with my  fingertip, but it was not intended  to silverize, its intention of the probe was to see if the liquid' work as intended...)

It is highly depending on how clean you (can) work. Every fingertip, every particle, or a faint residue' of oil, grease, fat, will hinder from bonding..

The liquids have to be made with demineralized'- or even distilled water, all rinse-procedures have to be done as well of course-  with dest/demin water ...

 

the 'receipt: liquids to silverize...
image

 

Activator, reductor  & silver in solution (light sensitive ! -  so I wrapped the bottles in alufoil...)
image

 

the  3  pumpspraybottles -  at the  location of the  test  - outside in the patio:

  (and  it silverize nearly  all, but, a bit nitric acid, diluted -  will swap it all clean again ... image  )

image

 

overall silver ! - here  to remark: at the  areas  where the  activator  could  reach - there, the  layer  is  very,

very  tightly  bound -  even to ceramic... !

image

 

the outcome from the first test, a  spray on, some 4 seconds.  So the layer is ultra thin and the object has to be highly clean before...

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


the  3 liquids:
1.: the activator contains stannum, tin ions (tin chloride) that gives any surface the possibility that the silver will have 'starting points -

from where the micro crystals do grow from - to form the metallic, conductive silver layer.

 

2.: the 'reductor' is based on organic acids, glucose (kind of sugar), and vitamin C

 

3.: the silver solution -  the main ingredient: Silver as 'nitrate (water soluble) and an organic complexer' (Glycine, Amino'aethanol) that 'carries' the silver-ions..
When the reductor and the silver solution meets at the surface - the silver (iones) will be reduced to metallic silver - the reflective layer... 

so far the metallizing actions - when I do spray it on the parabolic  - I let you know from, of course .. image

when once - the reflective layer is applied -

I have to clear it out, even to polish at certain areas - and then there is the need for a final UV protective, clear, fine lacquer coat,

witch the silver protects from atmospheric influences...

Oliver

my  facebook

account - if someone wants to contact me there, too,  you are welcome!
https://www.facebook.com/oliver.schalles.9
image

 

 

 

**********************************************
1st Update: from 19.09.2018
the 'new construction to the elevation axis -

 

 

the force  was so strong

that  the old rod nut  was

pushed out of its harness...

wow.  - I was looking for a new possibility to order the entries -  found until now ' nothing -  so I will append the material I do have.
Today  I  completely  was  able  to renew the elevation 'system:
the motor, the connection from the motor housing, case to the bear 'ring'housing was wobbling, so I used just a piece

of a wider metallic tube and resined (epoxy) the gap in between the housing of the motor and the bear'ring housing... perfect tight and rigid, now. ( some days ago ) ..
The rod nut, in its housing ' rod-nut-holder' -

a long 'nut, hexagonal, glued in - as well with epoxy. To make it  'fit in - I widened the existing channel, and

dremel'ed in, the hex profile,  so

the  long nut finally fitted in..

As  well some  days  ago

.
and  the

todays

' work: the strengthening to the  sides, which carry, will hold the rod nut'-holder...  (the  nearly  triangular pieces of metal, with the

bore hole

for the  axis) - glued to the

innerside

of the down-under-part of that parabol.. :
image


Here to see the motor, the rod and the housing of the hex-long-screw-nut', and the triangular strengtheners':



the hex-nut, glued in the holder (epoxy)
imageimage

 

the triangular strengthener'
image

 

does all fit to each other?
image

 

close'up of the hex-housing'
image

 

aside: the nut's, M6, Inox
image

 

the motor,  the black tube to the  housing,  and the silvery tube-housing of the  bear'ring:


a  shot from below, upwards: motor, rod, hex'housing, attached  to the bottom of the paraboldish;
      above the motor: the elevation axis..


.. about 55 degrees


imageimageimage

last year, what's  today's  left over - from the polishing  action ( without the  reflective  silver layer  !)

the laser beam reflects at first spot, to the second, to get reflected to the third. :
(5mW 405nm):

image

 

horizont' position - at  evenings and in the mornings.. (we  will see  image )

image

the  coloum cacteea in background are  Trichocerus - terchekki, -peruvianus & -panachoi.. image

I was totally overwhelmed - that more than 13.8 K visitors had sawn my project.
  and - I do 'Thank You' for your time - to see, and look and follow, or even comment.. image

A good day,  a good night - wherever you are - hope you are ok,  and  well -


greetings  from Andalucia, con mucho sol -
- Oliver

 

 

 

******************************************************************

My first entry from  24.07.2018 16:05

I am completely new here (joined today) ...

... and  have no idea about the  'what's about',  but I do work on a  'heart' project  - my  'GiraSol' Project, which I wanted to share  with  you :
its a 'device, consisting of a  reflective parabolic  dish, that collects  sunrays, energy  to a  focus  where a  converter' (copper pipes in where  a fluid  gets  heated  up and  is  lead to an isolated boiler, where the  heart is  given into it, to the usable water - for  a hot shower  or to use to wash up the  dishes  in the kitchen - it even could  be used  to heat up a  floor in the  house...
the  sunfollwer electronics, Program to calculate  is  made  for an Arduino Nano, it has  8  analogue 'In'put pins :

5  for them photodiodes, 3  for the temperature from the boiler


2  big motor driver ic's IBT ( h.bridges  for DC' motor's ), to drive by  PWM the rotation motor ( east-west )  and the  elevation motor ( zenith-horizont )

the  sensors are made of 2 pairs of photodiodes, and a centre PD, all in all, 5.
4 End-switches, to detect the max'mechanical limits  - after 2 Schmit-Trigger RS FlipFlop - polled' to  2 interrupt pins..  ( on D2, D3 @ Nano )

The  thermor  has got its own ArduinoUno - 
for the 3  NTC - and the mechanical overtemperature switch

the temperature - coming from the  Parabolic  Dish, to load the thermor,

the  water'temperature  'absolute, in the thermor, and -

the temperature at the out'let  - back to the focus,  to get reheated there again...

 

OpAmp followers  and  one comparator, to detect overtemperature,

a 0.9' Oled Display to show the current temperatures -
a pushbutton to show up the data on b.press..

I have  a load of photos already posted on Facebook on its  'project page - here: the link to it:
https://www.facebook.com/Project-GiraSol-1605063979506661/
shall i do upload them photos / clips  here too??  and if yes - where to ?  - I definitively need help not to get lost here ...

Greetings  from sunny Bédar, Andalucia, South Spain..

Oliver

 

 

 

first  steps - 2  photodiodes, arduino nano, the  sketch - listed  below -
the motor  driver, the dc windowlever motor, connected to the rotation axis:
(a rear-axis  from a opel astra, without all them mounted  stuff on it.. ) :

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Overview:  in front the  Parabol, in the back, the thermor in which the energy will be stored in'..image


a test to  pan, tilt the  system, to see how it responds to different voltages:
dc motors do reverse the direction of rotation when we do reverse the connections of the dc voltage.
the speed is pretty  high  with  current, steady 12 V DC - but in work modus',  the  speed is  really, really slow - realized via the  PWM... '
PWM: tiny spikes of  12  volts -> very slow motion;  5 ... 10%
longer, wider  spikes: half impulse <>  half delay' - forces to spin faster: 50 %
and real big ones,  long impulses witch nearly flowing to each other:  the motor spins really fast ...  90%:
These impulse and pause times were repeated in nearly 1:1.000, 1:500 seconds interval.. (Arduino et al. ) depends on which pin is  assigned.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image


the  GiraSol-box - the  Arduino Nano as the core - and two  mighty dc motordriver for the  asxis's:

image

Attachments:
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
  • oliverschalles
    oliverschalles over 8 years ago +5
    Thank you for your comments, mcb1, 14rhb - yes, I had a looog research time on U'tube', forums et al' - and finally found an old sattelite dish, here in Spain, that they are easy to achieve (used) - and…
  • 14rhb
    14rhb over 8 years ago +3
    Hi Oliver, I watched your videos which are really interesting. The speed of your dish made me smile Good luck and I'll be interested to see how you get on; looks like you've achieved a lot already. Ro…
  • oliverschalles
    oliverschalles over 8 years ago in reply to 14rhb +3
    Hi Rod - yes the speed from the rotation is pretty fast - as i used plain 12V DC to powerup the motor, just to see if the mechanics are ok'; but when the 'dish' is on 'work modus - the pwm amount is dirigated…
Parents
  • 14rhb
    14rhb over 8 years ago

    Hi Oliver,

     

    I watched your videos which are really interesting. The speed of your dish made me smile image

     

    Good luck and I'll be interested to see how you get on; looks like you've achieved a lot already.

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oliverschalles
    oliverschalles over 8 years ago in reply to 14rhb

    Hi Rod -  yes the  speed from the  rotation is  pretty  fast -  as i used  plain 12V DC to powerup the motor, just to see if the mechanics are ok';


    but when the  'dish' is on 'work modus - the pwm amount is  dirigated  by the difference of them photodiodes :
    differences  in between them west-east PD iex - the  motor  runs in the  direction of the  most light receiving PD,  and the  difference  in between the  pair - will set the speed via pwm; so:

     

    big difference  =  fast
    less difference  = slower
    no difference ( alligned to the  sun ) = motor  stop...

    so - I get soft movements, soft accelerating  and braking' forces, to the mass' of the dish - the  whole  construct ontop is about 16 -18 kg !


    Thank  you, for  your  attention  !

    Oliver


    here  one channel  basic  code for the arduino ide - that program runs  the motor due to the  received  light - cw or  ccw - with  different  speeds.. ( the  first video i posted )


    /*
    2 Analog input, 2 analog PWM output, Differenz, Dir; Serial output
    */
    
    
    // These constants won't change, they're used to give names:
    // Hardware: AnalogInputPins:
    const int analogInPin_xa = A0;      // Analog input pin that read'in deltVolt/dV from the PhotoDiode XA'
    const int analogInPin_xb = A1;      // Analog input pin that read'in dV from the PhotoDiode XB'
    
    
    // Hardware:
      //set Analog(PWM)OutputPins:
    const int x_mot_a = 10;             // PWM output pin the (indicating) DuoLED is attached to; PWM = 10 / 11 ='0'- clockwise.
    const int x_mot_b = 11;             // PWM output pin that the DuoLED is attached to; PWM = 11 / 10 ='0' - counter clockwise.
    
    // set DigitalOutput Pin:
    const int dir_led = 13;             // digital pin (13) is already conected on pcb to '+ LED, via resistor to GND.
    
    
    // Software:
      // variablen
    int val_xa_in = 0;                   // variable is to set = 0
    int val_xb_in = 0;                   // variable is to set = 0 
    //
    int speed_xa = 0;                      // value output to the PWM (analog out)
    int speed_xb = 0;                      // value output to the PWM (analog out)
    //
    int diff_x = 0;                      // Differenzwert der beiden PhotoDioden xa, xb
    int dir_x = 0;              // (if) dir.x_bit = 0  -> go 60°, Ost   (if) dir.x_bit = 1 -> go 300° West..
    
    void setup()
    {
      // initialize the digital pin as an output.
      pinMode(dir_led, OUTPUT);
      // initialize serial communications at 9600 bps:
      Serial.begin(9600);
    }
    
    void loop()
    {
      // read the analog in value:
      val_xa_in = analogRead(analogInPin_xa);
      val_xb_in = analogRead(analogInPin_xb);   
     
      // print the results to the serial monitor:
      Serial.print("  PD XA = " );                      
      Serial.print(val_xa_in);
      Serial.print("  PD XB = " );                      
      Serial.print(val_xb_in); 
     
       if (val_xa_in < val_xb_in)       // wenn diode xa(ost) 'grösser' (mehr licht erhält/höhere spannung)
        {
           dir_x = 0;                                                        // dann Dir = 0
           diff_x = val_xb_in - val_xa_in;                        // Differenzwert x = %PWM 
           speed_xa = map(diff_x, 0, 1023, 0, 255);        // mapping des Messwerts in PWM 'Einheiten'
    
           analogWrite(x_mot_b, 0);                                // first do 'GND'!
           analogWrite(x_mot_a, speed_xa);                   // than PWM to Pin; clockwise!
           digitalWrite(dir_led, HIGH);                              // 'go ost' = LED on
    
    
           Serial.print("    Diff % PWM = ");
           Serial.print(diff_x);
           Serial.print("   PWM an 'xa = ");     
           Serial.print(speed_xa);
           Serial.println("  -> Ost ! ");
         }
        else                                              // wenn: 'West' (xb) grösser ->
        {
          dir_x = 1;                                                               // dann, Dir = 1
          diff_x = val_xa_in - val_xb_in;                              // Differenzwert x = %PWM 
          speed_xb = map(diff_x, 0, 1023, 0, 255);          // mapping des Messwerts in PWM 'Einheiten'
    
    
          analogWrite(x_mot_a, 0);                                  // first do 'GND'!
          analogWrite(x_mot_b, speed_xb);                   // than PWM to Pin; counter-clockwise!
          // digitalWrite(dir_led, LOW);                              // 'go West' = LED off
           digitalWrite(dir_led, LOW);
        
          Serial.print("    Diff % PWM = ");
          Serial.print(diff_x);
          Serial.print("   PWM an 'xb = ");     
          Serial.print(speed_xb);
          Serial.println("  -> West ! ");    
         } 
    
      // wait 10 milliseconds before the next loop
      // for the analog-to-digital converter to settle
      // after the last reading:  was 2  - set to 10 - a 'bit more time to 'settle those 2 IN-Pins, pwmOut & serial-print..
      delay(10);                    
    }


    image
    Oliver








    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • 14rhb
    14rhb over 8 years ago in reply to oliverschalles

    Oliver,

     

    Great progress and code.

     

    Just for information, if you have code in a post that looks like this:

    void setup()

    {

      // initialize the digital pin as an output.

      pinMode(dir_led, OUTPUT);

      // initialize serial communications at 9600 bps:

      Serial.begin(9600);

    }

     

    you can highlight it, click on the ">>" format button, "syntax highlighting" and the "C++" and it then looks like this:

    void setup() 
    {
      // initialize the digital pin as an output.
      pinMode(dir_led, OUTPUT);
      // initialize serial communications at 9600 bps:
      Serial.begin(9600); 
    }

     

    regards,

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oliverschalles
    oliverschalles over 8 years ago in reply to 14rhb

    Thanks, Rod - yes,  i will try  to get it alike, next time  when I  do post code'

    it  really  looks  better  and is  easier to read  and  discuss  -  just  better image
    regards , Oliver

    ps:
    i just made it' to the code above  -  and it works genial: again , thank you !!!
    Oliver





    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oliverschalles
    oliverschalles over 8 years ago in reply to 14rhb

    as i  coded the  thermor  program, to measure the 3  different temperatures - ( connected  via serial to serial monitor - Arduino IDE on Mac ) I could  set the threshold temperature via  keyboard,  - BUT,  than I  implemented an Oled  display,  and since then the  serial  did  not work, the  program on the arduinowount work as well - it  was trapped in the  setup routine - setup, reset, setup, reset etc. and  again...
    as iremoved  serial' part ( all of it )  the oled worked ( ada fruit library), and showed all data correctly ...  
    here:

    //** based on: https://www.allaboutcircuits.com/projects/measuring-temperature-with-an-ntc-thermistor/
    /*
     3 NTC: In, Out &  Absolute Temperature in Thermor
     if deltaT - differenz in / out is low,  on low temp =  collect energy - no blur!
     if deltaT is low at high temp - ‚ blurr out off focus; less diff (in/out) : more blurring‘  (looking sideway: off focus) 
     over_temperature: umbra - overtemperaturswitch set: immediate blurr!!
     
     A.Uno on:  /dev/tty.wchusbserial620 / 410 - russian driver - same  as A.Nano-GiraSol 
     A.Uno_Thermor: to measure 3 analog NTC'Values/'temperatures: in, out, absolute
     
     Pins used on A.Uno - Thermor 
     A0 ntc_abs, white to Nano temperature in thermor, absolute
     A1 ntc_in,  yellow from collector to thermor
     A2 ntc_out,  blue from thermor to collector
     
     D8     Button           as ‚in‘        Button' to press, to see the display 'PullUp' 
     D9     TempMax          as ‚in‘        Thermor Overswitch - 
     
     D10    green as ‚out‘ Led
     D11 orange as ‚out‘ Led
     D12  red as ‚out‘ Led
     
     
     A.Nano - GiraSol
     D2 umbra           as ‚in‘ harware/ software - OVER Temperature alert'
     A5 ntc_in,  yellow ADC Val FROM collector to thermor
     A6 ntc_out,  blue ADC Themperature from thermor TO collector
     A7 ntc_abs, white ADC Temperature in thermor, absolute
     */
    //======================================================================================================
    // Library:
    // for OLED Display:
    #include <SPI.h>                             // (??)
    #include <Wire.h>                            // AnschlussDrähte 
    #include <Adafruit_SSD1306.h>                // Bangood Oled 256x 128  
    #include <Adafruit_GFX.h>                    // grafics Lib. 
    //
    #define OLED_ADDR   0x3C                     // address OLED ADR: 0x3C (as  contrary printed on pcb: 0x78 !)
    Adafruit_SSD1306 display(-1);                //  no reset, only  2  wire   SCL / SDA - interface, 5v Supply !!
    //
    //-------------------------------
    // Physical Pins @ ArduinoUno:
    // AnalogInPin:        Where the ADC samples the resistor divider's output
    const int AIP_ntc_abs = 0;        // AnalogIn temp, absolute white
    const int AIP_ntc_in = 1;         // AnalogIn ntc_in yellow
    const int AIP_ntc_out = 2;        // AnalogIn ntc_out            blue
    // DigitalInPin:
    const int DIP_Button = 8;         // D_In pin
    const int DIP_Umbra = 9;          // D_In pin
    // DigitalOutPin:
    const int DOP_Green = 10;         // D-Out pin
    const int DOP_Orange = 11;        // D-Out pin
    const int DOP_Red = 12;        // D-Out pin
    
    
    // --- Buttonstate ---------
    int buttonState = 0;   
    
    
    //--- constants: -------------------
    const int MAX_ADC = 1023;         // 10 bit ADC:  0 ...1023
    const float BETA = 3974.0;
    const float T26 = 299.15;         // [K]  26°C in Kelvin - 4 all Calculations 
    
    
    const int RT26_abs = 19610;       // [Ohm] NTC_abs @ 26° = 19.61k
    const int RT26_in = 11820;        // [Ohm] NTC_in  @ 26° = 11.82k
    const int RT26_out = 11040;        //[Ohm] NTC_out @ 26° = 11.04k
    
    
    const float Raux_abs = 2178.0;    // [Ohm] Raux -abs
    const float Raux_in = 998.1;      // [Ohm] Raux -in
    const float Raux_out = 998.1;     // [Ohm] Raux -out
    
    
    // --- variables: --------------------
    int ntc_read_abs = 0;             // Integer for ADC Values (0-1023) 
    int ntc_read_in = 0;              // Integer for ADC Values (0-1023)
    int ntc_read_out = 0;             // Integer for ADC Values (0-1023)
    
    
    // --- currentTemperatures: ----------
    float TempC_abs= 0.0;             // [C] Temperatur, absolute in Thermor 
    float TempC_in= 0.0;              // [C] Temp IN  from Collector to Theremor  c2t
    float TempC_out= 0.0;             // [C] Temp OUT from Thermor to Collector   t2c
    
    
    // for Umbra-set by Keybord, via Serial/USB, connected to UNO --------
    int umbraC_abs = 0;
    int TempC_abs_max = 60;           // Startvalue': temp cels abs maximal.. 
    int TempC_abs_hys = 0;
    // 
    // Strings$ for OLed --------------
    String state = "               ";     // leer$
    String state1 = "Ok, Charging";       // orange
    String state2 = "Ok, Ready";          // green
    String state3 = "OVER-TEMP";          // red
    /*
     algo mas  ?
     */
    // =========================================================================================
    void setup() 
    { 
      // --- pins to use by names: ---
      pinMode(AIP_ntc_abs, INPUT);                // AIn Pin        NTC amnalog in's
      pinMode(AIP_ntc_in, INPUT);                 // AIn
      pinMode(AIP_ntc_out, INPUT);                // AIn
      // --------------------------
      pinMode(DIP_Button,INPUT_PULLUP);           // DIn pin        Buttonswitch: show Display,Content, Pullup
      pinMode(DIP_Umbra,INPUT);                   // DIn            thermor'overtemperature switch
      // ---------------------
      pinMode(DOP_Red, OUTPUT);                   // DOut Pin        Led's
      pinMode(DOP_Orange, OUTPUT);                // DOut
      pinMode(DOP_Green, OUTPUT);                 // DOut 
    
    
      // --- initialize and clear display
      display.begin(SSD1306_SWITCHCAPVCC, OLED_ADDR);
      display.clearDisplay();
      display.display();
    
    
      // --- display a line of text (Logo) 
      display.setTextSize(2);                      // 1 = small, 2 = bigger, 3 = very 'big 
      display.setTextColor(WHITE);
      display.setCursor(1,10);
      display.print("GiraSol");                    // Logo: "GiraSol"
      display.setTextSize(1);  // 1 = small, 2 = bigger, 3 = very 'big
      display.setCursor(1,40);
      display.print(__FILE__);
    
    
      // --- update display with all of the above graphics
      display.display();
      delay (3000);                                // 1000 milicesonds = 1 second pause
      display.clearDisplay();                      // clear, new
      display.display();                           // show up'  - even its cleared !
    }
    //===============================================================================
    void loop() 
    {
      // ---  Hysterese temp @ Thermor to prevent toggele -----
      TempC_abs_hys = (TempC_abs_max - 20);  // Hysterese temp @ Thermor: 
      //
      TempC_abs = readNTC_abs();           // call subroutine
      TempC_in = readNTC_in();             // call subroutine
      TempC_out = readNTC_out();           // call subroutine
      //
      delay(500);                          // pause, 1/2 sec...
      //
      //-----------------
      // read the state of the pushbutton value:
      buttonState = digitalRead(DIP_Button);
      // check if the pushbutton is pressed. - if it is, the buttonState is 'logic HIGH (+ 5 Volt) 
      // if (buttonState == HIGH)          // input pin without pullup.  sw- pressed = input = high
      if (buttonState == LOW)              // input pin 'pullup: when switch pressed = input = low
      {  
        // --- datas to VRAM OLED
        display.clearDisplay();        
        display.setTextColor(WHITE);
        display.setTextSize(1);
        // ------------------------
        display.setCursor(3, 3);
        display.print("Absolute: "); 
        display.setCursor(65, 3);  
        display.print(TempC_abs );
        display.setCursor (100, 3);
        display.print("C"); 
        // --- Umbra C from Keybord via  USB Serial
        display.setCursor(3, 15);
        display.println("MaxTemp: ");  
        display.setCursor(65, 15);
        display.println(TempC_abs_max);
        display.setCursor(100, 15);
        display.println("C");
        // --- Temperature  In, from the Collector to Thermor
        display.setCursor(3, 27);
        display.print(" In: "); 
        display.setCursor(65, 27);
        display.print(TempC_in);
        display.setCursor (100, 27);
        display.print("C");
        // --- Temperature  Out, from the Thermor to Collector
        display.setCursor(3, 39);
        display.print("Out: "); 
        display.setCursor(65, 39);
        display.print(TempC_out);
        display.setCursor(100, 39);
        display.print("C");
        // --- Status : Ok-Charging- orange (red & green = on) , Ok-ready-green, OVERTEMPERATURE - red
        display.setCursor (3, 51);
        display.print("Status: "); 
        display.setCursor(50, 51);
        if (TempC_abs > TempC_abs_hys && TempC_abs < TempC_abs_max)    // with'in these 2 temps
        {
          digitalWrite(DOP_Green, HIGH);       // led on 
          digitalWrite(DOP_Red, LOW);          // led off
          state = state2;                         // green: Text: Ok, Ready
        } 
        else if (TempC_abs >= TempC_abs_max)      // over
        {
          digitalWrite(DOP_Green, LOW);          // led off
          digitalWrite(DOP_Red, HIGH);          // led on
          state = state3;                         // ' red : Text: OVERTEMPERATURE
        } 
        else
        {
          digitalWrite(DOP_Green, HIGH);          // led on:   both led on = orange !
          digitalWrite(DOP_Red, HIGH);          // led on
          state = state1;                         //  orange: Text: Ok, Charging
        } 
    
    
        display.print(state);    
        display.display();                      // show  all whats  in vram'  
      }
      else 
      { 
        display.clearDisplay();                           // delete  show, from last  loop
        display.display();
      }
      //
    }
    
    
    //
    //===============================================================================
    //  Functions:
    // --- read data from AnalogInput for to concert to Celsius: ------
    double readNTC_abs() 
    {
      // variables that live in this function
      double rThermistor = 0;                      // Holds thermistor resistance value
      double tKelvin     = 0;                      // Holds calculated temperature
      double tCelsius    = 0;                      // Hold temperature in celsius
      ntc_read_abs = analogRead(AIP_ntc_abs);    // read from pin and store
      rThermistor = Raux_abs * ( (MAX_ADC / ntc_read_abs) - 1);
      tKelvin = (BETA * T26) / (BETA + (T26 * log(rThermistor / RT26_abs)));
      tCelsius = tKelvin - 273.15;                 // convert kelvin to celsius 
      return tCelsius;                             // Return the temperature in Celsius
    }
    // -----------------------
    double readNTC_in() 
    {
      // variables that live in this function
      double rThermistor = 0;                      // Holds thermistor resistance value
      double tKelvin     = 0;                      // Holds calculated temperature
      double tCelsius    = 0;                      // Hold temperature in celsius
      ntc_read_in = analogRead(AIP_ntc_in);        // read from pin and store
      rThermistor = Raux_in * ( (MAX_ADC / ntc_read_in) - 1);
      tKelvin = (BETA * T26) / (BETA + (T26 * log(rThermistor / RT26_in)));
      tCelsius = tKelvin - 273.15;                 // convert kelvin to celsius 
      return tCelsius;                             // Return the temperature in Celsius
    }
    // -----------------------
    double readNTC_out() 
    {
      // variables that live in this function
      double rThermistor = 0;                      // Holds thermistor resistance value
      double tKelvin     = 0;                      // Holds calculated temperature
      double tCelsius    = 0;                      // Hold temperature in celsius
      ntc_read_out = analogRead(AIP_ntc_out);        // read from pin and store
      rThermistor = Raux_out * ( (MAX_ADC / ntc_read_out) - 1);
      tKelvin = (BETA * T26) / (BETA + (T26 * log(rThermistor / RT26_out)));
      tCelsius = tKelvin - 273.15;                 // convert kelvin to celsius 
      return tCelsius;                             // Return the temperature in Celsius
    }

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • oliverschalles
    oliverschalles over 8 years ago in reply to 14rhb

    as i  coded the  thermor  program, to measure the 3  different temperatures - ( connected  via serial to serial monitor - Arduino IDE on Mac ) I could  set the threshold temperature via  keyboard,  - BUT,  than I  implemented an Oled  display,  and since then the  serial  did  not work, the  program on the arduinowount work as well - it  was trapped in the  setup routine - setup, reset, setup, reset etc. and  again...
    as iremoved  serial' part ( all of it )  the oled worked ( ada fruit library), and showed all data correctly ...  
    here:

    //** based on: https://www.allaboutcircuits.com/projects/measuring-temperature-with-an-ntc-thermistor/
    /*
     3 NTC: In, Out &  Absolute Temperature in Thermor
     if deltaT - differenz in / out is low,  on low temp =  collect energy - no blur!
     if deltaT is low at high temp - ‚ blurr out off focus; less diff (in/out) : more blurring‘  (looking sideway: off focus) 
     over_temperature: umbra - overtemperaturswitch set: immediate blurr!!
     
     A.Uno on:  /dev/tty.wchusbserial620 / 410 - russian driver - same  as A.Nano-GiraSol 
     A.Uno_Thermor: to measure 3 analog NTC'Values/'temperatures: in, out, absolute
     
     Pins used on A.Uno - Thermor 
     A0 ntc_abs, white to Nano temperature in thermor, absolute
     A1 ntc_in,  yellow from collector to thermor
     A2 ntc_out,  blue from thermor to collector
     
     D8     Button           as ‚in‘        Button' to press, to see the display 'PullUp' 
     D9     TempMax          as ‚in‘        Thermor Overswitch - 
     
     D10    green as ‚out‘ Led
     D11 orange as ‚out‘ Led
     D12  red as ‚out‘ Led
     
     
     A.Nano - GiraSol
     D2 umbra           as ‚in‘ harware/ software - OVER Temperature alert'
     A5 ntc_in,  yellow ADC Val FROM collector to thermor
     A6 ntc_out,  blue ADC Themperature from thermor TO collector
     A7 ntc_abs, white ADC Temperature in thermor, absolute
     */
    //======================================================================================================
    // Library:
    // for OLED Display:
    #include <SPI.h>                             // (??)
    #include <Wire.h>                            // AnschlussDrähte 
    #include <Adafruit_SSD1306.h>                // Bangood Oled 256x 128  
    #include <Adafruit_GFX.h>                    // grafics Lib. 
    //
    #define OLED_ADDR   0x3C                     // address OLED ADR: 0x3C (as  contrary printed on pcb: 0x78 !)
    Adafruit_SSD1306 display(-1);                //  no reset, only  2  wire   SCL / SDA - interface, 5v Supply !!
    //
    //-------------------------------
    // Physical Pins @ ArduinoUno:
    // AnalogInPin:        Where the ADC samples the resistor divider's output
    const int AIP_ntc_abs = 0;        // AnalogIn temp, absolute white
    const int AIP_ntc_in = 1;         // AnalogIn ntc_in yellow
    const int AIP_ntc_out = 2;        // AnalogIn ntc_out            blue
    // DigitalInPin:
    const int DIP_Button = 8;         // D_In pin
    const int DIP_Umbra = 9;          // D_In pin
    // DigitalOutPin:
    const int DOP_Green = 10;         // D-Out pin
    const int DOP_Orange = 11;        // D-Out pin
    const int DOP_Red = 12;        // D-Out pin
    
    
    // --- Buttonstate ---------
    int buttonState = 0;   
    
    
    //--- constants: -------------------
    const int MAX_ADC = 1023;         // 10 bit ADC:  0 ...1023
    const float BETA = 3974.0;
    const float T26 = 299.15;         // [K]  26°C in Kelvin - 4 all Calculations 
    
    
    const int RT26_abs = 19610;       // [Ohm] NTC_abs @ 26° = 19.61k
    const int RT26_in = 11820;        // [Ohm] NTC_in  @ 26° = 11.82k
    const int RT26_out = 11040;        //[Ohm] NTC_out @ 26° = 11.04k
    
    
    const float Raux_abs = 2178.0;    // [Ohm] Raux -abs
    const float Raux_in = 998.1;      // [Ohm] Raux -in
    const float Raux_out = 998.1;     // [Ohm] Raux -out
    
    
    // --- variables: --------------------
    int ntc_read_abs = 0;             // Integer for ADC Values (0-1023) 
    int ntc_read_in = 0;              // Integer for ADC Values (0-1023)
    int ntc_read_out = 0;             // Integer for ADC Values (0-1023)
    
    
    // --- currentTemperatures: ----------
    float TempC_abs= 0.0;             // [C] Temperatur, absolute in Thermor 
    float TempC_in= 0.0;              // [C] Temp IN  from Collector to Theremor  c2t
    float TempC_out= 0.0;             // [C] Temp OUT from Thermor to Collector   t2c
    
    
    // for Umbra-set by Keybord, via Serial/USB, connected to UNO --------
    int umbraC_abs = 0;
    int TempC_abs_max = 60;           // Startvalue': temp cels abs maximal.. 
    int TempC_abs_hys = 0;
    // 
    // Strings$ for OLed --------------
    String state = "               ";     // leer$
    String state1 = "Ok, Charging";       // orange
    String state2 = "Ok, Ready";          // green
    String state3 = "OVER-TEMP";          // red
    /*
     algo mas  ?
     */
    // =========================================================================================
    void setup() 
    { 
      // --- pins to use by names: ---
      pinMode(AIP_ntc_abs, INPUT);                // AIn Pin        NTC amnalog in's
      pinMode(AIP_ntc_in, INPUT);                 // AIn
      pinMode(AIP_ntc_out, INPUT);                // AIn
      // --------------------------
      pinMode(DIP_Button,INPUT_PULLUP);           // DIn pin        Buttonswitch: show Display,Content, Pullup
      pinMode(DIP_Umbra,INPUT);                   // DIn            thermor'overtemperature switch
      // ---------------------
      pinMode(DOP_Red, OUTPUT);                   // DOut Pin        Led's
      pinMode(DOP_Orange, OUTPUT);                // DOut
      pinMode(DOP_Green, OUTPUT);                 // DOut 
    
    
      // --- initialize and clear display
      display.begin(SSD1306_SWITCHCAPVCC, OLED_ADDR);
      display.clearDisplay();
      display.display();
    
    
      // --- display a line of text (Logo) 
      display.setTextSize(2);                      // 1 = small, 2 = bigger, 3 = very 'big 
      display.setTextColor(WHITE);
      display.setCursor(1,10);
      display.print("GiraSol");                    // Logo: "GiraSol"
      display.setTextSize(1);  // 1 = small, 2 = bigger, 3 = very 'big
      display.setCursor(1,40);
      display.print(__FILE__);
    
    
      // --- update display with all of the above graphics
      display.display();
      delay (3000);                                // 1000 milicesonds = 1 second pause
      display.clearDisplay();                      // clear, new
      display.display();                           // show up'  - even its cleared !
    }
    //===============================================================================
    void loop() 
    {
      // ---  Hysterese temp @ Thermor to prevent toggele -----
      TempC_abs_hys = (TempC_abs_max - 20);  // Hysterese temp @ Thermor: 
      //
      TempC_abs = readNTC_abs();           // call subroutine
      TempC_in = readNTC_in();             // call subroutine
      TempC_out = readNTC_out();           // call subroutine
      //
      delay(500);                          // pause, 1/2 sec...
      //
      //-----------------
      // read the state of the pushbutton value:
      buttonState = digitalRead(DIP_Button);
      // check if the pushbutton is pressed. - if it is, the buttonState is 'logic HIGH (+ 5 Volt) 
      // if (buttonState == HIGH)          // input pin without pullup.  sw- pressed = input = high
      if (buttonState == LOW)              // input pin 'pullup: when switch pressed = input = low
      {  
        // --- datas to VRAM OLED
        display.clearDisplay();        
        display.setTextColor(WHITE);
        display.setTextSize(1);
        // ------------------------
        display.setCursor(3, 3);
        display.print("Absolute: "); 
        display.setCursor(65, 3);  
        display.print(TempC_abs );
        display.setCursor (100, 3);
        display.print("C"); 
        // --- Umbra C from Keybord via  USB Serial
        display.setCursor(3, 15);
        display.println("MaxTemp: ");  
        display.setCursor(65, 15);
        display.println(TempC_abs_max);
        display.setCursor(100, 15);
        display.println("C");
        // --- Temperature  In, from the Collector to Thermor
        display.setCursor(3, 27);
        display.print(" In: "); 
        display.setCursor(65, 27);
        display.print(TempC_in);
        display.setCursor (100, 27);
        display.print("C");
        // --- Temperature  Out, from the Thermor to Collector
        display.setCursor(3, 39);
        display.print("Out: "); 
        display.setCursor(65, 39);
        display.print(TempC_out);
        display.setCursor(100, 39);
        display.print("C");
        // --- Status : Ok-Charging- orange (red & green = on) , Ok-ready-green, OVERTEMPERATURE - red
        display.setCursor (3, 51);
        display.print("Status: "); 
        display.setCursor(50, 51);
        if (TempC_abs > TempC_abs_hys && TempC_abs < TempC_abs_max)    // with'in these 2 temps
        {
          digitalWrite(DOP_Green, HIGH);       // led on 
          digitalWrite(DOP_Red, LOW);          // led off
          state = state2;                         // green: Text: Ok, Ready
        } 
        else if (TempC_abs >= TempC_abs_max)      // over
        {
          digitalWrite(DOP_Green, LOW);          // led off
          digitalWrite(DOP_Red, HIGH);          // led on
          state = state3;                         // ' red : Text: OVERTEMPERATURE
        } 
        else
        {
          digitalWrite(DOP_Green, HIGH);          // led on:   both led on = orange !
          digitalWrite(DOP_Red, HIGH);          // led on
          state = state1;                         //  orange: Text: Ok, Charging
        } 
    
    
        display.print(state);    
        display.display();                      // show  all whats  in vram'  
      }
      else 
      { 
        display.clearDisplay();                           // delete  show, from last  loop
        display.display();
      }
      //
    }
    
    
    //
    //===============================================================================
    //  Functions:
    // --- read data from AnalogInput for to concert to Celsius: ------
    double readNTC_abs() 
    {
      // variables that live in this function
      double rThermistor = 0;                      // Holds thermistor resistance value
      double tKelvin     = 0;                      // Holds calculated temperature
      double tCelsius    = 0;                      // Hold temperature in celsius
      ntc_read_abs = analogRead(AIP_ntc_abs);    // read from pin and store
      rThermistor = Raux_abs * ( (MAX_ADC / ntc_read_abs) - 1);
      tKelvin = (BETA * T26) / (BETA + (T26 * log(rThermistor / RT26_abs)));
      tCelsius = tKelvin - 273.15;                 // convert kelvin to celsius 
      return tCelsius;                             // Return the temperature in Celsius
    }
    // -----------------------
    double readNTC_in() 
    {
      // variables that live in this function
      double rThermistor = 0;                      // Holds thermistor resistance value
      double tKelvin     = 0;                      // Holds calculated temperature
      double tCelsius    = 0;                      // Hold temperature in celsius
      ntc_read_in = analogRead(AIP_ntc_in);        // read from pin and store
      rThermistor = Raux_in * ( (MAX_ADC / ntc_read_in) - 1);
      tKelvin = (BETA * T26) / (BETA + (T26 * log(rThermistor / RT26_in)));
      tCelsius = tKelvin - 273.15;                 // convert kelvin to celsius 
      return tCelsius;                             // Return the temperature in Celsius
    }
    // -----------------------
    double readNTC_out() 
    {
      // variables that live in this function
      double rThermistor = 0;                      // Holds thermistor resistance value
      double tKelvin     = 0;                      // Holds calculated temperature
      double tCelsius    = 0;                      // Hold temperature in celsius
      ntc_read_out = analogRead(AIP_ntc_out);        // read from pin and store
      rThermistor = Raux_out * ( (MAX_ADC / ntc_read_out) - 1);
      tKelvin = (BETA * T26) / (BETA + (T26 * log(rThermistor / RT26_out)));
      tCelsius = tKelvin - 273.15;                 // convert kelvin to celsius 
      return tCelsius;                             // Return the temperature in Celsius
    }