Solar Power Devices
  • Challenges & Projects
  • Project14
  • Solar Power Devices
  • More
  • Cancel
Solar Power Devices
Blog Solar SPEC - Design Concept
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Solar Power Devices to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 4 Aug 2018 4:50 AM Date Created
  • Views 2497 views
  • Likes 9 likes
  • Comments 7 comments
  • solar power
  • solarpwrdevicesch
  • iot design
Related
Recommended

Solar SPEC - Design Concept

ralphjy
ralphjy
4 Aug 2018
image

Solar Power Devices

Enter Your Electronics & Design Project for Your Chance to Win a Grand Prize for the most inspiring project or a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

The initial Block Diagram for the SPEC:

image

 

First pass at component selection:

1) Solar cells - AOSHIKE Monocrystalline Silicon Solar Cells in Epoxy Package

    2V @ 160mA

    50mm x 50mm x 2mm

image

   These are compact, inexpensive cells which are reasonably robust mechanically.

   Use cells for both power and irradiance sensor.

 

2) Microcontroller Board - Sparkfun ESP8266 Thing

    80mm x 30mm x 5mm

image

   Features:

     ESP8266 microcontroller

     A/D Converter

     I2C Interface

     LiPo Battery charger

     802.11n Wifi

 

3) Temperature Sensor (x2)

    TMP102 Digital temperature sensor with I2C interface

imageimage

 

4) LiPo Battery

    3.7V @ 1000mAh

image

 

5) Mechanical housing and mounts

    Need a watertight and temperature tolerant box to house all the components except for the remote temperature sensor.

    Must have cutouts for the solar cells.

    Probably try to 3D print a custom unit.

    Needs to allow mounting with the solar cells in the same plane as the solar panels being monitored.

    Remote temperature sensor needs to mount to bottom of one of the solar panels (possibly just use adhesive).

 

Design considerations:

 

Power:

The ESP8266 has an average current consumption of 80mA @ 3.3V.  802.11n transmit current is typically 135mA and receive current is typically 62mA.  Standby is 0.9mA.

 

The solar cells are rated at 2V @ 160mA, but I do not have a detailed spec sheet.  I'm assuming that this is under standard test conditions.  I plan to use 3 cells in series to provide 6V @ 160mA.  I'll use a series diode to drop the voltage closer to 5V for the input to the Thing board.  I'll need to do some characterization to ensure that I won't exceed the 6V maximum of the board input.  I plan to use a 1000 or 1200mAh battery to provide power when there is no sunlight, so I think I'll be okay except for possibly a string of days with poor total irradiance (winter months).  Again, I'll need to do some characterization.  I can add another string of cells in parallel at the expense of a larger housing.

 

I'll need to have power management incorporated in the program (control the frequency and duration of WiFi activity, standby when there is no irradiance).  I don't think I'll need the deep sleep mode but that could be an option at night.

 

Irradiance sensor:

Since I don't have a detailed spec for the solar cell, I'll need to generate the I-V curves.  I'll determine the MPP voltage and current under standard test conditions (STC - 1000W/meter^2 and 25C) and use that to select the load resistor for the solar cell.  I'll need to scale the load resistor voltage as the A/D input range is only 0-1V.   The A/D reading will provide the voltage and current (voltage/load resistance) that are needed for the irradiance computation.

 

I plan to use a Daystar Irradiance meter as a reference check.

 

Possible additions:

1) OLED display to display irradiance and temperature locally without requiring WiFi connectivity.

2) External power switch - the Thing board has a power switch, I would just have to wire this to an external switch.

  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 8 years ago in reply to genebren +3
    Hi Gene, Thanks for the info. I'll have to admit that I did not consider the optimizations that you've suggested. And I really hate to admit that I had downloaded the MCP73831 spec but had not gotten around…
  • genebren
    genebren over 8 years ago +2
    Very interesting update to your solar powered devices project. You mention MPP (maximum power point), but I don't think that you can get the 'thing' board to control the charge rate for your battery. On…
  • DAB
    DAB over 8 years ago in reply to Jan Cumps +2
    Hi power or not, the basic cell still only outputs 1.2 volts across the p-n junction. So you just run the solar cell to the A/D converter with high value resistors to get the correct scaling and you have…
Parents
  • DAB
    DAB over 8 years ago

    Nice update.

     

    I am curious, why did you not just use the solar cell as your indicator for sunlight?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 8 years ago

    Nice update.

     

    I am curious, why did you not just use the solar cell as your indicator for sunlight?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ralphjy
    ralphjy over 8 years ago in reply to DAB

    Hi DAB,

     

    Not exactly sure what your question is.  Probably because I didn't write something clearly.

     

    Is the question why do I use a separate solar cell for the irradiance sensor rather than just measuring the cells that I am using for power?

    If that's the case - I need to measure the cell voltage with a fixed load to do the irradiance calculation.  The load value is related to the MPP current @ 1000W/m^2 irradiance.

     

    Or maybe you were asking a different question?

     

    Ralph

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to DAB

    DAB  wrote:

     

    ...

    I am curious, why did you not just use the solar cell as your indicator for sunlight?

    ...

    This may be possible. But the solar cells are high power. The signals they give would have to be transformed into something that's appropriate for a micro controller.  And the high power in the solar circuit would have to be isolated.

    A separate cell that doesn't have a connection with the power side may be cheaper and easier to keep safe?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago in reply to ralphjy

    When the sun is out, your solar cell will output a positive voltage, just like your light sensor.

    So the solar cell can be used as a light sensor as well as your source of power.

    You just need to run it into an A/D converter with the appropriate voltage scaling.

     

    Saves you needing a sensor.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago in reply to Jan Cumps

    Hi power or not, the basic cell still only outputs 1.2 volts across the  p-n junction.

    So you just run the solar cell to the A/D converter with high value resistors to get the correct scaling and you have an automatic light sensor.

     

    DAB