Spring Clean!
  • Challenges & Projects
  • Project14
  • Spring Clean!
  • More
  • Cancel
Spring Clean!
Spring Clean Projects 2025 Tap Tap Tap
  • News and Projects
  • Forum
  • Members
  • More
  • Cancel
  • New
Join Spring Clean! to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kmikemoo
  • Date Created: 4 Jun 2025 4:13 AM Date Created
  • Views 2911 views
  • Likes 13 likes
  • Comments 14 comments
  • RF Attenuator
  • RF Tap
  • spring cleaning
Related
Recommended

Tap Tap Tap

kmikemoo
kmikemoo
4 Jun 2025
Tap Tap Tap

A few months back while looking for information on oscillators, I stumbled across a 40dB tap. Okay, the article was really about a RF power meter, but that looked complicated and, besides, I already have a NanoVNA. I would really like to NOT blow up the NanoVNA so the tap caught my eye. The article is from the June 2001 edition of QST magazine by the ARRL. The authors are Wes Hayward and Bob Larkin. The article is attached below.

So... I ordered the little aluminum enclosures. Of course they come in a three pack. Fine. I need 1.5 inches of a brass strip. It comes in a 12 inch strip. Fine. I need a SMA bulkhead connector. They come in 5-packs. Fine. I don't have resistors of the correct power rating.  I can get 100 for the same price as 10.  Fine.  With all this excess material, I'll make a SO-239 version, a BNC version and a SMA version. It's a bit more than I was thinking about, but they will save me from using a bunch of adapters. This is a good thing.

So I built the SO-239 version. It turned out nice. It turned out that it wasn't quite as easy to build as I estimated AND... I built the easy one - the one in the article.  So the project stalled.  Onto the next bright shiny thing.

And the other versions? The only movement they have seen was to get pushed out of the camera shot for the 2-year antenna project.

In the spirit of Spring Clean, let's get this project completed.
Fantastic. I have just started and I'm using up all of the M2.5 hardware from my standoff kit. I need to order some hardware. Maybe this was why I stalled out a few months ago. At least I was able to find all of the SMA bulkhead connectors. The brass strip is still at the end of the work bench where I do my sawing. It hasn't moved in months. Even the resistors are still here – albeit buried under other stuff.

On a bright note, my custom brass plate feedline installation jig is still here as well.
image

The build isn't super complicated.  Here was the starting point.  You can see that I started drilling some of the mounting holes while I waited for the M2.5 hardware.  Both the SO-239 and the SMA connector mounting holes were tapped into the body of the enclosure.
image   image

image

The purple wire is a gimmick capacitor and is supposed to improve performance at higher frequencies (>500MHz).  

Pre-soldering the brass plate worked better than just buffing the plate and trying to solder on it while in place.

For the BNC version, the brass plate needed to be notched.  I used a hand nibbler for that.

For the SMA version, connecting to the brass plate proved to be quite a chore.  I used a piece of solid #14 to bridge the gap between SMA center pins.  Once they were finally secure, I cut out the middle so the signal would flow through the brass plate.  Soldering to the SMA connectors was by far the most difficult aspect of the project.

For the end SMA connector, I used longer mounting screws so I could secure the two 100 ohm resistors to chassis ground.  Wrap the resistor tail around the protruding screw and secure with a nut.  This proved to be quite handy.

Performance

So how do they work?  I give them a "Good" grade.  According to my NanoVNA, they start at about 33dB of attenuation at 3MHZ.  Since I really don't plan to blast 100 watts of power through these, I should be fine.  The span depicted below is from 3 MHz to 1 GHz, although the article said that the tap was good only to about 500MHz.  I could always try lengthening the gimmick capacitor.

SO-239 Version
image

BNC Version
image

SMA Version
image

Conclusion

Again, soldering to the SMA bulkhead connectors was by far the most challenging aspect of this project.  Truth be told, this was probably why I didn't complete the BNC and SMA versions until now.  If I had to do it over again, I would try to use 22-26 AWG butt splice connectors to bridge between the center pin of the SMA connector and the plate or resistors.  I would also not connect the two 100 ohm resistors until after the center run is soldered in place.  Last build tip:  Use way more wire than you need for the gimmick capacitor.  You'll need some to hold on to while soldering.  Once it's soldered in place, then trim to length

There are now less random pieces parts laying about on the workbench and a couple of more pieces of test gear on the shelf.   If nothing else, my workbench is looking better than it has in months.  Now if I could only figure out why I bought those 4 MHz TCXO's...

imagePDF     image

.

  • Sign in to reply

Top Comments

  • kmikemoo
    kmikemoo over 1 year ago in reply to jc2048 +1
    jc2048 I have not been into the radio hobby long enough to know the deep secrets. I do believe that the NanoVNA is "good" but it is not laboratory grade. I also believe that it is better at the lower frequencies…
  • jc2048
    jc2048 over 1 year ago in reply to kmikemoo +1
    If you want something that works better up towards the GHz area and don't need the hundreds of watts of power handling ability that the brass plate and N connectors give you, you might do better with a…
Parents
  • jc2048
    jc2048 over 1 year ago

     'I give them a "Good" grade.  According to my NanoVNA, they start at about 33dB of attenuation at 3MHZ.'

    I'm not very familiar with RF. Is a reading of -33dB for what is supposed to be -40dB really "good"? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago in reply to jc2048

    jc2048 Fair question.  For a homebrew DIY project with imprecise components and questionable assembly techniques... having it turn out somewhat close to the goal is acceptable in my book.  If this were a professionally made item that I purchased, I would not be so generous with my assessment.

    I cannot speak to all of RF.  In Amateur Radio, we really use dBm - where 0dBm = 1 milliwatt (mw).  A -30dB (or 30dB of attenuation) gives me 1,000 times less power into my instrument.  -40dB gives me 10,000 times less.  -30dB should be around 77uV.  -40dB should be around 67uV.
    Because decibels seem like magic math to me sometimes, I try to use online calculators.  https://www.everythingrf.com/rf-calculators
    Folks are welcome to check my work. Laughing

    I am not chasing precision power measurements.  I'm really most concerned with keeping the magic smoke inside components while still being able to see what is going on in the system.  I also plan to use them with my TinySA to view harmonics.  There may come a time where I want to improve the performance of these taps, but it will probably just be for the assembly techniques.  If I need more precise measurements, I have a friend with much better equipment.  I would just like to start in the ball park.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago in reply to jc2048

     jc2048 I have not been into the radio hobby long enough to know the deep secrets.  I do believe that the NanoVNA is "good" but it is not laboratory grade.  I also believe that it is better at the lower frequencies and less accurate at the higher frequencies.  Still... for $100-ish... it is fantastic.

    I chose not to try to get too deep into the "decibel" discussion because although it is a ratio, we tend to use it as an absolute value (because we use a standard reference value).  The discussion becomes too academic.  At work, we only worry about sound pressure decibels - but only the A-weighted version, dBA.

    HOWEVER, your comment about "into a fixed load" (50 ohms) got me thinking.  The screen shots in the original post were with no load - because my dummy loads were all built for 200MHz and below and they definitely impacted the performance curves.  But after reading your post a couple of times, I remembered that my calibration load is supposed to be good for something crazy - like 6GHz.

    SMA Version
    image     image

    SO-239 Version
    image     image

    As you can see, these have much better performance into the 50 ohm load.  THANK YOU - because now I won't feel the need to try to improve these. LaughingJoy

    My opinion:  In RF, there are always parasitics.  I tried to build a 100dB attenuator.  It's good for 46dB at 146MHz.  Why?  I don't know.  It could be that the parallel ground strips on either side of the main signal path are not at the same true potential and the inner tracks are allowing some RF signal conduction.  The signal could also just be jumping across the resistor.  After all, it is radiating signal.  And THIS is what makes RF a bit of magic.

    How is it that 46mW of transmitter power can be heard in Antarctica from Northeastern Wisconsin?  Or the West coast of Africa?  And yet... it is so.  Why does 1 cm of wire make all the difference between a good antenna and a terrible antenna?
    Sorry, not sorry, my friend.  Welcome to the Dark Side.  RF.  RelaxedThumbsup  Glad to have you on the team. Laughing

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 1 year ago in reply to kmikemoo

    That's more reasonable. The nanoVNA looks to be a useful piece of kit.

    If you did want to refine it a little, perhaps try reworking the two 100R resistors at the bottom of the attenuator to lose the excess lead length, and experiment with the gimmick capacitor, which in the SMA case looks like it's overcompensating a bit at the top end up towards 1GHz.

    Good luck with the competition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • FreeBird
    FreeBird over 1 year ago in reply to kmikemoo

    What I know about RF would fit in a child's thimble, what I don't know would fill volumes.  I am forming an analogy of a Tap to a shunt resistor in a Amp meter, where you use the resistor to shunt off a small portion of the current at a known ration and measure that to determine the strength of the whole? 

    Now that I have posted that analogy I will go look it up and see if I am correct.  No need to respond.  It just helps me to organize my thoughts by typing them out. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago in reply to FreeBird

    FreeBird  When you started in with "What I know...", it reminded me of a comment we used to make in the Army.  They were variants of "What I know about THAT could be written on the edge of a dime with a piece of chalk."  Laughing  Good memories.  Thumbsup

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 1 year ago in reply to FreeBird

    A better analogy might be a passive x10 oscilloscope probe, where the loading effect is reduce by having the attenuator, but there's a need to balance the capacitances so that the capacititive divider matches the resistive one for a good, level frequency response up to 100s of MHz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 1 year ago in reply to FreeBird

    A better analogy might be a passive x10 oscilloscope probe, where the loading effect is reduce by having the attenuator, but there's a need to balance the capacitances so that the capacititive divider matches the resistive one for a good, level frequency response up to 100s of MHz.