Spring Clean!
  • Challenges & Projects
  • Project14
  • Spring Clean!
  • More
  • Cancel
Spring Clean!
Spring Clean Projects 2025 Tap Tap Tap
  • News and Projects
  • Forum
  • Members
  • More
  • Cancel
  • New
Join Spring Clean! to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kmikemoo
  • Date Created: 4 Jun 2025 4:13 AM Date Created
  • Views 2918 views
  • Likes 13 likes
  • Comments 14 comments
  • RF Attenuator
  • RF Tap
  • spring cleaning
Related
Recommended

Tap Tap Tap

kmikemoo
kmikemoo
4 Jun 2025
Tap Tap Tap

A few months back while looking for information on oscillators, I stumbled across a 40dB tap. Okay, the article was really about a RF power meter, but that looked complicated and, besides, I already have a NanoVNA. I would really like to NOT blow up the NanoVNA so the tap caught my eye. The article is from the June 2001 edition of QST magazine by the ARRL. The authors are Wes Hayward and Bob Larkin. The article is attached below.

So... I ordered the little aluminum enclosures. Of course they come in a three pack. Fine. I need 1.5 inches of a brass strip. It comes in a 12 inch strip. Fine. I need a SMA bulkhead connector. They come in 5-packs. Fine. I don't have resistors of the correct power rating.  I can get 100 for the same price as 10.  Fine.  With all this excess material, I'll make a SO-239 version, a BNC version and a SMA version. It's a bit more than I was thinking about, but they will save me from using a bunch of adapters. This is a good thing.

So I built the SO-239 version. It turned out nice. It turned out that it wasn't quite as easy to build as I estimated AND... I built the easy one - the one in the article.  So the project stalled.  Onto the next bright shiny thing.

And the other versions? The only movement they have seen was to get pushed out of the camera shot for the 2-year antenna project.

In the spirit of Spring Clean, let's get this project completed.
Fantastic. I have just started and I'm using up all of the M2.5 hardware from my standoff kit. I need to order some hardware. Maybe this was why I stalled out a few months ago. At least I was able to find all of the SMA bulkhead connectors. The brass strip is still at the end of the work bench where I do my sawing. It hasn't moved in months. Even the resistors are still here – albeit buried under other stuff.

On a bright note, my custom brass plate feedline installation jig is still here as well.
image

The build isn't super complicated.  Here was the starting point.  You can see that I started drilling some of the mounting holes while I waited for the M2.5 hardware.  Both the SO-239 and the SMA connector mounting holes were tapped into the body of the enclosure.
image   image

image

The purple wire is a gimmick capacitor and is supposed to improve performance at higher frequencies (>500MHz).  

Pre-soldering the brass plate worked better than just buffing the plate and trying to solder on it while in place.

For the BNC version, the brass plate needed to be notched.  I used a hand nibbler for that.

For the SMA version, connecting to the brass plate proved to be quite a chore.  I used a piece of solid #14 to bridge the gap between SMA center pins.  Once they were finally secure, I cut out the middle so the signal would flow through the brass plate.  Soldering to the SMA connectors was by far the most difficult aspect of the project.

For the end SMA connector, I used longer mounting screws so I could secure the two 100 ohm resistors to chassis ground.  Wrap the resistor tail around the protruding screw and secure with a nut.  This proved to be quite handy.

Performance

So how do they work?  I give them a "Good" grade.  According to my NanoVNA, they start at about 33dB of attenuation at 3MHZ.  Since I really don't plan to blast 100 watts of power through these, I should be fine.  The span depicted below is from 3 MHz to 1 GHz, although the article said that the tap was good only to about 500MHz.  I could always try lengthening the gimmick capacitor.

SO-239 Version
image

BNC Version
image

SMA Version
image

Conclusion

Again, soldering to the SMA bulkhead connectors was by far the most challenging aspect of this project.  Truth be told, this was probably why I didn't complete the BNC and SMA versions until now.  If I had to do it over again, I would try to use 22-26 AWG butt splice connectors to bridge between the center pin of the SMA connector and the plate or resistors.  I would also not connect the two 100 ohm resistors until after the center run is soldered in place.  Last build tip:  Use way more wire than you need for the gimmick capacitor.  You'll need some to hold on to while soldering.  Once it's soldered in place, then trim to length

There are now less random pieces parts laying about on the workbench and a couple of more pieces of test gear on the shelf.   If nothing else, my workbench is looking better than it has in months.  Now if I could only figure out why I bought those 4 MHz TCXO's...

imagePDF     image

.

  • Sign in to reply

Top Comments

  • kmikemoo
    kmikemoo over 1 year ago in reply to jc2048 +1
    jc2048 I have not been into the radio hobby long enough to know the deep secrets. I do believe that the NanoVNA is "good" but it is not laboratory grade. I also believe that it is better at the lower frequencies…
  • jc2048
    jc2048 over 1 year ago in reply to kmikemoo +1
    If you want something that works better up towards the GHz area and don't need the hundreds of watts of power handling ability that the brass plate and N connectors give you, you might do better with a…
Parents
  • JWx
    JWx over 1 year ago

    nice work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • JWx
    JWx over 1 year ago

    nice work!