Spy Nerd
  • Challenges & Projects
  • Project14
  • Spy Nerd
  • More
  • Cancel
Spy Nerd
Blog Security System with Motion Detection
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Spy Nerd to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rahulkhanna
  • Date Created: 25 Sep 2021 2:45 PM Date Created
  • Views 4258 views
  • Likes 1 like
  • Comments 2 comments
  • spynerdch
Related
Recommended

Security System with Motion Detection

rahulkhanna
rahulkhanna
25 Sep 2021

The system is designed to detect intrusion (unauthorized entry) into a building or other area.Security System with Motion Detection

Things used in this project

Hardware components

Proximity Sensor- Pyroelectric Infrared Sensor Module
KEMET Electronics Corporation Proximity Sensor- Pyroelectric Infrared Sensor Module
×1
Raspberry Pi Zero
Raspberry Pi Zero
×1
Camera Module V2
Raspberry Pi Camera Module V2
×1
Buzzer
Buzzer
×1
LED (generic)
LED (generic)
×2
Arcade button
×1
5V 2.5A Switching Power Supply
Digilent 5V 2.5A Switching Power Supply
×1
60W PCIe 12V 5A Power Supply
Digilent 60W PCIe 12V 5A Power Supply
×1
Jumper wires (generic)
Jumper wires (generic)
×10

Software apps and online services

Raspbian
Raspberry Pi Raspbian
OpenCV
OpenCV

 

Why Did We Build This?

There is a lot of theft scenarios nowadays which causes a great loss to the owner. A recent incident at a popular jewelry shop urged me to do this project.Robbery at jewellery shop

     Robbery at jewelry shop

"A jewelry store in Tamil Nadu’s Tiruchirappalli district was burgled in the early hours of Wednesday morning after masked men gained entry into the store by drilling a hole in its wall. The incident took place at ####### Jewellery, a three-storeyed building near Chathiram bus Stand in Tiruchirappalli.

Diamond, Gold and Platinum jewelry worth 13 crore rupees were stolen from the store. I am satisfied with the way the investigation is being carried, the robbers will be caught soon" - Source from Indian Express

Idea image

The system is designed to detect intrusion (unauthorized entry ) into a building or other area. This project can be used in residential, commercial, industrial, and military properties for protection against burglary or property damage, as well as personal protection against intruders

A compact, a low-profile project is attached to the wall of the area which has to be monitored. This project consists of a camera that will capture the image of the intruder and notify the owner.

To test the real-time scenario, we deployed it on one of the jewelry shops to test how possibly it could help them and the results were pretty affirmative.

Working of the Project

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Hardware Build

First of all, I would like to thank KEMET for supporting this project with an efficient and low-profile pyro sensor. It really felt helpful to achieve some of the complex designs with this tiny sensor.

packed and sealed parcel

     packed and sealed parcel

SS-430 Pyro sensor
     SS-430 Pyro sensor

Step 1: Getting Started with Pyroelectric Proximity Infrared Sensors (Content from KEMET)

KEMET Electronics Pyroelectric Proximity Infrared Sensor Modules use the pyroelectric proximity effect of ceramic by absorbing infrared rays emitted from the human body. This detects the natural infrared signature produced by humans. It can detect infrared rays without using lenses, allowing a detection distance up to 2 meters. By adding a KEMET proprietary lens, the detection distance can be further improved up to 5 meters. The lens is available in three different colors, to enable some design flexibility. KEMET Electronics Pyroelectric Proximity Sensor Modules in the module solution are even easier to install with the driving being already included in the package, making it just "plug and sense".

 

KEMET Pyro Sensor

 

KEMET Pyro Sensor

FEATURES

  • Reflow capable SMD configuration
  • Lens not required
  • Wide view angle up to ±60°
  • Detection possible through glass or resin
  • Low power consumption, down in the μA range
  • Excellent radio wave performance in a high-frequency band
  • Compact and low profile (5.0 x 4.8 x 1.7mm)
  • Human presence detection sensing for energy-saving functions in a variety of applications

 

APPLICATIONS

  • Contactless switching
  • Office automation equipment
  • Home appliances
  • Lighting
  • Display products
  • Air-conditioners
  • TVs
  • PC monitors
  • Rice cookers
  • Smart toilets

We use the sensor with a white lens which gives a 74° view angle and a range up to 5m.To learn more about the KEMET pyro sensor, do watch the webinar.

Step 2: Burn Raspbian to the SD card

Raspbian is the Linux distribution of choice running on the Raspberry Pi. In this guide, we will be using the Lite version, but the Desktop version (which comes with a graphical environment) can be used as well.

  • Download Etcher and install it.
  • Connect an SD card reader with the SD card inside.
  • Open Etcher and select from your hard drive the Raspberry Pi .img or .zip file you wish to write to the SD card.
  • Select the SD card you wish to write your image to.
  • Review your selections and click 'Flash!' to begin writing data to the SD card

 

 

Download Raspbian Stretch Lite

Download Raspbian Stretch Lite

Connect the device to your network

  • Enable SSH access by adding empty file ssh, again placed at the root of the boot volume on your SD card.
  • Insert the SD card into the Raspberry Pi. It will boot in roughly 20 seconds. You should now have SSH access to your Raspberry Pi. By default, its hostname will be raspberrypi.local.

 

     On your computer, open a terminal window and type the following:ssh pi@raspberrypi.local. The default password is raspberryimage

 

Step 3: Interfacing with Raspberry Pi (Project Motion Dashcam)

KEMET's PYROSENSOR - SS430

The Block Diagram of this circuit is given below.

 

Block Diagram

 

Block Diagram

To make these connections, I've used separate connectors for power, relay output, and sensor input. Each connector is soldered to the Raspberry Pi as shown below.

 

 

 

 

 

 

 

Connector

 

 

 

     Connector

Since the output from the pyro sensor is a digital signal, we connect the KEMET pyro sensor to the GPIO Pin 15 of Raspberry Pi.Raspberry Pi with SD card

     Raspberry Pi with SD card

The Pinout of the SS-430 pyroelectric sensor is given below

 

SS-430 pinoutSS-430 pinout

The connection is made as shown below.

SS-430 ---> Raspberry Pi

Vcc (1) ---> +5V

Signal (4) ---> GPIO15

GND (5)---> GND

Sensor Connection

 

Sensor Connection

PI-CAMERA

The Pi-camera is connected to the CSI port of the Raspberry Pi.Raspberry Pi Camera Module V2

     Raspberry Pi Camera Module V2

Pi-cam to Raspberry Pi

     Pi-cam to Raspberry Pi

 

RELAY BOARD

We connect the Buzzer and an Emergency light using a relay circuit to the GPIO pins 23 & 24 of the Raspberry Pi.RELAY DRIVE CIRCUIT

 

     RELAY DRIVE CIRCUIT

The Power Supply is used to deliver the power for the Status Light, Emergency Light, and the Alarm.Power Supply

     Power Supply

The Industrial grade Light Indicators and Buzzer are used to show the status and alert signal to the security (user).

 Industrial grade Light Indicators

 

Industrial grade Light Indicators

Relay Board ---> Raspberry Pi

Vcc ---> +5V

IN1 (Secure Light)---> GPIO23

IN2 (AlertLight & Buzzer) ---> GPIO24

GND ---> GND

The Industrial grade Light Indicators and Buzzer are connected to the GPIOs of the Raspberry Pi.Sensor ConnectionSensor Connection

PUSH BUTTON

The Emergency reset button is connected to the GPIO pin 14 of the Raspberry Pi.Push ButtonPush Button

Arcade Button connected to raspberry piArcade Button connected to raspberry pi

The emergency button is used to turn off the alert manually by pressing it once.

The Overall connection is shown below.

Overall ConnectionOverall Connection

 

Step 4: Code

GPIO of the Raspberry Pi can be accessed using the GPIO library which can be imported using the GPIO library.

The libraries such as RPi.GPIO and time are used in this project.

import RPi.GPIO as GPIO 
import time

The GPIO pin is then configured to digital input using the following lines

sensorPIN = 15
GPIO.setmode(GPIO.BCM)
GPIO.setup(sensorPIN, GPIO.IN)

GPIO Pin 15 is configured to use as digital input which reads for every 50ms. Whenever the intruder/human enters in the range, the sensor detects and produces the digital pulse.

while True:           
    if GPIO.input(sensorPIN): # if sensorPIN == 1
        print "Intruder Alert !!!"
    else:
        print "No intruder"
    time.sleep(0.05)         # wait 50 milliseconds

Although the above code worked, I had a few false triggering. After going through the documentation from KEMET, The SS-430 produces two output pulses of 200msec per detection. This can be interpreted by the Raspberry pi using the following code:

 

Timing Diagram from the webinar

 

Timing Diagram from the webinar

import RPi.GPIO as GPIO
import time
sensorPIN = 15
GPIO.setmode(GPIO.BCM)
GPIO.setup(sensorPIN, GPIO.IN)
pulse = 0
PyroRead = 0
IR_threshold = 198000
IR_sensed = 0
start_time = 0
end_time = 0
try:
    while True:
        while(IR_sensed < 2):
            start_time = time.time()
            GPIO.wait_for_edge(sensorPIN, GPIO.FALLING)
            GPIO.wait_for_edge(sensorPIN, GPIO.RISING)
            GPIO.wait_for_edge(sensorPIN, GPIO.FALLING)
            end_time = time.time()
            PyroRead = round((end_time - start_time)*1000000)
            print(PyroRead)

            if(PyroRead > IR_threshold):
                IR_sensed += 1
        pulse = pulse + 1
        print(pulse)
        print("Intruder Alert !!!")
        PyroRead = 0
        IR_sensed = 0
        time.sleep(1)         # wait 1 second
finally:
    print("clean up")
    # GPIO.cleanup([sensorPIN])
    GPIO.cleanup() # cleanup all GPIO

Now the sensor can determine the presence of the human within the specified range and view angle.Screenshot - sensor-testScreenshot - sensor-test

After a lot of struggles and effort, I have created a library to interface KEMET's pyro sensor with the Raspberry Pi.

The picamera library is installed using the following command

sudo apt-get install python-picamera
installing picamera lib

 

installing picamera lib

Next, we interface the Raspberry Pi Camera Module V2 to the Raspberry Pi. We import picamera library to interface the camera with the raspberry pi. We have set the resolution of the camera at 1024 x 768 so that the images are captured at a lower resolution. This allows us to reduce memory usage and to send the images.

import picamera

with picamera.PiCamera() as camera:
     camera.resolution = (1024, 768)

When the intruder is detected, the event is triggered and the system captures the images of the intruder. The images captured are stored in a folder with the timestamp attached to it.

with picamera.PiCamera() as camera:
     camera.resolution = (1024, 768)
     for filename in camera.capture_continuous('/home/pi/Intruder/img{timestamp:%H-%M-%S-%f}.jpg'):
Camera output and a screenshot of the directory

 

Camera output and a screenshot of the directory

From the above example, the picture of the intruder is captured by the device which has to be transmitted to the master (owner).

First, we add the Smtplib package allows us to set up the Gmail server. Install an SMTP service with the command

sudo apt-get install ssmtp

 

Screenshot - SMTP package

 

Screenshot - SMTP package

Make sure that Allow less secure apps setting is turned on for allowing Gmail SMTP Access Authentication.

SMTP - AUTH

 

SMTP - AUTH

import glob
import smtplib
import os

These four modules are used to send the emails from a Raspberry Pi:

from email.mime.multipart import MIMEMultipart
from email.mime.base import MIMEBase
from email.mime.text import MIMEText
from email.utils import formatdate
from email import encoders

We need to add the receiver's email and sender's email address and password, in our case both, are the same email as shown below:

sender = 'x@gmail.com'
password = ' Replace the pass '
receiver = 'x@gmail.com'

By making several adjustments to the code, you can change the Subject, sender address, receiver address, and the content of the body. The images are sorted and the latest image is sent via Gmail (SMTP).

Screenshot of the Gmail

 

Screenshot of the Gmail

We have also added two relay circuit and a manual reset push button to the circuit. These are treated as normal GPIO to indicate or to inform the status of the theft alert using LED and Buzzers.

# Set pins 23, 24 to be an output pin and set initial value to low (high), since relay ckt is pull-down mechanism
Green = 23
Red = 24
GPIO.setup(Green, GPIO.OUT, initial=GPIO.HIGH)
GPIO.setup(Red, GPIO.OUT, initial=GPIO.HIGH)

# Set pin 14 to be an input pin
reset_button = 14
GPIO.setup(reset_button, GPIO.IN)

while True:          
    if GPIO.input(sensorPIN): # if sensorPIN == 1
        GPIO.output(23, GPIO.HIGH) # Turn off Green
        GPIO.output(24, GPIO.LOW) # Turn on Red
        if !GPIO.input(reset_button):
            break
    else:
        GPIO.output(23, GPIO.LOW) # Turn on Green
        GPIO.output(24, GPIO.HIGH) # Turn off Red
    sleep(0.05)         # wait 50 milliseconds

 

Step 5: Enclosure

enclosure
  • A small section is needed to attach the SS-430 pyro sensor to the project. I have adhered the sensor to the Indicator firmly as shown below.Indicator with SS-430

 

          Indicator with SS-430

 

  • Make sure that the required wires/connects are soldered to the raspberry pi. This is a crucial part to meet the size of the device. I have used the terminal block connector to make the common connections. One end of the wires is soldered to the Raspberry Pi.Cables soldered to RPi & End of the wires to terminal block

 

               Cables soldered to RPi & End of the wires to a terminal block

 

  • Now Insert the device inside the enclosure and It would look something like thisFinal Setup1

Final Setup

image

image

Voila! The connection is done and we are equipped to test it.

Working of the Project image

To test the real-time scenario, we deployed it on one of the jewelry shops to test how possibly it could help them and the results were pretty supportive.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

If you faced any issues in building this project, feel free to ask me. Please do suggest new projects that you want me to do next.

Give a thumbs up if it really helped you and do follow my channel for interesting projects. image

Share this video if you like.

Happy to have you subscribed: https://www.youtube.com/c/rahulkhanna24june?sub_confirmation=1

https://www.youtube.com/c/rahulkhanna24june?sub_confirmation=1Thanks for reading!

  • Sign in to reply
Parents
  • BigG
    BigG over 4 years ago

    This is a very nice project, even if the write up is a copy n paste of your Hackster.io project... I tend to remember the good ones when I find them. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • BigG
    BigG over 4 years ago

    This is a very nice project, even if the write up is a copy n paste of your Hackster.io project... I tend to remember the good ones when I find them. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • rahulkhanna
    rahulkhanna over 4 years ago in reply to BigG

    Thanks for following up on my projects image