Spy Nerd
  • Challenges & Projects
  • Project14
  • Spy Nerd
  • More
  • Cancel
Spy Nerd
Blog Snoop Dog or Snoop Cat
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Spy Nerd to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 18 Nov 2021 4:38 AM Date Created
  • Views 30476 views
  • Likes 10 likes
  • Comments 16 comments
  • cat detector
  • spynerdch
  • doug wong
  • color sensor
  • cat sensor
  • Snoop Cat
  • snoopcat
  • Snoop Dog
  • pir sensor
Related
Recommended

Snoop Dog or Snoop Cat

dougw
dougw
18 Nov 2021

Intro

The theme of this project is spy nerd. I am a fan of spy novels, but I am not really into spying on people, so I thought I would have some fun experimenting with spying on my cats. That is about as nerdy as it gets.

I wanted to do something a bit original - something that you can't buy, which meant a nannycam was out. And of course since this is just for fun and not likely to be used regularly, the price needed to be low.

The simple description is several passive infrared sensors and a color sensor that can:

- detect cats or dogs

- detect people and differentiate them from animals

- detect the direction of travel of the animal

- identify which animal is detected

image

This sensor system requires an MCU to analyze the sensor data and deduce the above information.

To help the MCU, the sensors are arranged in a specific geometry. Two PIR sensors which will detect any hot body are used to figure out which direction the body is travelling by recognizing which one was triggered first. The third PIR sensor is aimed higher than pet height so it only detects people. This sensor can be used to confirm that the other sensors are seeing a pet and not a person. The final sensor is a color sensor that is used to figure out which pet is detected by their chacteristic color. We have 2 cats that have different coloring.

 

The Breadboard

The first video  shows the electronics and sensors that are used in the system as well as how the electronics work to detect pet activity using a breadboard.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The Schematic

Here is the schematic of how the electronics are hooked up:

image

The 3D Printed Plastic Parts

This video shows all the plastic parts and 3D printed parts used to build the system:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
 

This video  walks through design of the 3D printed parts:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The Assembled System

This video shows the system completely wired up and working .... and of course being photobombed by a curious cat.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The Cat House PC Software

This cat house video shows the remote computer program that displays where the cats are. It has some footage of cats walking in the appropriate direction as well as cat images to indicate where they end up.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This VB6 program was whipped up in 20 minutes because the publishing deadline is imminent. It runs fine, although I was going to embed the video clips if I had time. Also in the interests of full disclosure, it is faking a bit because the cat color detection is not tuned properly yet.

 

The Firmware

Here is the arduino code for those who need to know....

/*
This program detects cats and their direction of travel
Doug Wong 2021-11-07
Hardware:
0.96" TFT 80x160 SPI ST7735 display
TCS34725 color sensor
HC-SR501 PIR sensors
bluetooth
arduino Pro Micro


Hardware SPI Pins:
 * Arduino Pro Micro   SCK=15, SDA=16


*/


#include <Adafruit_GFX.h>  // Include core graphics library
#include <Adafruit_ST7735.h>  // Include Adafruit_ST7735 library to drive the display
#include <Wire.h>
#include <Adafruit_TCS34725.h>  //color sensor library


// Declare pins for the display:
#define TFT_CS     7
#define TFT_RST    -1  // You can also connect this to the Arduino reset in which case, set this #define pin to -1!
#define TFT_DC     5
// The rest of the pins are pre-selected as the default hardware SPI for Arduino Uno (SCK = 13 and SDA = 11)


// Create color sensor
Adafruit_TCS34725 tcs = Adafruit_TCS34725(TCS34725_INTEGRATIONTIME_50MS, TCS34725_GAIN_1X);


// Create display:
Adafruit_ST7735 tft = Adafruit_ST7735(TFT_CS, TFT_DC, TFT_RST);


#include <Fonts/FreeSerif18pt7b.h>  // Add a custom font


char btchar = 0;      // bluetooth input character
int cat;              // cat ID : 0 = dark cat, 1 = light cat
int event = 0;
int lrevent = 0, rlevent = 0, rlfevent = 0, lrfevent = 0;
char catevent;
int catc;             // cat color


void setup()  // Start of setup
{


  // Display setup:


  // Use this initializer if you're using a 0.96" TFT
  tft.initR(INITR_MINI160x80);  // Initialize a ST7735S chip, mini display


  tft.fillScreen(ST7735_BLACK);  // Fill screen with black


  //tft.setRotation(0);  // Set orientation of the display = portait


  tft.setTextWrap(false);


  // Display static text:
  tft.setTextSize(2);  // Set text size. Goes from 0 (the smallest) to 20 (very big)
  tft.setCursor(0, 0);  // Set position (x,y)
  tft.setTextColor(0x001F, ST7735_BLACK);  // RED text with BLACK background
  tft.println("RED");  // Print a text or value
  tft.setCursor(0, 18);  // Set position (x,y)
  tft.setTextColor(0x07E0, ST7735_BLACK);  // GREEN text with BLACK background
  tft.println("GRN");  // Print a text or value
  tft.setCursor(0, 36);  // Set position (x,y)
  tft.setTextColor(0xF800, ST7735_BLACK);  // BLUE text with BLACK background
  tft.println("BLU");  // Print a text or value
  
  tft.setTextColor(ST7735_WHITE, ST7735_BLACK);  // Set text white on black background


  // Color Sensor setup:
  pinMode(8, OUTPUT); // color sensor white LED


  //PIR Setup
  pinMode(18, INPUT); // right PIR
  pinMode(19, INPUT); // high PIR
  pinMode(20, INPUT); // left PIR


  Serial1.begin(9600);
  Serial1.println("Cat Spy");

}  // End of setup


void loop()  // Start of loop
{
  int lp, hp, rp;
  char cato = "N";
  int color, r, g, b, c, colorTemp, lux, catl;
  int isf;  // color scaling factor
  float sf; // color scaling factor
  float rd, gr, bl; // color components
  int rc, gc, bc; // corrected RGB
 rp = 0;
 lp = 0;
 rp = digitalRead(18);
 hp = digitalRead(19);
 lp = digitalRead(20);
  if (lp == 1)  // left PIR detected
  {
    tft.fillRect(0, 60, 10, 10, 31);  // light left
  } else
  {
    tft.fillRect(0, 60, 10, 10, 0);  // light off left
  }
  if (hp == 1)  // high PIR detected
  {
    tft.fillRect(35, 60, 10, 10, 31);  // light high
  } else
  {
    tft.fillRect(35, 60, 10, 10, 0);  // light off high
  }
  if (rp == 1)  // rihgt PIR detected
  {
    tft.fillRect(70, 60, 10, 10, 31);  // light right
  } else
  {
    tft.fillRect(70, 60, 10, 10, 0);  // light off right
  }
  if (lp == 1 && event == 0)
  {
    event = 1;
    lrevent = 1;
  }
  if (rp == 1 && event == 0)
  {
    event = 1;
    rlevent = 1;
  }
  if (event == 1)
  {
    tft.setCursor(35, 80);  // Set position (x,y)
    tft.println("E");  // event
  }
  if (lp == 1 && rlevent == 1)
  {
    rlfevent = 1;
  }
  if (rp == 1 && lrevent == 1)
  {
    lrfevent = 1;
  }
  if (rlfevent == 1 && lp == 0)
  {
    event = 0;
    rlfevent = 0;
    lrfevent = 0;
    rlevent = 0;
    lrevent = 0;
    tft.setCursor(10, 100);  // Set position (x,y)
    if (catc == 0)
    {
      catevent = "L";
      tft.println("L");  // left event
    }
    else
    {
      catevent = "l";
      tft.println("l");  // left event
    }
  }
  if (lrfevent == 1 && rp == 0)
  {
    event = 0;
    lrfevent = 0;
    rlfevent = 0;
    rlevent = 0;
    lrevent = 0;
    tft.setCursor(60, 100);  // Set position (x,y)
    if (catc == 0)
    {
      catevent = "R";
      tft.println("R");  // right event
    }
    else
    {
      catevent = "r";
      tft.println("r");  // right event
    }
  } 
  
 digitalWrite(8, LOW);  // turn on LED
 delay (10);
  tcs.getRawData(&r, &g, &b, &c);
//  tcs.getRGB(&rd, &gr, &bl);
  delay(110);
 digitalWrite(8, LOW);  // turn off LED
  colorTemp = tcs.calculateColorTemperature(b, g, r);
  lux = tcs.calculateLux(r, g, b);
  if ((r > 255) || (g > 255) || (b > 255))
  {
    r = r/8;
    g = g/8;
    b = b/8;
  }
  if ((r > 255) || (g > 255) || (b > 255))
  {
    r = r/8;
    g = g/8;
    b = b/8;
  }
  if ((r > 255) || (g > 255) || (b > 255))
  {
    r = r/8;
    g = g/8;
    b = b/8;
  }
  sf = 32/r;
  if ((r > g) && (r > b)) sf = 31/r;
  if ((g > r) && (g > b)) sf = 31/g;
  if ((b > r) && (b > g)) sf = 31/b;
  rc = int(r * sf);
  gc = int(g * sf);
  bc = int(b * sf);
//  bitWrite(color, 0, rc);
//  bitWrite(color, 5, gc);
//  bitWrite(color, 10, bc);
  color = rc + gc*32 + bc*2048; // display color
  catl = r + g + b;       // cat luminance
//  if (catl > 400)
  if (rc > bc)
  {
    catc = 1;   //Nugget
  }
  else
  {
    catc = 0;   //Shmoopy
  }
    // Fill the digit space with background color:
  tft.fillRect(64, 0, 40, 60, ST7735_BLACK);  // blank the values


    // Fill the color space with RGB color:
  tft.fillRect(0, 72, 80, 70, color);  // Draw filled rectangle (x,y,width,height,color)
  
  // Write RGB values to the display:
  if (r < 10)
  { 
    tft.fillRect(50, 0, 14, 16, 0);
  }
    if (r < 100)
  { 
    tft.fillRect(64, 0, 14, 16, 0);
  }


  tft.setCursor(40, 0);  // Set position (x,y)
  tft.println(rc);  // Print RED value
  if (g < 10)
  { 
    tft.fillRect(50, 17, 14, 16, 0);
  }
    if (g < 100)
  { 
    tft.fillRect(64, 17, 14, 16, 0);
  }
  tft.setCursor(40, 18);  // Set position (x,y)
  tft.println(gc);  // Print GREEN value
  if (b < 10)
  { 
    tft.fillRect(50, 34, 14, 16, 0);
  }
    if (b < 100)
  { 
    tft.fillRect(64, 34, 14, 16, 0);
  }
  tft.setCursor(40, 36);  // Set position (x,y)
  tft.println(bc);  // Print BLUE value


    if (Serial1.available() > 0)
    {
      btchar = Serial1.read();
      if (btchar == 'A')
      {
        Serial1.println(catevent);
        catevent = "N";
      }
    }
}  // End of loop

 

Discussion

The project was a lot of fun even though it involved a lot more mechanical design than electronic design.

The PIR sensors and their shrouds work extremely well, very reliably detecting the cats and their direction. Both the PIR sensors and the color sensor are passive - they do not emit any harmful radiation or even ultrasonic noise.

The color sensor was a lot more problematic. Although the telephoto lens did a great job of allowing colors to be detected at a distance, it needs the lighting to be pretty consistent and the firmware needs to employ a lot of normalizing and other clever analysis techniques. Daylight is way different from artificial light and each light has a unique spectrum. The color sensor datasheet indicates it can do a decent job if you have a way of calibrating it. It might need a separate color sensor just to sort out what the ambient light composition is.

If you use one of these interesting color sensors, be prepared to mess around for quite a while tuning it to your application.

Training cats to walk in front of a sensor so you can tune up its performance is just wishful thinking. This made tuning up the color sensor extremely challenging, and it still isn't where it needs to be.

The mechanical design successfully attempted to utilize an empty filament spool as a stand, and now that I have a working way to adapt a spool to a shaft, I may find more uses for all my empty spools. The plastic shaft is from a Dollar Store toy.

Considering the system has an MCU, a color graphics display, four sensors and 8 custom plastic parts, the total cost of under $15 was a nice achievement.

It took some meticulous measurement work to ensure the color sensor chip was exactly where the lens was focusing the light, but 3D printing eliminated a lot of fiddling around with files to adjust position.

Overall I learned a lot and it is always fun to see how cats respond to new situations. I was very happy with the way the PIR sensors worked and that the telephoto lens worked so well with the color sensor.

 

Related Links:

Project14 | Spy Nerd: Win Spy Gadgets for Your Security or Spy Related Project!

Spy Nerd

  • Sign in to reply

Top Comments

  • javagoza
    javagoza over 4 years ago +3
    Great project, I love it. Your design of the 3D printed parts is very ingenious. I am now working on a design to warn about unattended cooking with stoves and cooktops that could start a fire and does…
  • genebren
    genebren over 4 years ago +2
    Very fun project! I like your low cost approach to detecting cats and their direction. The mechanical aspects of the project are very cool. You friction and diamond locks work very well. I have have to…
  • dougw
    dougw over 4 years ago in reply to genebren +1
    The diamond shape for the indent locks is because that shape can be printed flawlessly on a 3D printer.
  • dougw
    dougw over 4 years ago

    Incidentally, I cannot edit the blog to fix the videos - there is no "Edit" button and no way to join the group to allow editing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago in reply to dougw

    Assembled Sensor System In Operation

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Cat House Spy Software In Action

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago in reply to dougw

    That seems to work so here are the rest of the videos that are supposed to be in the blog:

    Plastic Parts:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    3D Printed Parts Design

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago

    This is just an attempt to embed one of the videos from the blog in a comment since the videos aren't showing up in the blog.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 4 years ago

    Unfortunately, the videos didn't survive to the new forum platform.

    I cannot even post links of the videos in the comments here because the comment then gets flagged as spam and deleted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>