Spy Nerd
  • Challenges & Projects
  • Project14
  • Spy Nerd
  • More
  • Cancel
Spy Nerd
Blog Spy Nerd - Laser Communicator
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Spy Nerd to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scottiebabe
  • Date Created: 3 Nov 2021 1:52 AM Date Created
  • Views 5284 views
  • Likes 5 likes
  • Comments 9 comments
  • spynerdch
Related
Recommended

Spy Nerd - Laser Communicator

scottiebabe
scottiebabe
3 Nov 2021

The Project14 program manager(s) have put forth yet another exciting monthly project theme, this one is for all of us spy nerds. I did struggle to think of a project that would be worthy of the ‘Ultimate Spy Nerd’ crown. I had contemplated trying to prototype a laser microphone (https://en.wikipedia.org/wiki/Laser_microphone) which uses optical interferometry to measure the vibrations of objects in the vicinity of the sound emitter and then be converted into an equivalent audio signal. So, one can remotely monitor a bag of chips to learn all the latest spy gossip. That being said, I don’t have the optics for a laser Interferometry laying around in a box. So, I have instead decided to pursue a long-range laser communicator.

 

image

 

The Laser Communicator allows a spy to stay off the LF to UHF air waves while still communicating with their spy colleagues at long distances, provided there is line of sight.

image

 

 

Even if this isn’t This is the ultimate spy gadget for a spy nerd. It has been a lot of fun to building and testing this 'spy tech'. Playing with this kit reminds of playing with walkie talkies as a child, only now with lasers!

 

Proof of Concept

I am hoping to amplitude modulate the laser diode at the same carrier frequency used in mediumwave radio. So hopefully, all I need to do for the receiver side, is to add a photodiode coupled to the ferrite rod antenna. All of this rests on achieving a system bandwidth greater than the desired carrier frequency. So, I setup the laser diode and photodiode on my precision optical bench and did a quick test.

image

 

Here I am driving the laser diode module with a 1Vpp sinewave with a 4 VDC offset. Here are the results of sweeping the frequency from 100 kHz to 1200 kHz,

image

 

While this isn’t an overly scientific test, it does show I am on the right track. I think I have a pretty good chance of success with the electronics. I don’t know how well I am going to be able to test this over a 20 km optical path, but I think across a field should be quite manageable.

 

Receiver

I was able to find a low-cost pocket radio with a resonant ferrite rod antenna from a local hobby shop. I had hoped to source the radio at the Dollar store, however there was no pocket radios to be found on the store’s shelves. I had also hoped the radio would have one end of the ferrite rod antenna coil grounded. So, I could directly attach the photodiode to LC tank this would provide DC bias to maintain the photodiode operating in photoconductive mode and reject any optical signal not near the resonant frequency of the LC tank. The radio I sourced did not have one end of the ferrite rod antenna grounded. Before I even knew if this was going to be the case, I received a brilliant suggestion from member shbaz  to wind a secondary receive coil on the ferrite rod. This turned out to be an excellent solution. So, I hand wound 10 turns of 34 AWG enamel wire around ferrite rod, which operates as coupled inductor to the main resonant antenna winding. A TEFD4300 Silicon PIN Photodiode https://www.vishay.com/docs/83471/tefd4300.pdf, was then solder reverse biased to the newly added secondary receive coil.

 

image

 

For the stealthy spy look, I drilled a 7/64” hole near the telescoping antenna and forcefully slide the T1 photodiode into place. After making these modifications to the pocket radio, we now have a laser communicator receiver suitable for any spy nerd.

image

 

Transmitter

I am going to run a DDS on the 2nd core of a RPI Pico and then AM modulate the carrier by simply using a multiplying DAC (DAC0800).https://www.ti.com/lit/ds/symlink/dac0800.pdf

image

Audio Input

image

Amplitude Modulation

I Implemented amplitude modulation by using the audio input to derive the reference current for the DAC0800 (single quadrant multiplying DAC)

image

 

The audio source volume/level then defines the AM modulation index. Here I am adjusting the playback volume from minimum to maximum which eventually results in clipping:

image

 

DDS - Sample Clock

For this project, I am going to use a PIO state machine on the Rp2040 to define the DDS sample clock. To instantiate an 8-bit parallel FIFO state machine in uPython one can make use of the following python code:

# 8-bit parallel transmit FIFO
@rp2.asm_pio(out_shiftdir=1, autopull=True, pull_thresh=8, out_init=([PIO.OUT_LOW]*8),fifo_join=PIO.JOIN_TX)
def ddspio():
    wrap_target()
    out(pins, 8)
    wrap()

# Create a PIO StateMachine with the ddspio program, outputting on pins gp0 - gp7
sm = rp2.StateMachine(0, ddspio, freq=25_000_000,  out_base=Pin(0))
sm.active(0)
# load FIFO with some interesting data
for i in range(8):
   sm.put(i)
    
print('TX0 FIFO Count: {}'.format(mem32[0x50200000+0xc]))
sm.active(1)

 

Which will output binary codes 0 through 7 across GPIO pins 0 through 7, with a sample clock of 25 MHz

 

image

 

DDS - Assembly Template

This looks simple now, but it took along time to get to that point from hard lessons in past projects. Here I am counting down from 32 and during each loop iteration writing the counter value (r1) to the PIO TX0 FIFO.

@micropython.asm_thumb
def ddsasm(r0):
    ldr(r1,[r0,0])
    ldr(r2,[r0,4]) # r2 = addr PIO_BASE
    label(START)
    ldr(r3,[r2,0x0C]) # check to see if TX0 FIFO is full
    cmp(r3,8)
    beq(START)
    str(r1,[r2,0x10])
    sub(r1,1)
    cmp(r1,0)
    bne(START)
    
fptr = array.array('i',[ 32, 0x50200000, addressof(LUT), 3])
ddsasm(fptr)

 

I also had to slow down the PIO state machine to 15 MHz as this assembly loop takes more than 5 clock cycles. Also note, in this basic example the compare and branch not-equal falls through on 0, so a 0 is never written to the TX FIFO.

image

 

DDS - Sine Look Up Table

It's moments like this where uPython really presents a warm charm. In the past I would have hardcoded a lookup table as an array, but it's a one liner in python. So, during initialization I instantiate a sine lookup table in memory by:

# Sine LUT 10-bit phase input to 8-bit DAC code
ILUT = [ int(127.5*math.sin(x*2*math.pi/1024) + 127.5) for x in range(1024)]
LUT = bytearray(ILUT)
del ILUT

I exported the LUT to double check it was correct, this was as simple as:

f = open('lut.dat','wb')
f.write(LUT)
f.close()

Here is the LUT plotted for all input phase codes:

image

DDS - NCO

Just a sneak peak before I consider this ready for primetime:

    add(r4,r4,r1) # Add the TUNEING word to the phase accumulator
    lsr(r5,r4,22) # slice the upper 10 bits of the ACCUM into r5
    add(r5,r3,r5) # add the LUT address to r5
    ldrb(r6,[r5,0]) # r6 = LUT[ACCUM<31:22>]
    str(r6,[r2,0x10]) #store in sio memory 1 cycle

We are definitely getting close:

image

Making Waves... Sine Waves image

image

Here I am just using a 1kHz tone generated from my function generator as the audio input and running the DDS at 20 kHz.

image

DDS - Reconstruction Filter

The DDS is operating with a sample rate of 22.5 MHz, so I have arbitrarily chosen my reconstruction filter to have a cut-off frequency of 10 MHz. Depending on the level of attenuation achieved in the filter's stop band, the reconstruction filter will attenuate the unwanted aliased sampling images.

image

I prototyped a 3rd order Butterworth filter designed for a source and load impedance of 600 Ohms.

image

In order to measure the frequency response of the filter with my NanoVNA, I needed to increase the effective source and load resistance as seen by the filter.

image

The series inductor was sourced from 270 uH inductor with approximately 70% of the turns removed (inductance scales with the square of the number of turns). The two shunt capacitors each consisted of a 20 pF and 10 pF capacitor in parallel.

image

 

To measure the frequency response of the filter I make a S21 measurement with my NanoVNA:

image

 

Note because I added series resistors to achieve the 600 ohm source/load impedance there will be a baseline insertion loss of -22 dB.

image

Not too bad for a quick little prototype. You can see the inductor self-resonate at approximately 33 MHz, which limits the high-frequency stop band attenuation. The Nano-Savers filter analysis tool reported a cut-off frequency of 10.3 MHz.

 

image

 

DDS – NCO V2.0

Some of the DDS calculations and bit operations can be implemented on one of the RP2040’s Interpolators located in the single-cycle IO block.

image

I was able to implement some of the DDS core operations, namely, incrementing the phase accumulator and generating the DAC lookup table element address.

ACUM0 : Phase Accumulator

BASE0: NCO Tuning Word

BASE2: LUT Base Address

Upon reading from one of the POP registers, in this case POP_RESULT2, the accumulator registers are clocked and new DDS sample is calculated and available on the next read of the result2 register. After making use of the interpolator to offload some of the DDS calculations I was able to achieve a sample rate of 30 MSa/s. A sample rate of 30 MSa/s is really pushing the vintage through-hole DAC0800 to its limits, however there are modern surface mount DACs available. If one doesn’t need amplitude modulation, you can use a resistor R-2R ladder DAC connected directly to the RP2040’s GPIO pins. Ultimately, I was able to reduce the following instructions:

    add(r4,r4,r1) # Add the TUNEING word to the phase accumulator
    lsr(r5,r4,22) # slice the upper 10 bits of the ACCUM into r5
    add(r5,r3,r5) # add the LUT address to r5

To a single register load from the interpolator's result2 register:

    ldr(r5,[r4,0]) # Read Interp Result

 

Essential Bill of Materials

 

 

ComponentNewark PN
RPi PicoRaspberry Pi Pico, Microcontroller Board, RP2040, 32 bit, 2MB Flash, ARM Cortex-M0+Raspberry Pi Pico, Microcontroller Board, RP2040, 32 bit, 2MB Flash, ARM Cortex-M0+
DAC0800IC, 8BIT DAC, PARALLEL, 16DIPIC, 8BIT DAC, PARALLEL, 16DIP
MCP601Operational Amplifier, Single, 2.8 MHz, DIP, 8Operational Amplifier, Single, 2.8 MHz, DIP, 8
7660 Charge PumpCharge Pump Voltage Converter, 1.5V to 12V in, -12V to -1.5V/45 mA out, DIP-8Charge Pump Voltage Converter, 1.5V to 12V in, -12V to -1.5V/45 mA out, DIP-8

650 nm Laser Diode

-
Pocket Radio-
TEFD4300 PhotodiodePhotodiode, 20 °, 150 pA, 950 nm, T-1 (3mm)Photodiode, 20 °, 150 pA, 950 nm, T-1 (3mm)

 

 

 

Demo

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Thanks for reading! Comments and suggestions are always welcome image.

Attachments:
main.txt.zip
  • Sign in to reply

Top Comments

  • dougw
    dougw over 5 years ago +1
    Cool - a laser phone
  • scottiebabe
    scottiebabe over 5 years ago in reply to shabaz +1
    Nonsense about image quality, you always post the most interesting photos. I have one of the TECSUNs with an SI Labs DSP radio and I am really happy with it, I will keep your suggestion on my shortlist…
  • scottiebabe
    scottiebabe over 5 years ago +1
    Dollar store pocket radios may be a relic of yesterdays. Though you can now buy a water-resistant Bluetooth speaker for ~$3 USD, just amazing. You can find the FCC application for this Bluetooth speaker…
Parents
  • scottiebabe
    scottiebabe over 5 years ago

    Success! I managed to find cheap pocket radio,

    image

    The circuitry is almost identical to the solder kit I showed above. Taking shabaz's recommendation I wound a few turns on the ferrite antenna:

    image

    With the addition of a photodiode I had a working prototype for the receiver side. Too cool! I am feeling like a spyimage

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to scottiebabe

    Awesome results - very creative LoS comms

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 5 years ago in reply to scottiebabe

    Awesome results - very creative LoS comms

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • scottiebabe
    scottiebabe over 5 years ago in reply to dougw

    Thanks! Though I must confess for that example I transmitted the audio FM modulated as my function-gen doesn't haven't have AM modulation abilities.

    image

     

    Then relied on the resonant tank to slope demodulate the FM to AM.

     

    It going to make for an exciting demo, unlike the laser to cds cell baseband transmission examples, this methodology can tolerate significant path loss. I can place a piece of paper or white bubble foam in front of the detector and still recovery the transmitted audio.