Techno Toys
  • Challenges & Projects
  • Project14
  • Techno Toys
  • More
  • Cancel
Techno Toys
Blog Which Project Theme Do You Want for June 2017?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Techno Toys to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 13 Apr 2017 9:28 PM Date Created
  • Views 2995 views
  • Likes 6 likes
  • Comments 16 comments
  • monthly_theme_poll
  • which project theme do you want for june 2017?
  • project14
Related
Recommended

Which Project Theme Do You Want for June 2017?

tariq.ahmad
tariq.ahmad
13 Apr 2017
image

Project14

Monthly project competitions, chances to win prizes, you decide monthly themes, your ideas, your projects, turn ideas into projects.

Back to The Project14 homepage image

About Project14
Theme Archive
Monthly Theme Poll

 

This poll is now closed.  You voted for Going Green and it will launch on June 14, 2017! 

 

 

Please visit Project14 | You Decide the Next Monthly Project Competition! to continue the conversation and vote on the next project competition.  

 

This will be the new place to discuss ideas and vote on project themes moving forward! 

 

 

How are Monthly Themes selected?

  • On the 14th of every month a new poll will go up with themes to choose from (initial themes and the first two monthly themes were chosen based on feedback from Top Members)*
  • Comments will be used to decide themes for upcoming polls.
  • If you like an idea for a theme you can increase the odds that it will be used in a poll by "liking", "commenting", or "marking it helpful".
  • The poll will close on the 14th of the following month at which time it will be replaced by a new poll.
  • The poll will decide the monthly project competition for the next following month.

 

How do you submit your own Project14 idea?

  • Present your theme idea in the comments section of the monthly poll
    • If you think of an idea for a monthly project competition theme you can select the final option to vote a new idea which you present in the comments section.
    • You can also vote for an existing theme idea in the monthly poll and submit as many monthly theme ideas as you like in the comments section.
  • If you would like to present an idea but would like feedback from other community members first, you can start a new discussion thread.

 

Have an idea of your own for a Monthly Theme?

 

Use the comments below to give community members more ideas to vote on!

  • Sign in to reply

Top Comments

  • dougw
    dougw over 9 years ago +8
    These are all great topics, if they are not selected right away, they shouldn't be completely discarded. Maybe the Project14 page could keep a running list of all ideas. Ideas for future polls home-made…
  • dougw
    dougw over 9 years ago in reply to jc2048 +4
    "Home-made test instrument sounds good. I'd do that one (but then I can cheat because it's on the go already)." Getting a head start is perfectly acceptable "Cool LED display. What does 'display' mean…
  • mcb1
    mcb1 over 9 years ago in reply to dougw +3
    wacky automation device or Rube Goldberg machine - like the box with a toggle switch - when you turn it on the box opens and turns off the switch. I like that one ....needs to have something clever about…
Parents
  • dougw
    dougw over 9 years ago

    tariq.ahmad is this the right place to keep suggesting more Project14 ideas?

    I was thinking it might be interesting to have a contest to put together a classroom demonstration of some physics phenomenon.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to dougw

    That's an interesting idea.

     

    I can immediately think of two that I've thought of doing, but have never got around to:

     

    1) measurement of the speed of propagation of a signal in a metre of hook-up wire, first with the insulation intact and then with the insulation removed

     

    2) measurement of the vertical voltage field due to the ionosphere (that would have to be done outside and not in a classroom - hooray, we're off on a field trip). Apparently, it's something like 100V per metre, but I'm not sure it's very easy to measure what with air being such a good insulator. [I can vaguely remember something from years ago - maybe it was done by the 'Amateur Scientist' in Scientific American back in the late sixties or early seventies - where a JFET was used, though I can't quite puzzle out how you get power to the device without that then messing up the measurement. Perhaps the source load could be a long chain of resistors a metre high, or something, with a tap near the bottom to measure a known proportion of the value.]

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 9 years ago in reply to jc2048

    Great ideas.

    2) Perhaps if the measurement circuit is far from the measurement location and the leads are kept several meters apart .....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 9 years ago in reply to jc2048

    Great ideas.

    2) Perhaps if the measurement circuit is far from the measurement location and the leads are kept several meters apart .....