Techno Toys
  • Challenges & Projects
  • Project14
  • Techno Toys
  • More
  • Cancel
Techno Toys
Blog Xylophonomatic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Techno Toys to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tech_nut81
  • Date Created: 21 Apr 2017 6:48 PM Date Created
  • Views 2706 views
  • Likes 5 likes
  • Comments 9 comments
  • techno_toys
  • auto_avoidance
  • xylophone
  • ttoysch
  • project 14
Related
Recommended

Xylophonomatic

tech_nut81
tech_nut81
21 Apr 2017

So, if you've seen my comment on "Give New Life to Old Toys by Turning Them Into Techno Toys! ", then you know I'm trying to turn my old Fisher Price, pull-a-tune xylophone into an object avoiding, robot xylophone.

image

image

I took the advice of the people that replied to my idea and built an auto avoidance prototype first. I used one of my sons old remote control trucks that no longer worked by remote control.

Here is a picture of my prototype. (I'll try and upload some videos a little later).

For this prototype I used an old RC car, an Arduino Uno, ultrasonic rangefinder, and an L293 H-bridge. After I finally got the code worked out, it worked pretty well. It could be better of course. The range sensor is facing upward slightly so it will still bump into stuff every now and then because it sees it too late to stop. I haven't been coding long at all, but I was able to find several examples to point me in the right direction.image

For my final build, I plan on using another of my sons dilapidated RC cars, (he's really rough on em), to power the xylophone. I think attaching motors to the existing axles will be too difficult because they are bent in a way that will allow them to control the hammers that strike the plates. So, I had originally thought about drilling new axle holes and making a new axle that I could attach my motors to, but I've scrapped that plan now too. Now I'm leaning toward attaching the axle and wheels from the RC car to the rear of the xylophone and having them push and pull it across the floor.

Kinda like this,

image

That leaves me with only one problem. How am I going to get this thing to turn? The RC car axle is fixed with one motor controlling both wheels simultaneously. So that's where I'm at with that.

If anyone has any tips or suggestions I'd be happy to hear them.

 

.......

Update #1

OK. As promised, here is the video of my prototype.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I've made some improvements to the prototype thus far. I mounted the range sensor to a servo so that it can look around and I modified the axle so that the two drive tires could be powered separately.

.......

Update #2

Alright, as embarrassing as this next video is, I'm still going to post it for the sake of transparency in my project.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The problem here is that my left wheel does not have as much torque as my right wheel after I modified the axle. So, I'm gonna have to open it back up and add gears, or 'recreate the wheel', no pun intended. I thought about using a different motor for the left wheel, but I barely fit the little motor that's in there now, so, I'm sure I don't have room for anything bigger.

 

Back to the drawing board.

 

DJ

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 9 years ago +5
    With a bit of redesign you could perhaps steer it BigTrak style, with two independently controlled motors in the centre of the xylophone. ( There is a BigTrak conversion going on over at this blog: BigTrak…
  • beacon_dave
    beacon_dave over 9 years ago +5
    I think when tackling a project like this you need to be aware of the 'essence' of the original toy that you should try and retain where possible. For me, I think the overall shape and colour scheme and…
  • tech_nut81
    tech_nut81 over 9 years ago +5
    I've added a brief update in the blog along with a video of my prototype. I hope to have everything completed and uploaded next week. This week as well as the past two weeks have been really hectic with…
Parents
  • beacon_dave
    beacon_dave over 9 years ago

    With a bit of redesign you could perhaps steer it BigTrak style, with two independently controlled motors in the centre of the xylophone.

     

    ( There is a BigTrak conversion going on over at this blog:

    BigTrak Conversion Part 1 )

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 9 years ago

    With a bit of redesign you could perhaps steer it BigTrak style, with two independently controlled motors in the centre of the xylophone.

     

    ( There is a BigTrak conversion going on over at this blog:

    BigTrak Conversion Part 1 )

    • Cancel
    • Vote Up +5 Vote Down